Hot!MPLAB X IDE 4.00 on Windows XP and co-existing with MPLAB 8

Author
IO
Starting Member
  • Total Posts : 76
  • Reward points : 0
  • Joined: 2011/01/08 11:45:44
  • Location: 0
  • Status: offline
2017/08/13 02:46:11 (permalink)
0

MPLAB X IDE 4.00 on Windows XP and co-existing with MPLAB 8

Hi,
I would like to install MPLAB X IDE 4.00 on Window XP Pro SP3.
From the release notes:
 MPLAB X IDE is no longer supported on Windows XP. This means MPLAB X IDE will no longer be tested on Windows XP and JRE8 will be the new default JRE. To continue using Windows XP, JRE 7 will need to be installed. The MPLAB X IDE installer will search for JRE 7 on your system, and if it is not found will recommend sites for download.

 
Does anyone here run the recent versions of the MPLAB X on Windows XP?
 
And more importantly, will it break an existing MPLAB 8 installation? I cannot afford to break it.
 
Thanks.
#1

3 Replies Related Threads

    CinziaG
    morite
    • Total Posts : 3142
    • Reward points : 0
    • Joined: 2016/12/07 14:20:36
    • Location: Wien
    • Status: offline
    Re: MPLAB X IDE 4.00 on Windows XP and co-existing with MPLAB 8 2017/08/13 03:02:52 (permalink)
    +2 (2)
    Yep, all ok in here Smile
    I.e. nothing changed since last version 3.65
    I use both without special issues apart from Switching Drivers for my ICD3 from 8 to X when needed: but yesterday I tried IPE for programming a HEX generated with 8 and it does work.
    Crazy interface just like the one for X (...) but it does work.
     
     

    get my books!
    lulu.com search.ep?keyWords=greggio&type=
     
    #2
    IO
    Starting Member
    • Total Posts : 76
    • Reward points : 0
    • Joined: 2011/01/08 11:45:44
    • Location: 0
    • Status: offline
    Re: MPLAB X IDE 4.00 on Windows XP and co-existing with MPLAB 8 2017/08/13 03:09:23 (permalink)
    +1 (1)
    That is good to hear.
    #3
    RISC
    Super Member
    • Total Posts : 4991
    • Reward points : 0
    • Status: offline
    Re: MPLAB X IDE 4.00 on Windows XP and co-existing with MPLAB 8 2017/08/14 17:12:32 (permalink)
    +1 (1)
    Hi,
    MPLAB X is totally different from MPLAB V8 so you can install both without any issue.
    Just remember that MPLAB X is not tested on XP machines sinces several years so it may / may not work.
    As you know XP support has been dropped by MS for several years.
    Regards
     
    #4
    Jump to:
    © 2018 APG vNext Commercial Version 4.5