Hot!MPLABX (+harmony)

Author
xpicolo
Starting Member
  • Total Posts : 35
  • Reward points : 0
  • Joined: 2010/08/05 23:38:59
  • Location: 0
  • Status: offline
2017/08/12 23:39:25 (permalink)
5 (2)

MPLABX (+harmony)

Hi,
 
I have some experience in using IDEs.
And I appreciate the effort to make MPLABX and Harmony.
But many , many errors make their use a torture.
For simple things, it's good. If you want to do something more complex, it's ... embarrassing.
 
"Connection failed" (at PICkit3) after a few minutes. after restarting MPLABX, it's good.
Debugging tools were not found ... for no reason, after restart mplabx, pickit3 work Ok.
Many false alert / error notifications.
Breakpoints are garbage (many times when they refuse to put them or hold them)... after restart, works Ok.

I think you are not in the right direction with this development.
 
post edited by annapolis - 2017/08/13 08:47:34
#1

2 Replies Related Threads

    TS9
    Super Member
    • Total Posts : 514
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: MPLABX (+harmony) 2017/08/13 00:13:20 (permalink)
    0 (2)
    What is yours expectations?
    In Simple If you don't like harmony Write your code by own. Like many do
    post edited by annapolis - 2017/08/13 08:48:02
    #2
    RISC
    Super Member
    • Total Posts : 4991
    • Reward points : 0
    • Status: offline
    Re: MPLABX (+harmony) 2017/08/14 17:18:28 (permalink)
    0
    Hi,
    Which PIC32 do you use ?
    Pickit3 is very slow at programming large flash devices so it is probably not the right tool to use to develop PIC32...
    I generally use ICD3 or Real-Ice with PIC32 harmony projects because flash images become large as soon as you use protocol stacks...and I don't want to wait a couple of mn for programming ;=)
    Additionally Pickit3 does not support SW breakpoints or data breakpoints
    Regards
    #3
    Jump to:
    © 2018 APG vNext Commercial Version 4.5