Induction Cooktop Reference Design
Search
To Bottom
Evaluation and Demonstration Boards
Induction Cooktop Reference Design
2017/05/05 15:09:53
AlertIowa1234
Hello, are the reference designs for the Induction Cooktop still available? Because I've been looking for schematics & gerber files of it but not having any luck. Any help would be appreciated.
2017/05/05 15:17:30
qhb
Are you sure you are on the right website?
Have Microchip ever done anything related to induction cooking?
2017/05/05 15:19:56
AlertIowa1234
Yes they have, see here:
http://www.microchip.com/...oktop-reference-design
2017/05/05 16:25:41
qhb
I guess you need to contact them via the email address on that page.
For more information, please email
appliance@microchip.com
.
2017/05/05 16:45:12
AlertIowa1234
I tried emailing them at that email but it says it failed because its not a valid email address.
2017/05/05 18:02:08
NKurzman
Put in a Support Ticket.
Than call after 24 Hours.
2017/05/06 10:56:35
CinziaG
wow! interesting
2017/05/07 01:46:20
Nikolay_Po
Pair month ago I had repaired an induction cooktop with 4 heaters. The induction part was built on dsPIC33EP...MC chip. 4 current transformers, 4 half bridge drivers and one dsPIC in the middle. It was one of Europe's home appliances brand. The problem was the damage of high side driver supply by some liquid due to bad mounting. Except the liquid damage the rest of power circuit under dsPIC control survived.
2020/10/12 07:22:25
Aeronautics
Looking for this reference design too.
Microchip's page seems to be deleted, page on webarchive do not include any design content.
Contacted on official email without a luck.
Send to Recycle Bin
Delete Permanently
© 2021
APG vNext
Commercial Version 4.5
Latest
Active
Sign up
Log in
Full Ver.
About
back
Use My Existing Forum Account
Username:
Password:
Log in