Suggestion for ICD 2 Users
Search
To Bottom
General PIC32 Topics
Suggestion for ICD 2 Users
2009/01/27 10:24:54
PIC32 Support
When using the MPLAB ICD 2 in MPLAB IDE make sure the configure->configuration bits window is is closed when not in use. This will reduce lock-ups.
From the MPLAB ICD 2 readme in the
MPLAB IDE 8.20 release notes
ICD2-322:
PIC32 debugging using MPLAB ICD 2 under MPLAB IDE may lock-up on heavily loaded systems if the Configure>Configuration Bits window is open during the debug session. Please close the Configure>Configuration Bits window before programming if the ICD2 is selected as a Debugger.
2010/03/08 11:31:39
Mr Checkbox
Another suggestion: Use ICD3. It rocks!
2011/08/08 01:18:20
Tempest
I am using in ICD2 to try and program a PIC32MX440 chip but it keeps giving me the "device not ready" error. Since it gives the same error when the board is disconnected I'm assuming a communications error or a fault with my ICD module. The self check comes back ok however. I have checked all the connections manually since I had to make a new cable to account for the positioning of the connections on my board. Is there anything in MPLAB I should try or should I try a different ICD2 module?
2011/10/02 17:47:00
DmitriK
Yes, try to manually re-load the firmware on the ICD2
2011/12/27 12:33:46
eng.cleber
For programming, erasing, Verification and reading, with the ICD 2 for the new chips produced from August 2011 ("after 1120 batch") no longer works. Thus you need to buy the ICD 3.
Somebody know about this? Could someone explain better?
Cléber
2012/04/17 09:10:34
kimberly8r
Thanks for your information
2012/12/15 16:56:40
Aladin
Hello please advice where I can find a table for ...
To PIC32MX795.
void __ISR( _TIMER2_VECTOR, ip14){..
What is it:
?????????i p14 ???????
?????????i p17 ???????
Thank you best regards Aladin
Czech Land
Send to Recycle Bin
Delete Permanently
© 2021
APG vNext
Commercial Version 4.5
Latest
Active
Sign up
Log in
Full Ver.
About
back
Use My Existing Forum Account
Username:
Password:
Log in