• Ethernet
  • KSZ8895 as unmanaged/managed switch is not working.
2020/11/13 04:05:11
m_snaeem@hotmail.com
Hello,

Ihave tried to create an unmanaged switch using ksz8895 ethernet switch IC.
but i can get connected with internet using switch.
i have tried to use it is as unmanaged switch in default setting but no success.
Board is getting 122mA current which is constant.
i have attached the Circuit diagram. 
Can any body help me to find the error.
© 2021 APG vNext Commercial Version 4.5

Use My Existing Forum Account