2020/10/08 10:09:01
jmxiqz
Hello, I hope you can help me, I am trying to use the ds18b20 with the pic18f4550, I have been investigating a lot according to me my code should work but it does not work, according to me the problem is when starting the communication. If I declare adcon1 to configure the digital inputs the reset function returns 0, if I do not configure adcon1, the reset function returns 0 but the temperature reading is always 0


2020/10/09 19:29:16
ric
© 2021 APG vNext Commercial Version 4.5

Use My Existing Forum Account