2020/09/23 06:24:44
AlbinCaliber@
 I want to use wifi USB dongle in sam9x60 board . So that I  build atmel-poky OS for sam9x60 and it's working fine. But when I see the wlan0 section it's populating error at the time of  booting and also I can't see the wlan0 when am using ifconfig command.


Error:

Could not read interface wlan0 flags: No such device
nl80211: Driver does not support authentication/association or connect commands
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
Could not read interface wlan0 flags: No such device
wlan0: Unsupported driver ''
Cannot find device "wlan0"
 
I wonder if you could help me with this?

Thank you.
 
 
© 2021 APG vNext Commercial Version 4.5

Use My Existing Forum Account