2020/09/05 06:33:50
ChristianIPM
Hello,
 
i have a problem implemintig a bluetooth connection with the RN4871 to a controller where is cannot modify the software. So every time when i connect to the RN4871 with my mobile divice, it sends out the status string which cuases the controller to reboot. The Controller does not have an option to ignore the masked status string.
Is there any possibility to switch off the status string output completely or could this function be added?
2020/11/13 07:44:08
Nicolas Det
Same here. I would like to disable the status messages to get a clean UART comunication..
© 2021 APG vNext Commercial Version 4.5

Use My Existing Forum Account