HI,
I have added the KSZ8895 as an unmanned switch.
If I erase the I²C eeprom then the switch works OK.
If I fill the 256 bytes and program the eeprom, the switch stops responding.
Is there a file with all 256 parameters for a unmanned switch?
Is there some documentation how to setup the eeprom to get the switch working just as if there was no eeprom present?
It would be much easier to start working with a known setup.
Best regards,