Hi Gents,
I've just received some BM62 bluetooth module, I've mouted them on my PCB design.
According to the steps described on the DevKit manual I've done the following steps :
- Generate the .txt file with the DSP parameters using DSPTool_IS206x_012_DualModeSPK1.1_v1.06.exe
- Generate the .txt file with UITool_IS206x_012_DualModeSPK1.1_v1.03.exe with IC package=BM62
- Merge the files using MPET.exe using the default bin file IS206X_012_DUALMODESPK1.1_E1.0.0.2_0FCD.bin
-> then I generate an Ipf file to write on BM62 EEPROM
Using EEPROM_Tool_V4851.exe I've got MPSE Name : IS2064S_012_SPK02_V2.1_BETA
I'm trying to write on the EEPROM but i've got the following error : ''Device's IC version doesn't match file's IC Version: IS206X_012_DUALMODESPK1.1_E1.0""
When I'm doing the same steps with the DevKit it is working fine, the EEPROM tool is giving me MPSE name = IS206X_012_DUALLMODESPK1.1_E1.0
both module are BM62 so I'm not really understanding the meaning of the MPSE Name
Can anyone help with this error?
Thanks for your help
Regards
Bruno