LAN7800 NDIS Driver v18.12.12.0 for Windows (x86, amd64, arm32 and arm64) ========================================================================= This file provides information about the Ndis drivers for Windows Operating Systems (32 bit x86, 64 bit amd64, 32 bit arm, and 64 bit arm) for the LAN7800 family of devices. Contents -------- A. Microchip Devices and Windows Operating systems Supported B. Pre-installation requirements B.i. x86/x64/arm64 based Computers/Devices (Desktop/Laptop/Notebook/Tablets/2in1s/etc) B.ii. Windows Embedded handheld / Windows RT (ARM) and Windows 10 IOT (arm 32 bit and x86/x64 based) devices B.iii. Test Signing C. Automated Installer based instructions D. Installer Multi-language support E. INF based installation instructions E.i. Intel Processor (x86/x64) based Computers/Devices (Desktop/Laptop/Notebook/Tablets) E.ii. Windows Embedded handheld / Windows RT (ARM) and Windows 10 IOT (ARM and x86/x64 based) devices E.iii. INF based Package Contents F. Driver Configurable Parameters G. Release Types H: Testing I. Known issues J. Release History A. Microchip Devices and Windows Operating systems Supported ------------------------------------------------------------ This release is targeted for the following purposes (see section "G. Release Types" for details): Production (X) PreProduction (X) Engineering Testing ( ) | | | | | --> arm64 driver | --> all drivers except arm64 For Engineering Releases additional installation steps might be required, be sure to pay attention to "Pre-installation Requirements" under Section B. This distribution supports the following Microchip Devices: - LAN7800 - LAN7801 - LAN7850 This distribution contains drivers compliant to the NDIS 6.0 (Windows Vista), 6.20 (Windows 7), 6.30 (Windows 8.x) and 6.50 (Windows 10). Microsoft Certification (see Section G for Submission IDs/reports) - Windows 10 (32 bit x86) : v3.8.4.0 Yes - Windows 10 (64 bit x64) : v3.8.4.0 Yes - Windows 10 (32 bit arm) : v3.8.4.0 No (Not Available) - Windows 10 (64 bit arm64) : v3.8.4.1 No (Preview Release) - Windows 8.1 (32 bit x86) : v3.8.4.0 Yes - Windows 8.1 (64 bit x64) : v3.8.4.0 Yes - Windows 8.1 (32 bit arm) : v3.8.4.0 No (No longer Available) - Windows 8 (32 bit x86) : v3.8.4.0 Yes - Windows 8 (64 bit x64) : v3.8.4.0 Yes - Windows 8 (32 bit arm) : v3.8.4.0 No (No longer Available) - Windows 7 (32 bit x86) : v3.8.4.0 Yes - Windows 7 (64 bit x86) : v3.8.4.0 Yes - Windows Vista (32 bit x86) : v3.5.2.0 No (No longer Available) - Windows Vista (64 bit x64) : v3.5.2.0 No (No longer Available) B. Pre-installation Requirements -------------------------------- B.i x86/x64arm64 based Computers and Devices (Desktop/Laptop/Notebook/Tablets/2in1s/etc) "Must-have" pre-installation requirements for both Production and Engineering releases: - Windows 7 x64 You must have windows update KB3033929 (Security Update for Windows 7 for x64-based Systems) installed. Without this update (available through Windows Update or from the download link https://www.microsoft.com/en-us/download/details.aspx?id=46148) the driver will not install properly since the OS will not be able to understand the new EV code signing certificates. - Vista: + You must have windows update KB3033929 (Update for Root Certificates [June 2011]) installed. Without this update (available through Windows Update or from the download link https://www.microsoft.com/en-us/download/details.aspx?id=26609) the Microchip code signing certificate (either SHA1 or SHA2) used to sign the drivers will not be recognized and the driver installation will fail. + It is highly recommended to install KB2763674 (You cannot run an application that is signed with a SHA-256 certificate on a computer that is running Windows Vista SP2 or Windows Server 2008 SP2). Without this update (available through Windows Update or from the download link https://support.microsoft.com/en-us/kb/2763674) the automated installer might not be able to run (INF based installation would still work though) "Must-have" pre-installation requirements only applicable to Engineering releases: - Windows 10 For Windows 10, only drivers signed with Microsoft certificates can be installed in a standard Windows 10 installation. Microchip is currently only signing production (Logo) and PreProduction (Attestation) drivers with Microsoft certificates, so an engineering release will not install properly in a standard Windows 10 installation unless additional steps are followed to enable what is called "Test Signing" in the system. (See B.iii Test Signing) "Should-have" pre-installation requirements for All releases: - For all Windows Operating Systems it is strongly recommended that ALL Critical Windows Updates be installed. B.ii Windows Embedded handheld / Windows RT (ARM) and Windows 10 IOT (ARM and x86/x64 based) devices Currently Microchip is only signing drivers with standard Microchip EV code signing certificates widely used in the x86/x64 desktop OS signing process. Handheld and IoT versions of the Operating System have other signing requirements which Microchip does not currently have access to. While EV signed drivers are recognized by Windows RT, we have observed that Windows 8 Embedded handheld and Windows 10 IoT core will not consistently recognize them. However, various OEMs integrating our drivers into their applications have been able to re-sign our drivers with their own certificates appropriate for the target environment. If you are evaluating these drivers, do not yet have target specific signing capability (contact your Microsoft representative for guidance on how to obtain that) and are encountering problems loading your driver into your target device / OS the best course of action is to enable what is called "Test Signing" in the system. (See B.iii Test Signing) In systems without a full GUI, you may need to enable test-signing in a different way (i.e. Remote Powershell, telnet as administrator, etc). Consult the specific instructions for your environment. B.iii Test Signing The procedure is very simple, but we recommend it only be done in test machines since it relaxes the system protection against not only Microchip but any other third party signed driver. If you do not want to enable test signing, please use the latest production release instead of an engineering release. In order to enable test-signing in a system: 1. If "Secure boot" is enabled, disable it. This setting is available through your systems' BIOS settings and will require you to reboot your system to take effect. 2. Open an Administrative Command prompt (right click over the start button, select "Command Prompt (Admin)" and accept the User Account Control prompt by clicking 'Yes' 3. Type "bcdedit /set TESTSIGNING on" (without the quotes) and press ENTER. You should see the message "The operation completed successfully" 4. Reboot the system. 5. The system should now be TESTSIGNING enabled and an engineering release should install with no problems. C. Automated Installer based instructions ----------------------------------------- This section is only applicable to Intel Processor (x86/x64) based Computers and Devices (Desktop/Laptop/Notebook/Tablets). To install the driver double click on the LAN7800-WDF-vx.x.x.x.exe (where x.x.x.x is the version number of the installer). The dialogs will guide you through the installation. The driver package creates the control panel entry (Programs and Features). The driver can be uninstalled from the control panel (Programs and Features -> uninstall). Note: If the driver is uninstalled from the device manager the control panel entry will not be removed. Silent installation: To install the driver without the user interaction please execute below command on the windows command prompt. >LAN7800-WDF-vx.x.x.x.exe /exenoui /q Silent un-installation: To un-install the driver without the user interaction please execute below command on the windows command prompt. >LAN7800-WDF-vx.x.x.x.exe REMOVE=ALL /q D. Installer Multi-language support ----------------------------------- This section is only applicable to Intel Processor (x86/x64) based Computers and Devices (Desktop/Laptop/Notebook/Tablets). The installer LAN7800-WDF-vx.x.x.x.exe supports multiple languages. The installer detects the native OS language and display the dialogs in the respective language. The below languages are supported: 1. Arabic 2. Bulgarian 3. Chinese Traditional 4. Chinese Simplified 5. Czech 6. Danish 7. Dutch 8. English (US & UK) 9. Finnish 10. French 11. German 12. Hungarian 13. Italian 14. Japanese 15. Korean 16. Polish 17. Russian 18. Spanish 19. Swedish 20. Catalan (Spain) 21. Croatian (Croatia) 22. Norwegian 23. Portuguese (Portugal & Brazil) 24. Slovak (Slovakia) 25. Slovenian (Slovenia) 26. Ukrainian E. INF based installation instructions -------------------------------------- E.i x86/x64/arm64 based Computers and Devices (Desktop/Laptop/Notebook/Tablets/2in1s/etc) If you received this driver package as a zip file containing just sys, inf, cat, dll and this readme.txt file you need to do an "INF based" installation. 1. Plug the USB cable to the PC's USB host port and the other end to the USB connector. 2. Device will show up in "Device Manager" window as Unknown device. Right click on the device and select "update device driver" option. Follow the onscreen instructions answering the questions to instruct Windows NOT to search for drivers and that you will provide them yourself. Enter the path to the Drivers subdirectory of the root of this distribution (where the sys and inf driver files are located) and let Windows complete the installation process as usual for any network interface card. E.ii Windows Embedded handheld / Windows RT (ARM) and Windows 10 IOT (ARM and x86/x64 based) devices 1. Installation in Plug and Play capable version of Windows 8.x or Windows 10 (such as Windows RT tablets) is performed in the same was as explained in E.i section above. 2. Installation from a command prompt using devcon. The driver can be installed using the devcon install command in devices providing a local or remote administrative level command prompt and the devcon utility. After copying the driver files (inf, sys, and cat files) to the device run the following command from the folder holding the copied files: devcon install net7800-arm-n650f.inf "USB\VID_0424&PID_7800" 3. Other Installation procedures Note that installation procedures may vary across platforms. In particular non plug and play platforms are likely not to support INF based installations as detailed above and instead require either manual or programmatic driver file copying as well as addition of VID/PID, services and/or other assorted key entries into the registry which are platform specific and outside of the scope of these generic PnP installation instructions. E.iii INF based Package contents: \LAN7800-WDF-vx_x_x_x_Readme.txt - This file Windows Vista ------------- ndis60\x86\net7800-x86-n60f.inf - NDIS 6.0 driver installation file for x86 ndis60\x86\lan7800-x86-n60f.cat - NDIS 6.0 driver catalog file for x86 ndis60\x86\lan7800-x86-n60f.sys - NDIS 6.0 driver file for x86 ndis60\x86\WdfCoInstaller01009.dll - MSFT's Wdf Coinstaller v1.9 for x86 ndis60\x64\net7800-x64-n60f.inf - NDIS 6.0 driver installation file for x64 ndis60\x64\lan7800-x64-n60f.cat - NDIS 6.0 driver catalog file for x64 ndis60\x64\lan7800-x64-n60f.sys - NDIS 6.0 driver file for x64 ndis60\x64\WdfCoInstaller01009.dll - MSFT's Wdf Coinstaller v1.9 for x64 Windows 7 --------- ndis620\x86\net7800-x86-n620f.inf - NDIS 6.20 driver installation file for x86 ndis620\x86\lan7800-x86-n620f.cat - NDIS 6.20 driver catalog file for x86 ndis620\x86\lan7800-x86-n620f.sys - NDIS 6.20 driver file for x86 ndis620\x86\WdfCoInstaller01009.dll - MSFT's Wdf Coinstaller v1.9 for x86 ndis620\x64\net7800-x64-n620f.inf - NDIS 6.20 driver installation file for x64 ndis620\x64\lan7800-x64-n620f.cat - NDIS 6.20 driver catalog file for x64 ndis620\x64\lan7800-x64-n620f.sys - NDIS 6.20 driver file for x64 ndis620\x64\WdfCoInstaller01009.dll - MSFT's Wdf Coinstaller v1.9 for x64 Windows 8, Windows 8.1 ---------------------- ndis630\x86\net7800-x86-n630f.inf - NDIS 6.30 driver installation file for x86 ndis630\x86\lan7800-x86-n630f.cat - NDIS 6.30 driver catalog file for x86 ndis630\x86\lan7800-x86-n630f.sys - NDIS 6.30 driver file for x86 ndis630\x86\WdfCoInstaller01011.dll - MSFT's Wdf Coinstaller v1.11 for x86 ndis630\x64\net7800-x64-n630f.inf - NDIS 6.30 driver installation file for x64 ndis630\x64\lan7800-x64-n630f.cat - NDIS 6.30 driver catalog file for x64 ndis630\x64\lan7800-x64-n630f.sys - NDIS 6.30 driver file for x64 ndis630\x64\WdfCoInstaller01011.dll - MSFT's Wdf Coinstaller v1.11 for x64 Windows 8.x Embedded Handheld and Windows RT -------------------------------------------- ndis630\arm32\net7800-arm-n630f.inf - NDIS 6.30 driver installation file for ARM 32 bit ndis630\arm32\lan7800-arm-n630f.cat - NDIS 6.30 driver catalog file for ARM 32 bit ndis630\arm32\lan7800-arm-n630f.sys - NDIS 6.30 driver file for ARM 32 bit Windows 10 ---------- ndis650\x86\net7800-x86-n650f.inf - NDIS 6.50 driver installation file for x86 ndis650\x86\lan7800-x86-n650f.cat - NDIS 6.50 driver signed catalog file for x86 ndis650\x86\lan7800-x86-n650f.sys - NDIS 6.50 driver file for x86 ndis650\x64\net7800-x64-n650f.inf - NDIS 6.50 driver installation file for x64 ndis650\x64\lan7800-x64-n650f.cat - NDIS 6.50 driver signed catalog file for x64 ndis650\x64\lan7800-x64-n650f.sys - NDIS 6.50 driver file for x64 ndis650\arm64\net7800-arm64-n650f.inf - NDIS 6.50 driver installation file for arm64 ndis650\arm64\lan7800-arm64-n650f.cat - NDIS 6.50 driver signed catalog file for arm64 ndis650\arm64\lan7800-arm64-n650f.sys - NDIS 6.50 driver file for arm64 Windows 10 IoT -------------- ndis650\x86\net7800-x86-n650f.inf - NDIS 6.50 driver installation file for x86 ndis650\x86\lan7800-x86-n650f.cat - NDIS 6.50 driver signed catalog file for x86 ndis650\x86\lan7800-x86-n650f.sys - NDIS 6.50 driver file for x86 ndis650\x64\net7800-x64-n650f.inf - NDIS 6.50 driver installation file for x64 ndis650\x64\lan7800-x64-n650f.cat - NDIS 6.50 driver signed catalog file for x64 ndis650\x64\lan7800-x64-n650f.sys - NDIS 6.50 driver file for x64 ndis650\arm32\net7800-arm-n650f.inf - NDIS 6.50 driver installation file for ARM 32 bit ndis650\arm32\lan7800-arm-n650f.cat - NDIS 6.50 driver MCHP signed catalog file for ARM 32 bit ndis650\arm32\lan7800-arm-n650f.sys - NDIS 6.50 driver file for ARM 32 bit F. Driver Configurable Parameters --------------------------------- The following parameters are configurable thru the LAN7800 Advanced properties page: 1. Flow Control: Configure flow control advertised capabilities -Disabled -Tx Enabled (Generate only) -Rx Enabled (Respond only) -Rx & Tx Enabled (Generate and Respond) 2. Speed & Duplex: Selection of one of the following enumerated values -1.0 Gbps Full Duplex: Forces 1000FD Master without autonegotiating -10 Mbps Half Duplex: Forces 10HD without autonegotiating -10 Mbps Full Duplex: Forces 10FD without autonegotiating -100 Mbps Half Duplex: Forces 100HD without autonegotiating -100 Mbps Full Duplex: Forces 100FD without autonegotiating -Auto Negotiation: Advertises support for all combos of 10/100/1000 and HD/FD (except 1000HD) (default) 3. Network Address (optional): Allows overriding the MAC address of the device 4. Priority & VLAN: Enable or Disable support for VLAN tagging. - Priority & VLAN Disabled - Priority & VLAN Enabled (default) 5. VLANID: If "Priority & VLAN" are enabled this value selects the VLANID to insert on transmits and to filter upon on receives. 6. USBBandwidthMode: Selects how the driver uses USB bandwidth - Maximum Throughput: Uses as much USB bandwidth as it needs to maximize the LAN7800's device networking performance. (default) - Sharing Friendly: While providing adequate networking performance, in this mode the driver is conservative with USB bandwidth usage for a better experience of other devices with which it shares USB bandwidth. - Automatic: Sets itself to Sharing for High and Super Speed, and to Maximum Throughput for full speed. 7. Wake on pattern match: Enable or disable wake on pattern match (Ndis 6.20/Win7 or later) 8. Wake on magic packet: Enable or disable wake on magic packet (Ndis 6.20/Win7 or later) 9. NetDetach: Controls operation of the NetDetach feature (device is disconnected from the USB when Ethernet link is down, and reconnected to the USB when Ethernet link is up. (Except Ndis 6.30/Win8 or later) - Disabled: Always OFF. (default) - Enabled: Always ON. - Automatic: Enabled when system operating under battery power, disabled if system operating under AC power. 10. Jumbo Frame Size: Controls Jumbo Frame Size - min: 1514 Bytes (default) - max: 9230 Bytes 11. Device Sleep On Disconnect (*): Indicated whether putting the device in low power state when the link is down is supported. note that NDIS will not take advantage of this feature for USB devices. - Disabled - Enabled 12. Selective Suspend: Selective suspend capability (Ndis 6.30/Win8 or later) - Disabled: Enabled selective suspend (default) - Enabled: Disables selective suspend 13. Selective suspend Idle Timeout: NDIS considers the network adapter to be idle if it has been inactive for longer than selective suspend idle timeout. If idle device will be placed to suspend. This value specified in seconds (default 10). (Ndis 6.30/Win8 or later) 14. PM ARP Offload: Power Management Offload Capability - Disable: No PM ARP Offload - Enable: ARP protocol offload only while device is sleep (default) 15. PM NS Offload: Power Management Offload Capability - Disable: No PM NS Offload - Enable: NS protocol offload only while device is sleep (default) 16. Large Send Offload V1 (IPv4): Tx Large Send Offload Capability - Disable: Disable Large Send Offload support - Enable: Supports Large Send Offload version 1 (Only supports IPv4 and up to 64K byte LSO frame) (default) 17. Large Send Offload V2 (IPv4): Tx Large Send Offload Capability - Disable: Disable Large Send Offload support - Enable: Supports Large Send Offload version 2 (Only supports IPv4 and up to 1M byte LSO frame) (default) (Ndis 6.20/Win7 or later) 18. Large Send Offload V2 (IPv6): Tx Large Send Offload Capability - Disable: Disable Large Send Offload support - Enable: Supports Large Send Offload version 2 (supports IPv6 and up to 1M byte LSO frame) (default) (Ndis 6.20/Win7 or later) 19. IPv4 Checksum Offload: H/W Checksum Offload Capability Setting - Disable: Disable Tx/Rx IP Checksum Offload - Tx Only: Supports only IP Header Checksum Offload in Tx Path (Including IP Options) - Rx Only: Supports only IP Header Checksum Offload in Rx Path (Including IP Options) - Tx and Rx: Supports IP Header Checksum Offload in Tx/Rx Paths (Including IP Options) (default) 20. TCP Checksum Offload (IPv4/6): H/W Checksum Offload Capability Setting - Disable: Disable Tx/Rx TCP Checksum Offload - Tx Only: Supports only TCP Header Checksum Offload in Tx Path (Including TCP Options) - Rx Only: Supports only TCP Header Checksum Offload in Rx Path (Including TCP Options) - Tx and Rx: Supports TCP Header Checksum Offload in Tx/Rx Paths (Including TCP Options) (default) 21. UDP Checksum Offload (IPv4/6): H/W Checksum Offload Capability Setting - Disable: Disable Tx/Rx UDP Checksum Offload - Tx Only: Supports only UDP Header Checksum Offload in Tx Path - Rx Only: Supports only UDP Header Checksum Offload in Rx Path - Tx and Rx: Supports UDP Header Checksum Offload in Tx/Rx Paths (default) 22. Power Down Phy on Link Down: Controls whether the PHY is powered down when the Ethernet link is down. - Disabled: PHY remains active (default) - Enabled: PHY is placed in Low Power Mode 23. EEE: Enables EEE operation - Enabled - Disabled 24. Speed Duplex Autonegotiated Advertised Capabilities: Allows selection of the Advertised Capabilities (speed and duplex) Only applicable when the Speed Duplex property is set to "Auto Negotiation". This field resolves into an enumerartion value between 0 and 31. It is interpreted as the following bifield flags: 00001 - Advertises 10HD 00010 - Advertises 10FD 00100 - Advertises 100HD 01000 - Advertises 100FD 10000 - Advertises 1000 FD By default the value set is 1F for all capabilities advertised 25. USB3 LTM (optional): Controls LTM Behavior - Disabled: LTM support in the device is disabled regardless of the LTM values in the Superspeed Capabilities descriptor. - Enabled: LTM support in the device is enabled. However if the LTM values in the Superspeed Capabilities descriptor do not advertise it, the host will never do a SET_FEATURE.LTM_ENABLE and therefore LTM messages will not be sent by the device. - Hardware Controlled: LTM values in the the Superspeed Capabilities descriptor defines whether the feature is supported. The parameter is optional and if not present driver defaults to hardware controlled 26. USB2 LPM (optional): Controls LPM Behavior - Disabled: LPM support in the device is disabled regardless of the LPM flag in the USB 2.0 Extension Capability descriptor. - Enabled: LPM support in the device is enabled. However if the LPM flag in the USB 2.0 Extension Capability descriptor does not advertise it the host will not send LPM transactions. - Hardware Controlled: The LPM flag in the USB 2.0 Extension Capabilities descriptor defines whether the feature is supported. The parameter is optional and if not present driver defaults to hardware controlled 27. AutoMdix: Control whether the feature is enabled or disabled - OFF & Straight: Disabled. Device cabling behaves like legacy Ethernet device with no support for automdix (TPO = output, TPI = input). - OFF & Crossed: Disabled. Device has cabling reversed with respect to an Ethernet legacy device with no support for automdix. (TPO = input, TPI = output) - ON: Enabled 28. Gigabit Master slave Mode: Control which master - slave modes to advertise support for - Force Master Mode Advertises only Master - Force Slave Mode Advertises only Slave - Auto Detect Advertises both Master and Slave (default) G: Release Types ---------------- As marked in section A, this release contains drivers of three possible types: a. Production: The release has undergone full internal Microship testing and external Microsoft HLK certification testing ("MSFT Logo"). Drivers are all "Microsoft Hardware Quality Labs signed". There should be no Windows Security Pops for the user to accept during the driver installation. b. PreProduction: The release has undergone internal Microchip testing and deemed to be a Production Candidate but has not yet undergone external Microsoft HLK certification testing ("MSFT Logo"). Drivers for Windows 7 and Windows 8.x have been signed with Microchip certificates and drivers for Windows 10 have been "attestation" signed with Microsoft certificates (but not HLK/"Logo" certified). During installation there will likely be Windows security pop-ups for the user to accept driver software installation / trust software from Microchip Technologies c. Engineering: The release is produced to provide a quick turnaround fix and request confirmation of it for a previously reported problem. It has been either testsigned, or only signed with Microchip certificates and will most likely require testsigning to be enabled in the test system (as explained in section Bii) in order for the driver to start. There will also be Windows security pop-ups for the user to accept driver software and/or trust software from Microchip Technologies during installation. Note that even if the current software release you have received is not Production Type, the LAN743X hardware and software has been has been previously fully Microsoft HLK logo certified as of software release 3.8.4.0 for x86 and x64 and those versions of the x86 x64 and arm drivers have also been inboxed on Windows 10 v1803 (RS4). The certification reports for those releases can be downloaded from the following locations: For Win10 x86/x64 submission ID 1152921504627770282: https://partner.microsoft.com/en-us/dashboard/hardware/Driver/DownloadCertificationReport/30039700/14366420909814289/1152921504627770282 For Win8.x x86/x64 submission ID 1152921504627872218: https://partner.microsoft.com/en-us/dashboard/hardware/Driver/DownloadCertificationReport/30039700/14486789556232250/1152921504627872218 For Win7 x86/x64 submission ID 1152921504627846114: https://partner.microsoft.com/en-us/dashboard/hardware/Driver/DownloadCertificationReport/30039700/13677140740752094/1152921504627846114 H: Testing ---------- These production releases have been Microsoft Logo certified for Windows 7 and higher for x86 and amd64 Operating Systems architectures. It should be possible to install the same x86 and x64 driver binaries used in the Desktop/Laptop/Notebook/Tablet Computer that were mentioned in the previous paragraph, but in Windows 10 IoT for those architectures using devices such as MinnowBoard Max or Intel Joule. Microchip has NOT yet tested these drivers in those environments as of this release. For the ARM driver the following testing information is applicable a. Ndis 6.30 driver: This driver is derived from a LAN7500 driver that was originally developed for the Windows RT operating system (now discontinued) that was launched during the Windows 8 timeframe. It was a closed platform and official certification could only be done (and was) for the LAN7500 device. Therefore, while available certification tests were run and any pertinent issues observed were fixed in preceding driver versions, neither this driver or it's preceding versions has undergone formal official Microsoft Logo certification. In addition to informally running certification tests in a preceding version, this driver has also been tested as follows: - basic network connectivity on a Raspberry Pi 2 running Windows 10 IoT v1703 Preceding versions of this driver have been integrated successfully and thoroughly vetted by various OEMs in Production ready Windows Embedded Handheld 8 / 8.1 applications. b. Ndis 6.50 driver: This driver is derived from a LAN9500 driver that was originally developed for the Windows 10 IoT operating system that was launched during the Windows 10 timeframe. The LAN9500 driver has been part of the official Windows 10 IoT Raspberry Pi image distributed by Microsoft since the LAN9514 device is onboard the Raspberry Pi 3B or earlier. While no official certification program exists for IoT and (unlike Windows RT for the Ndis6.30 drivers) no framework is currently available to even be able to run the tests, the LAN9500 driver has undergone significant vetting by Microsoft and has been in use by millions of users with the Raspberry Pi. Additionally the LAN7800 driver has been provided to Microsoft for intergration into the preview builds of Windows 10 IoT for the Raspberry 3B+ since the LAN7515 device (which is software compatible with LAN7800) is onboard the Raspberry Pi 3B+. This LAN7800 driver has been tested as follows: - basic internet connectivity and file transfers on Raspberry Pi 3B and Raspberry Pi 3B+ devices. c. Common certified Source Code These drivers are compiled from the exact same source code used in the x86 and x64 Ndis 6.30 and Ndis 6.50 drivers that are officially MSFT WHQL certified for Windows 8/8.1/10 as per Section G. I: Known Issues --------------- On Windows 7, confirm that you have windows update KB3033929. If you have not updated from Windows Update since March 15, 2015, go to Windows Update and install KB3033929. The driver will not install experiencing signing problems otherwise. On Windows Vista confirm that you have KB3033929 & KB2763674. The driver will not install experiencing signing problems otherwise. On Windows 10, Engineering Releases will not install unless the system has had Test Signing enabled. See Section B, "Pre-installation Requirements" above for additional information. See Section B, "Pre-installation Requirements" above for additional information on all of these three issues. J. Release History ----------------- ** v18.12.14.0 ** 12/14/18 3.8.4.1 - Added preview build of ARM64 driver 3.8.4.0 - VS2017 build environment and make Win 10 x86 and x64 targets Universal. Fixed code analysis warnings - Reduce Advertised Ethernet Speed to 10 Mbps when operating in USB full speed. - Ensure EEE is not advertised by an external PHY when it is disabled. - Added features for 7801 Operation + autodetect unmanaged PHY operation (default to GigE speed in that case) + Support dfferent external clock options. - Added fix to MPCancelSendNetBufferLists - Bugzilla 33553 - Fixes for BSODs in some systems during sleep and Halt operations - Disable U2 at GigE speed (78W-151) - Preserve ETH_MAC_CR_AUTO_DUPLEX_ if set in EEPROM (Jira 78W-171) - Add indication of NDIS_STATUS_TASK_OFFLOAD_CURRENT_CONFIG - Jira 78W-153 - EnableFlowControlGuard as per Win10 RS3 inboxing requirements - Ensure statistics are ok / accessed atomically - Bugzilla 32545 - Return NDIS_STATUS_SEND_ABORTED in MPCancelSendNetBufferLists - Bugzilla 32867 ** v17.04.21.0 ** 04/21/17 - Resolved BSOD due to surprise removal during sleep. - Resolved LAN7801 Automatic Duplex Polarity (ADP) Error. - Disable EEE on KSZ9031 - Resolved MAC error after link changes (HD->FD->HD) while transmissions in progress - Changes to handling of surprise removal and reset. - Enhanced event log reporting. - Changes on the handling of reset triggering to limit exposure to synchronization problems between MiniportReset and MiniportPause/MiniportRestart while handling OID_GEN_LINK_PARAMETERS, as well as improve stability in other scenarios. - Fixed improper reporting of MediaConnectState in OID_GEN_LINK_STATE query. - Fix for 78W-135. Oscillation when in CS with link down and we wake due to link up change. We now neither restart negotiation on the SetPower OID if waking up from like up; nor do we do any media indication during PM changes. - 78W-40: Implement support to properly check and populate NDIS_RESTART_GENERAL_ATTRIBUTES if present during MiniportRestart. - Improve support for OID_GEN_TRANSMIT_QUEUE_LENGTH: We now return the number of packets that have been pended in MiniportSendNetBufferLists and have not yet been returned back using NdisMSendNetBufferListsComplete - Improvements to power consumption of the Ethernet PHY when not in use and device suspends. - General robustness and stability improvements ** v16.01.20.0 ** 01/20/16 - Replaced Win10x64 v3.5.1.0 driver with v3.5.2.0 which just completed AOAC certification. ** v16.01.15.0 ** 01/15/16 - Rebuild Ndis 6.0 (Vista) packages and sign them with SHA1 standard code signing certificate instead of SHA2 EV code signing certificate which is not fully supported for kernel drivers under Vista - Ndis 6.0 (Vista) driver binaries are unchanged in functionality from v16.01.06.0, though the binaries are different (sys EV signatures stripped). - Ndis 6.30 (Windows 8.x) x64 driver binaries are unchanged in functionality from v16.01.06.0, though binaries have been replaced with a package that supports both Windows 8.0 and 8.1 (16.01.09.0 package supported only Win 8.1 and would fail installing in Win 8.0) - All other driver binaries remain unchanged from v16.01.06.0s ** v16.01.09.0 ** 01/09/16 - Use Caphyon Advanced Installer for proper Windows 10 OS detection. - Driver binaries remain unchanged from v16.01.06.0 ** v16.01.06.0 ** 01/06/16 3.5.2.0 - Fixes for 78W-119. Issue could cause wake packets not being indicated on receive or early Tx replies to wake packets not transmitted. This mostly affected maintaining connectivity throughout connected standby in AOAC systems. - Robustness improvements 3.5.1.0 - Improve Ndis versioning support so that later Ndis driver only report use of the portion of the structure they use during OID set, and only return structures of the size they filled up during OID queries. This future proofs drivers. - Fix 78W-125: HLK test DF-HyperVisor Code Integrity Readiness fails on Win10: + Use NonPagedPoolNx instead of NonPagedPool. + Use MdlMappingNoExecute in the call to MmGetSystemAddressForMdlSafe - Fix bug where a pending OID query could have attempted to copy more data than the available space in the information buffer - Fix bug in offload OIDs setting where we could set internal state based on some parameters of the structure and yet fail the OID because other portions of the structure where invalid - Fix bug where we used the inccorect offset to advanced to a next pattern (if present) in a set pattern OID. Verify Next pattern fits within InformationBuffer before adding it. - Fix bug where we used the inccorect offset to advanced to a next pattern (if present) in a set PM protocol offload OID. Verify Next PM protocol offload fits within InformationBuffer before adding. - Fix bug where if there was a intermittent surprise related status returned but the device remains connected without the driver unloading, internal driver state would be as if device remained disconnected idling waiting for an unload that would not occur. - Correct some failure codes in OID handling to match the documentation recommendations - Change event log message on Reset failure to be informative rather than error if a surprise remove occured and prevent repetitions. - Several other stability, performance and internal diagnostic improvements. ** v15.11.13.0 ** 11/13/15 - Initial Release