Getting Started Application on PIC32CM JH01 Curiosity Nano+ Touch Evaluation Kit

Download


Description:

This application demonstrates an LED (LED0) toggle on timeout basis and print the LED toggling rate on the serial terminal. The periodicity of the timeout will change from 500 milliseconds to one second, two seconds, four seconds and back to 500 milliseconds every time you press the switch SW0 on the PIC32CM JH01 Curiosity Nano+ Touch Evaluation Kit.

Modules/Technology Used:

Hardware Used:

Software/Tools Used:

This project has been verified to work with the following versions of software tools:

Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/pic32cm_jh01_cnano
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version. Alternatively, Click Here. - Any Serial Terminal application like Tera Term/PuTTY terminal application.

Because Microchip regularly update tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project doesn’t seem to work and version incompatibility is suspected, It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature

Setup:

Programming hex file:

The pre-built hex file can be programmed by following the below steps.

Steps to program the hex file

Programming/Debugging Application Project:

Running the Demo:

Comments:

Revision: