6.1. Source Tree Structure¶
The MCAF is organized into several subdirectories.
When used with motorBench™ Development Suite, these are generated under the MPLAB® X
project directory under motorBench/generated_code.
- Most modules are located under the top-level directory.
halcontains the Hardware Abstraction Layerparameterscontains header files with configurable parameters.librarycontains library files for the Motor Control Libraryaux-filescontains auxiliary files that aren’t C code, such as report files generated by motorBench™ Development Suite.
Information on particular source code files is organized by module name,
in the index under “modules”. (Module name is just
the base name of the file, ignoring the file extension and, if present,
the trailing _types: for example,
commutation.c, commutation.h, and commutation_types.h
are all part of the commutation module.)