3.2. Naming Conventions¶
The MCAF uses the following naming conventions:
A prefix is used for all functions and types, so that these functions are less likely to conflict with user-defined code. The major prefixes are
MC_— Motor Control LibraryMCAF_— Motor Control Application FrameworkHAL_— Hardware Abstraction LayerBSP_— Board Support Package
Functions use a prefix and UpperCamelCase, i.e. one or more words with each word capitalized including the first one. These generally fall into one of two types:
Actions: <noun-phrase> <action>
MCAF_CoastdownTimerReset() MCAF_PllEstimatorInit()
Getters: <noun-phrase> <adjective-phrase> or <noun-phrase> <property>
MCAF_OperatingModeNormal() MCAF_StartupHasCompleted()
Types are defined in all capital letters with underscores between words:
typedef struct { int16_t d; int16_t q; } MC_DQ_T;
Enum constants are defined in all capital letters with underscores between words. Enum constants in the same type should have a common prefix that is specific to that type, for instance the
MADC_prefix in this example:typedef enum tagMCAF_ADC_SELECT { MADC_VDC = 0, MADC_POTENTIOMETER = 1 } MCAF_ADC_SELECT;
Variables and struct/union members are declared in lowerCamelCase, i.e. one or more words with each word capitalized except the first one:
int16_t thetaElectrical; int16_t omegaElectrical; MC_SINCOS_T sincos; MCAF_MOTOR_DATA *pmotor; uint16_t subsampleCounter;
- Underscore characters in variable names and structure members are discouraged.
- Prefixes are not used in global variables, because the number of global variables is minimal. In addition, their names may be changed by customers without impact to the MCAF, since the framework’s modules do not access them directly.
The MCAF uses the standard C types defined in
<stdint.h>and<stdbool.h>, such asint16_t,uint16_t,int32_t, andbool, to denote integers of specific bit widths. Earlier application note code included lines such as the following:// use of implementation-dependent types int count = 0; short qVqRef; unsigned long Startup_Ramp = 0; // attempt to define specific type aliases typedef unsigned short WORD; typedef signed int SFRAC16; typedef unsigned char BYTE; typedef unsigned char bool; #define False 0 #define True 1
These have since been converted to use
<stdint.h>and<stdbool.h>.
3.2.1. Additional Naming Guidelines¶
- The MCAF sometimes uses variable names which are symbolic in nature
(for example
thetaoromegaoriq) because these have specific meanings in motor control theory. - The camelCase convention in symbolic names should not change the
capitalization of subscripts, for example we use
idqandialphabetarather thaniDQoriAlphaBeta. - In general, variable names should start off with a general description of the
quantity they represent and should be followed by more specific qualifiers.
This allows related sibling variables or structure members to be
alphabetically adjacent, and allows readers to narrow down the topic of
interest as they read from left to right. Thus
iMaximum,iMinimum,vMaximum,vMinimumis better thanmaximumCurrent,minimumCurrent,minimumVoltage,maximumVoltage.