3.8. Treatment of Numerical Algorithms¶
3.8.1. Numerical Representation¶
The MCAF at present utilizes only fixed-point (and not floating-point)
computation. The majority of state variables and parameters
are represented as Q15 fixed-point stored in a signed 16-bit number (int16_t),
with a handful of 32-bit values (usually in integrators or filter state)
and a few unsigned Q15 16-bit values. Some gains use other scaling factors
like Q11 or variable shifts, where appropriate.
3.8.1.1. Normalization Factors¶
The primary normalization factors in MCAF v1.0 are shown below. (Please note that v1.0 supports only the dsPICDEM® MCLV‑2 Development Board.)
| quantity | factor (in general) | factor used with MCLV2 |
|---|---|---|
| Voltage (PI output) | Nominal bus voltage divided by \(\sqrt{3}\) | 13.86V |
| DC link voltage | Maximum ADC input for DC link | 52.8V |
| Current | Twice the maximum phase current, which allows room for gain calibration and avoids overflow in Park and Clarke transforms, at the cost of reduced resolution on the low end. | 8.87V |
| Velocity | Not yet determined for general usage | 30000RPM electrical |
3.8.2. Constants in Code¶
Constants found in code are sometimes considered “magic numbers” if the reason for choosing their value is unclear. We try to avoid this situation in the Motor Control Application Framework.
Constants used in the Motor Control Application Framework generally fall into one of five categories.
Automatically calculated values: In the
parameters/directory, in header files or in C run-time initialization functions –- these are calculated by motorBench™ Development Suite during the autotuning and code generation steps. We do not recommend changing these values manually. Where they are fixed-point integer constants, a comment generally accompanies them indicating the floating-point equivalent and the corresponding engineering value, along with quantization accuracy, for example:#define KIP 8696 // Q15( 0.26538) = +414.67629 mV/A = +414.65940 mV/A + 0.0041% #define KII 643 // Q15( 0.01962) = +613.24024 V/A/s = +613.20687 V/A/s + 0.0054%
Among many other tasks, we are working on improving the documentation within our code to clarify how these constants are calculated, or at least what factors they depend on. In some cases the calculations are proprietary formulas within motorBench™ Development Suite.
Part of the Hardware Abstraction Layer: In the
hal/directory. These are intended to be consistent with, and eventually replaced by, automatically-generated output from MCC.“Obvious” values in the C source files outside the
parameters/directory, including some examples shown below. In these cases, hiding them behind an abstracted symbolic constant obscures rather than clarifies their usage. If you see an example where they seem inappropriate, please bring them to our attention, and we will consider alternatives.- 0
- +1 or -1 as a sign/direction value
- maximum representative values like 0xFFFF or 0x7FFF
- shift counts, e.g.
>> 16when converting fromint32_ttoint16_t, or>> Nwhere multiplying a QN fixed-point number, and the value of N is clarified in code comments - array indices for unrolled loops
MCAF_DelayNanoseconds(500);(used to output a “short pulse” as mentioned in an accompanying comment)
Hand-calculated constants with accompanying comment explaining how they were derived — these are uncommon; if any are unclear, please bring these to our attention.
Legacy code constants — if for some reason you notice a constant in code that does not fall into one of the above categories, it is probably an oversight, in which case please bring it to our attention.