| txcwdata | array of random data, which is permanently sent out. It is recommended, that the array has a length of 127, which is the maximum possible framesize, which can be stored in the SRAM of the radio transceiver. If the synchronisation header (SHR: 0,0,0,0,0xA7) is included in this array, and PRBS mode is selected, the continuous transmission can be recognized as a loop of individual 802.15.4-2003 frames without interframe spacing. | |
| txcwmode | Select the mode of the continuous transmission
|
trxstat = trx_bit_read(SR_TRX_STATUS); ASSERT(trxstat==TRX_OFF); trx_bit_write(SR_TX_AUTO_CRC_ON, 0); trx_frame_write(len(txcwdata), txcwdata); trx_reg_write(0x36, 15); trx_reg_write(0x3d, txcwmode); trx_pinset_tst(1); trx_bit_write(SR_TRX_CMD, CMD_PLL_ON); delay_us(180); /* TRX_IRQ_PLL_LOCK occurs within this period */ trx_bit_write(SR_TRX_CMD, CMD_TX_START);
trx_pinset_tst(0); trx_pinset_reset(0); delay_us(6); trx_pinset_reset(1);
1.5.2