| State | Comment |
|---|---|
| SLEEP | see section Transitions to/from State SLEEP [15] |
| TRX_OFF | see section Transitions to State TRX_OFF [08] |
| PLL_ON | see section Transitions to State PLL_ON [09] |
| RX_ON | see section Transitions to State RX_ON [06] |
| RX_ON_NOCLK | see section Transitions to State RX_ON [06] while the pin TRX_PIN_SLP_TR is HIGH. |
| RX_AACK_ON | see section Transitions to State RX_AACK_ON [22] |
| RX_AACK_ON_NOCLK | see section Transitions to State RX_AACK_ON [22] while the pin TRX_PIN_SLP_TR is HIGH |
| TX_ARET_ON | see section Transitions to State TX_ARET_ON [25] |
| State | Comment |
|---|---|
| P_ON | This state is reached only during power up of the radio transceiver. If this state is left once, it will be reached only with the next power up. |
| BUSY_TX | This state is reached during a frame transmission in basic operating mode. |
| BUSY_RX | This state is reached during a frame reception in basic operating mode. |
| BUSY_TX_ARET | This state is reached during a frame transmission in TX_ARET mode. |
| BUSY_RX_AACK | This state is reached during a frame reception in RX_AACK mode. |
| BUSY_RX_AACK_NOCLK | This state is reached during frame reception in RX_AACK mode, while TRX_PIN_SLP_TR is HIGH. |
| STATE_TRANSITION_IN_PROGRESS | This state means, that an internal transaction of the radio transceiver is in progress and the status needs to be read another time, in order to obtain a valid result. |
| State Group | States |
|---|---|
| [READY] | any state except P_ON |
| [ACTIVE] | any state except P_ON and SLEEP |
| [AWAKE] | any state except SLEEP |
| [PLL_ACTIVE] | RX_ON, PLL_ON, TX_ARET_ON, RX_AACK_ON |
| [PLL_BASIC] | PLL_ON, RX_ON |
| [RX_BASIC] | RX_ON, BUSY_RX |
| [NOT_RX_AACK] | TRX_OFF, RX_ON, PLL_ON, TX_ARET_ON, BUSY_TX, BUSY_RX, BUSY_TX_ARET |
| [FTN] | TRX_OFF, PLL_ON |
| [TX_BUSY] | BUSY_TX, BUSY_TX_ARET |
| [RX_BUSY] | BUSY_RX, (BUSY_RX_AACK_MATCH) |
| [BUSY] | [TX_BUSY], [RX_BUSY] |
| [BUSY_BASIC] | BUSY_TX, BUSY_RX |
| [CMD] | TRX_OFF, RX_ON, PLL_ON, TX_ARET_ON, RX_AACK_ON (all states which can be reached by writing to the SR_TRX_CMD sub register) |
| (BUSY_DEFAULT) | This is a pseudo state. It is a symbol for the default fallback state for any of the busy states. BUSY_TX => PLL_ON / BUSY_RX => RX_ON / BUSY_TX_ARET => TX_ARET_ON / BUSY_RX_AACK => RX_AACK_ON |
| (BUSY_RX_AACK_MATCH) | pseudo state for BUSY_RX_AACK / BUSY_RX_AACK_NOCLK when the received frame does match the address filter and has an valid FCS. In this case the interrupt TRX_IRQ_TRX_END is generated.. |
| (BUSY_RX_AACK_NOMATCH) | pseudo state for BUSY_RX_AACK / BUSY_RX_AACK_NOCLK when the received frame does not match the address filter or/and has an invalid FCS. In this case no interrupt TRX_IRQ_TRX_END is generated. |
1.5.2