Introduction

This section describes the hardware interface (SPI, GPIO, IRQ), the basic interface functions (read/write, interrupt) and the main states of the radio transceiver. Details about the radio transceiver parameters are given in the AT86RF230 data sheet. This section also introduces MSCs, which are used for the representation of the use cases.


Generated on Fri Sep 28 14:07:33 2007 for SWPM AT86RF230 Rev. B by  doxygen 1.5.2