This section describes how the states of radio transceiver are changed. An overview of all states and state groups can be found in section
Grouping Radio Transceiver States. All states and allowed state changes are illustrated in
figure 5-8 (Extended Operating Mode State Diagram) of the AT86RF212 datasheet.
- Note:
- At the end of all state change sequences, the sub register SR_TRX_STATUS is read and compared against an expected value. This operation is shown only for the purpose of illustration of the state change and it is not an operational part of the state change process itself.