This section describes, how the filter and PLL calibration algorithms are started manually. The filter calibration algorithm is done automatically, whenever a state change from the states
P_ON or
SLEEP to the state
TRX_OFF occurs or a transceiver reset (see
TRX_RESET) is performed. The PLL is calibrated during a state change from state
TRX_OFF to any of the
[PLL_ACTIVE] states. If these state changes do not occur during the normal operation of the radio transceiver frequently every 5 minutes, it is recommended to start it manually within this period. If the operating conditions of the radio transceiver (temperature, voltage) are nearly constant, the recalibration period may be increased.
Use Cases:
- Code example
The calibration of the PLL center frequency (CF) and delay calibration unit (DCU) is initiated with the folowing sequence.
- Note:
- This calibration sequence can also be started in the state TX_ARET_ON.
- Code example
-