The battery monitor conccept is described in more detail in
section 7.6 (Battery Monitor) of the AT86RF212 datasheet.
The interrupt
TRX_IRQ_BAT_LOW occurs, when the supply voltage drops below the adjusted threshold value. In this case a special handling of the interrupt is needed, which is described in
PHY_SIGNAL_BAT_LOW (see also section
Battery Monitor and
section 7.6 (Battery Monitor) of the AT86RF212 datasheet).
- Code example
-