#include "usb_user_configuration.h"
Go to the source code of this file.
Data Structures | |
| struct | S_UsbRequest |
| Usb Request. More... | |
| struct | S_usb_device_descriptor |
| Usb Device Descriptor. More... | |
| struct | S_usb_configuration_descriptor |
| Usb Configuration Descriptor. More... | |
| struct | S_usb_interface_descriptor |
| Usb Interface Descriptor. More... | |
| struct | S_usb_endpoint_descriptor |
| Usb Endpoint Descriptor. More... | |
| struct | S_usb_device_qualifier_descriptor |
| Usb Device Qualifier Descriptor. More... | |
| struct | S_usb_language_id |
| Usb Language Descriptor. More... | |
| struct | S_usb_hid_descriptor |
| Usb HID Descriptor. More... | |
Defines | |
| #define | Usb_str_28(a1, a2, a3, a4, a5, a6, a7, a8, a9, a10, a11, a12, a13, a14, a15, a16, a17, a18, a19, a20, a21, a22, a23, a24, a25, a26, a27, a28) |
| #define | GET_STATUS 0x00 |
| Standard Requests. | |
| #define | GET_DEVICE 0x01 |
| #define | CLEAR_FEATURE 0x01 |
| see FEATURES below | |
| #define | GET_STRING 0x03 |
| #define | SET_FEATURE 0x03 |
| see FEATURES below | |
| #define | SET_ADDRESS 0x05 |
| #define | GET_DESCRIPTOR 0x06 |
| #define | SET_DESCRIPTOR 0x07 |
| #define | GET_CONFIGURATION 0x08 |
| #define | SET_CONFIGURATION 0x09 |
| #define | GET_INTERFACE 0x0A |
| #define | SET_INTERFACE 0x0B |
| #define | SYNCH_FRAME 0x0C |
| #define | GET_DEVICE_DESCRIPTOR 1 |
| #define | GET_CONFIGURATION_DESCRIPTOR 4 |
| #define | REQUEST_DEVICE_STATUS 0x80 |
| #define | REQUEST_INTERFACE_STATUS 0x81 |
| #define | REQUEST_ENDPOINT_STATUS 0x82 |
| #define | ZERO_TYPE 0x00 |
| #define | INTERFACE_TYPE 0x01 |
| #define | ENDPOINT_TYPE 0x02 |
| #define | DEVICE_DESCRIPTOR 0x01 |
| Descriptor Types. | |
| #define | CONFIGURATION_DESCRIPTOR 0x02 |
| #define | STRING_DESCRIPTOR 0x03 |
| #define | INTERFACE_DESCRIPTOR 0x04 |
| #define | ENDPOINT_DESCRIPTOR 0x05 |
| #define | DEVICE_QUALIFIER_DESCRIPTOR 0x06 |
| #define | OTHER_SPEED_CONFIGURATION_DESCRIPTOR 0x07 |
| #define | FEATURE_DEVICE_REMOTE_WAKEUP 0x01 |
| Standard Features. | |
| #define | FEATURE_ENDPOINT_HALT 0x00 |
| #define | TEST_J 0x01 |
| #define | TEST_K 0x02 |
| #define | TEST_SEO_NAK 0x03 |
| #define | TEST_PACKET 0x04 |
| #define | TEST_FORCE_ENABLE 0x05 |
| #define | BUS_POWERED 0 |
| Device Status. | |
| #define | SELF_POWERED 1 |
| #define | ATTACHED 0 |
| Device State. | |
| #define | POWERED 1 |
| #define | DEFAULT 2 |
| #define | ADDRESSED 3 |
| #define | CONFIGURED 4 |
| #define | SUSPENDED 5 |
| #define | USB_CONFIG_ATTRIBUTES_RESERVED 0x80 |
| #define | USB_CONFIG_BUSPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x00) |
| #define | USB_CONFIG_SELFPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x40) |
| #define | USB_CONFIG_REMOTEWAKEUP (USB_CONFIG_ATTRIBUTES_RESERVED | 0x20) |
| #define | HID 0x21 |
| #define | REPORT 0x22 |
Functions | |
| void | usb_enum_var_init (void) |
| usb_enum_variable_init. | |
| void | usb_process_request (void) |
| usb_process_request. | |
Use of this program is subject to Atmel's End User License Agreement. Please read file license.txt for copyright notice.
This file contains the USB endpoint 0 management routines corresponding to the standard enumeration process (refer to chapter 9 of the USB specification. This file calls routines of the usb_user_enum.c file for non-standard request management. The enumeration parameters (descriptor tables) are contained in the usb_user_configuration.c file.
Definition in file usb_enum.h.
|
|
Value:
Definition at line 31 of file usb_enum.h. |
|
|
Standard Requests.
Definition at line 41 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 42 of file usb_enum.h. |
|
|
see FEATURES below
Definition at line 43 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 44 of file usb_enum.h. |
|
|
see FEATURES below
Definition at line 45 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 46 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 47 of file usb_enum.h. Referenced by usb_process_request(), and usb_user_read_request(). |
|
|
Definition at line 48 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 49 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 50 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 51 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 52 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 53 of file usb_enum.h. Referenced by usb_process_request(). |
|
|
Definition at line 55 of file usb_enum.h. |
|
|
Definition at line 56 of file usb_enum.h. |
|
|
Definition at line 58 of file usb_enum.h. Referenced by usb_get_status(). |
|
|
Definition at line 59 of file usb_enum.h. Referenced by usb_get_status(). |
|
|
Definition at line 60 of file usb_enum.h. Referenced by usb_get_status(). |
|
|
Definition at line 61 of file usb_enum.h. Referenced by usb_clear_feature(). |
|
|
Definition at line 62 of file usb_enum.h. Referenced by usb_clear_feature(), and usb_set_feature(). |
|
|
Definition at line 63 of file usb_enum.h. Referenced by usb_clear_feature(), and usb_set_feature(). |
|
|
Descriptor Types.
Definition at line 67 of file usb_enum.h. Referenced by usb_get_descriptor(). |
|
|
Definition at line 68 of file usb_enum.h. Referenced by usb_get_descriptor(). |
|
|
Definition at line 69 of file usb_enum.h. Referenced by usb_user_get_descriptor(). |
|
|
Definition at line 70 of file usb_enum.h. |
|
|
Definition at line 71 of file usb_enum.h. |
|
|
Definition at line 72 of file usb_enum.h. |
|
|
Definition at line 73 of file usb_enum.h. |
|
|
Standard Features.
Definition at line 77 of file usb_enum.h. |
|
|
Definition at line 78 of file usb_enum.h. Referenced by usb_clear_feature(), and usb_set_feature(). |
|
|
Definition at line 80 of file usb_enum.h. |
|
|
Definition at line 81 of file usb_enum.h. |
|
|
Definition at line 82 of file usb_enum.h. |
|
|
Definition at line 83 of file usb_enum.h. |
|
|
Definition at line 84 of file usb_enum.h. |
|
|
Device Status.
Definition at line 88 of file usb_enum.h. |
|
|
Definition at line 89 of file usb_enum.h. |
|
|
Device State.
Definition at line 93 of file usb_enum.h. |
|
|
Definition at line 94 of file usb_enum.h. |
|
|
Definition at line 95 of file usb_enum.h. |
|
|
Definition at line 96 of file usb_enum.h. |
|
|
Definition at line 97 of file usb_enum.h. |
|
|
Definition at line 98 of file usb_enum.h. |
|
|
Definition at line 100 of file usb_enum.h. |
|
|
Definition at line 101 of file usb_enum.h. |
|
|
Definition at line 102 of file usb_enum.h. |
|
|
Definition at line 103 of file usb_enum.h. |
|
|
Definition at line 107 of file usb_enum.h. |
|
|
Definition at line 108 of file usb_enum.h. |
|
|
usb_enum_variable_init. This function initializes the main usb variables:
< USB is not connected < Default configuration number is 0 Definition at line 78 of file usb_enum.c. References endpoint_status, ep_num, FALSE, NB_ENDPOINTS, rx_bank, U8, usb_configuration_nb, and usb_connected. Referenced by usb_interrupt().
|
|
|
usb_process_request. This function reads the SETUP request sent to the default control endpoint and calls the appropriate function. When exiting of the usb_read_request function, the device is ready to manage the next request.
< un-supported request => call to user read request Definition at line 115 of file usb_enum.c. References bmRequestType, CLEAR_FEATURE, EP_CONTROL, FALSE, GET_CONFIGURATION, GET_DESCRIPTOR, GET_INTERFACE, GET_STATUS, SET_ADDRESS, SET_CONFIGURATION, SET_DESCRIPTOR, SET_FEATURE, SET_INTERFACE, SYNCH_FRAME, U8, Usb_ack_receive_setup, usb_clear_feature(), Usb_enable_stall_handshake, usb_get_configuration(), usb_get_descriptor(), usb_get_status(), Usb_read_byte, Usb_select_endpoint, usb_set_address(), usb_set_configuration(), usb_set_feature(), and usb_user_read_request(). Referenced by usb_task().
|
1.3.7