Main Page | Alphabetical List | Data Structures | File List | Data Fields | Globals | Related Pages

scheduler.h File Reference

Copyright (c) 2004 This file is the definition of the scheduler. More...

Go to the source code of this file.

Defines

#define Wait_semaphore(a)   while(!(a)) (a) = FALSE
 _____ I N C L U D E S ____________________________________________________

#define TASK_DUMMY   0x00
 _____ M A C R O S ________________________________________________________ Definition of Task ID.

#define TASK_0   0x01
#define TASK_1   0x02
#define TASK_2   0x04
#define TASK_3   0x08
#define TASK_4   0x10
#define TASK_5   0x20
#define TASK_6   0x40
#define TASK_7   0x80
#define ALL_TASK   (TASK_0|TASK_1|TASK_2|TASK_3|TASK_4|TASK_5|TASK_6|TASK_7)
#define SCHEDULER_CUSTOM   0
 End Task ID ----- Scheduler Types -----.

#define SCHEDULER_TIMED   1
#define SCHEDULER_TASK   2
#define SCHEDULER_FREE   3
#define Scheduler_call_next_task()
#define Scheduler_new_schedule()
#define Scheduler_call_next_init()

Functions

void scheduler_init (void)
 _____ D E C L A R A T I O N ______________________________________________

void scheduler_tasks (void)
 Task execution scheduler.

void scheduler (void)
 Init & run the scheduler.

void scheduler_empty_fct (void)
 Do nothing Avoid uncalled segment warning if the empty function is not used.


Variables

bit scheduler_tick_flag
 _____ D E F I N I T I O N ________________________________________________


Detailed Description

Copyright (c) 2004 This file is the definition of the scheduler.

Please read file license.txt for copyright notice.

This file contains the scheduler definition and the task function to be executed by the scheduler NOTE: SCHEDULER_TICK & FPER are defined in config.h

Version:
1.11 (c5131-usb-generic-1_2_0)

Todo:

Bug:

Definition in file scheduler.h.


Define Documentation

#define Wait_semaphore  )     while(!(a)) (a) = FALSE
 

_____ I N C L U D E S ____________________________________________________

Definition at line 29 of file scheduler.h.

#define TASK_DUMMY   0x00
 

_____ M A C R O S ________________________________________________________ Definition of Task ID.

This ID is used to properly send the event to a specific task. Mind, it will be possible to send an event to many task by TASK_1 | TASK_0. The name of the define can be changed by another define. That customization should be done in the file mail_evt.h

Definition at line 38 of file scheduler.h.

#define TASK_0   0x01
 

Definition at line 39 of file scheduler.h.

#define TASK_1   0x02
 

Definition at line 40 of file scheduler.h.

#define TASK_2   0x04
 

Definition at line 41 of file scheduler.h.

#define TASK_3   0x08
 

Definition at line 42 of file scheduler.h.

#define TASK_4   0x10
 

Definition at line 43 of file scheduler.h.

#define TASK_5   0x20
 

Definition at line 44 of file scheduler.h.

#define TASK_6   0x40
 

Definition at line 45 of file scheduler.h.

#define TASK_7   0x80
 

Definition at line 46 of file scheduler.h.

#define ALL_TASK   (TASK_0|TASK_1|TASK_2|TASK_3|TASK_4|TASK_5|TASK_6|TASK_7)
 

Definition at line 49 of file scheduler.h.

#define SCHEDULER_CUSTOM   0
 

End Task ID ----- Scheduler Types -----.

Definition at line 53 of file scheduler.h.

#define SCHEDULER_TIMED   1
 

Definition at line 54 of file scheduler.h.

#define SCHEDULER_TASK   2
 

Definition at line 55 of file scheduler.h.

#define SCHEDULER_FREE   3
 

Definition at line 56 of file scheduler.h.

 
#define Scheduler_call_next_task  ) 
 

Definition at line 177 of file scheduler.h.

Referenced by scheduler_tasks().

 
#define Scheduler_new_schedule  ) 
 

Definition at line 180 of file scheduler.h.

Referenced by scheduler_tasks().

 
#define Scheduler_call_next_init  ) 
 

Definition at line 183 of file scheduler.h.

Referenced by scheduler_init().


Function Documentation

void scheduler_init void   ) 
 

_____ D E C L A R A T I O N ______________________________________________

Task_x_init() and Task_x_fct() are defined in config.h

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 49 of file scheduler.c.

References Scheduler_call_next_init, Scheduler_task_1_init, Scheduler_task_2_init, and Scheduler_time_init().

Referenced by scheduler().

00050 { 00051 #ifdef Scheduler_time_init 00052 Scheduler_time_init(); 00053 #endif 00054 #ifdef TOKEN_MODE 00055 token = TOKEN_FREE; 00056 #endif 00057 #ifdef Scheduler_task_1_init 00058 Scheduler_task_1_init(); 00059 Scheduler_call_next_init(); 00060 #endif 00061 #ifdef Scheduler_task_2_init 00062 Scheduler_task_2_init(); 00063 Scheduler_call_next_init(); 00064 #endif 00065 #ifdef Scheduler_task_3_init 00066 Scheduler_task_3_init(); 00067 Scheduler_call_next_init(); 00068 #endif 00069 #ifdef Scheduler_task_4_init 00070 Scheduler_task_4_init(); 00071 Scheduler_call_next_init(); 00072 #endif 00073 #ifdef Scheduler_task_5_init 00074 Scheduler_task_5_init(); 00075 Scheduler_call_next_init(); 00076 #endif 00077 #ifdef Scheduler_task_6_init 00078 Scheduler_task_6_init(); 00079 Scheduler_call_next_init(); 00080 #endif 00081 #ifdef Scheduler_task_7_init 00082 Scheduler_task_7_init(); 00083 Scheduler_call_next_init(); 00084 #endif 00085 #ifdef Scheduler_task_8_init 00086 Scheduler_task_8_init(); 00087 Scheduler_call_next_init(); 00088 #endif 00089 #ifdef Scheduler_task_9_init 00090 Scheduler_task_9_init(); 00091 Scheduler_call_next_init(); 00092 #endif 00093 #ifdef Scheduler_task_10_init 00094 Scheduler_task_10_init(); 00095 Scheduler_call_next_init(); 00096 #endif 00097 #ifdef Scheduler_task_11_init 00098 Scheduler_task_11_init(); 00099 Scheduler_call_next_init(); 00100 #endif 00101 Scheduler_reset_tick_flag(); 00102 }

void scheduler_tasks void   ) 
 

Task execution scheduler.

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 110 of file scheduler.c.

References Scheduler_call_next_task, scheduler_empty_fct(), Scheduler_new_schedule, Scheduler_task_1, and Scheduler_task_2.

00111 { 00112 // To avoid uncalled segment warning if the empty function is not used 00113 scheduler_empty_fct(); 00114 00115 for(;;) 00116 { 00117 Scheduler_new_schedule(); 00118 #ifdef Scheduler_task_1 00119 Scheduler_task_1(); 00120 Scheduler_call_next_task(); 00121 #endif 00122 #ifdef Scheduler_task_2 00123 Scheduler_task_2(); 00124 Scheduler_call_next_task(); 00125 #endif 00126 #ifdef Scheduler_task_3 00127 Scheduler_task_3(); 00128 Scheduler_call_next_task(); 00129 #endif 00130 #ifdef Scheduler_task_4 00131 Scheduler_task_4(); 00132 Scheduler_call_next_task(); 00133 #endif 00134 #ifdef Scheduler_task_5 00135 Scheduler_task_5(); 00136 Scheduler_call_next_task(); 00137 #endif 00138 #ifdef Scheduler_task_6 00139 Scheduler_task_6(); 00140 Scheduler_call_next_task(); 00141 #endif 00142 #ifdef Scheduler_task_7 00143 Scheduler_task_7(); 00144 Scheduler_call_next_task(); 00145 #endif 00146 #ifdef Scheduler_task_8 00147 Scheduler_task_8(); 00148 Scheduler_call_next_task(); 00149 #endif 00150 #ifdef Scheduler_task_9 00151 Scheduler_task_9(); 00152 Scheduler_call_next_task(); 00153 #endif 00154 #ifdef Scheduler_task_10 00155 Scheduler_task_10(); 00156 Scheduler_call_next_task(); 00157 #endif 00158 #ifdef Scheduler_task_11 00159 Scheduler_task_11(); 00160 Scheduler_call_next_task(); 00161 #endif 00162 } 00163 }

void scheduler void   ) 
 

Init & run the scheduler.

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 171 of file scheduler.c.

References scheduler_init(), and scheduler_tasks().

00172 { 00173 scheduler_init(); 00174 scheduler_tasks(); 00175 }

void scheduler_empty_fct void   ) 
 

Do nothing Avoid uncalled segment warning if the empty function is not used.

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 185 of file scheduler.c.

00186 { 00187 }


Variable Documentation

bit scheduler_tick_flag
 

_____ D E F I N I T I O N ________________________________________________

Definition at line 143 of file scheduler.h.


Generated on Mon Apr 10 17:23:31 2006 for Atmel by doxygen 1.3.7