Main Page | Alphabetical List | Data Structures | File List | Data Fields | Globals | Related Pages

scheduler.c File Reference

Copyright (c) 2004 This file contains the scheduler routines. More...

#include "config.h"
#include "conf/conf_scheduler.h"
#include "scheduler.h"

Go to the source code of this file.

Defines

#define _SCHEDULER_C_
 _____ I N C L U D E S ____________________________________________________


Functions

void scheduler_init (void)
 _____ D E C L A R A T I O N ______________________________________________

void scheduler_tasks (void)
 Task execution scheduler.

void scheduler (void)
 Init & run the scheduler.

void scheduler_empty_fct (void)
 Do nothing Avoid uncalled segment warning if the empty function is not used.


Detailed Description

Copyright (c) 2004 This file contains the scheduler routines.

Please read file license.txt for copyright notice.

Configuration:

Version:
1.11 (c5131-usb-generic-1_2_0)

Todo:
Bug:

Definition in file scheduler.c.


Define Documentation

#define _SCHEDULER_C_
 

_____ I N C L U D E S ____________________________________________________

Definition at line 18 of file scheduler.c.


Function Documentation

void scheduler_init void   ) 
 

_____ D E C L A R A T I O N ______________________________________________

Task_x_init() and Task_x_fct() are defined in config.h

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 49 of file scheduler.c.

References Scheduler_call_next_init, Scheduler_task_1_init, Scheduler_task_2_init, and Scheduler_time_init().

Referenced by scheduler().

00050 { 00051 #ifdef Scheduler_time_init 00052 Scheduler_time_init(); 00053 #endif 00054 #ifdef TOKEN_MODE 00055 token = TOKEN_FREE; 00056 #endif 00057 #ifdef Scheduler_task_1_init 00058 Scheduler_task_1_init(); 00059 Scheduler_call_next_init(); 00060 #endif 00061 #ifdef Scheduler_task_2_init 00062 Scheduler_task_2_init(); 00063 Scheduler_call_next_init(); 00064 #endif 00065 #ifdef Scheduler_task_3_init 00066 Scheduler_task_3_init(); 00067 Scheduler_call_next_init(); 00068 #endif 00069 #ifdef Scheduler_task_4_init 00070 Scheduler_task_4_init(); 00071 Scheduler_call_next_init(); 00072 #endif 00073 #ifdef Scheduler_task_5_init 00074 Scheduler_task_5_init(); 00075 Scheduler_call_next_init(); 00076 #endif 00077 #ifdef Scheduler_task_6_init 00078 Scheduler_task_6_init(); 00079 Scheduler_call_next_init(); 00080 #endif 00081 #ifdef Scheduler_task_7_init 00082 Scheduler_task_7_init(); 00083 Scheduler_call_next_init(); 00084 #endif 00085 #ifdef Scheduler_task_8_init 00086 Scheduler_task_8_init(); 00087 Scheduler_call_next_init(); 00088 #endif 00089 #ifdef Scheduler_task_9_init 00090 Scheduler_task_9_init(); 00091 Scheduler_call_next_init(); 00092 #endif 00093 #ifdef Scheduler_task_10_init 00094 Scheduler_task_10_init(); 00095 Scheduler_call_next_init(); 00096 #endif 00097 #ifdef Scheduler_task_11_init 00098 Scheduler_task_11_init(); 00099 Scheduler_call_next_init(); 00100 #endif 00101 Scheduler_reset_tick_flag(); 00102 }

void scheduler_tasks void   ) 
 

Task execution scheduler.

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 110 of file scheduler.c.

Referenced by scheduler().

00111 { 00112 // To avoid uncalled segment warning if the empty function is not used 00113 scheduler_empty_fct(); 00114 00115 for(;;) 00116 { 00117 Scheduler_new_schedule(); 00118 #ifdef Scheduler_task_1 00119 Scheduler_task_1(); 00120 Scheduler_call_next_task(); 00121 #endif 00122 #ifdef Scheduler_task_2 00123 Scheduler_task_2(); 00124 Scheduler_call_next_task(); 00125 #endif 00126 #ifdef Scheduler_task_3 00127 Scheduler_task_3(); 00128 Scheduler_call_next_task(); 00129 #endif 00130 #ifdef Scheduler_task_4 00131 Scheduler_task_4(); 00132 Scheduler_call_next_task(); 00133 #endif 00134 #ifdef Scheduler_task_5 00135 Scheduler_task_5(); 00136 Scheduler_call_next_task(); 00137 #endif 00138 #ifdef Scheduler_task_6 00139 Scheduler_task_6(); 00140 Scheduler_call_next_task(); 00141 #endif 00142 #ifdef Scheduler_task_7 00143 Scheduler_task_7(); 00144 Scheduler_call_next_task(); 00145 #endif 00146 #ifdef Scheduler_task_8 00147 Scheduler_task_8(); 00148 Scheduler_call_next_task(); 00149 #endif 00150 #ifdef Scheduler_task_9 00151 Scheduler_task_9(); 00152 Scheduler_call_next_task(); 00153 #endif 00154 #ifdef Scheduler_task_10 00155 Scheduler_task_10(); 00156 Scheduler_call_next_task(); 00157 #endif 00158 #ifdef Scheduler_task_11 00159 Scheduler_task_11(); 00160 Scheduler_call_next_task(); 00161 #endif 00162 } 00163 }

void scheduler void   ) 
 

Init & run the scheduler.

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 171 of file scheduler.c.

00172 { 00173 scheduler_init(); 00174 scheduler_tasks(); 00175 }

void scheduler_empty_fct void   ) 
 

Do nothing Avoid uncalled segment warning if the empty function is not used.

Warning:
Code:XX bytes (function code length)
Parameters:
:none 
Returns:
:none

Definition at line 185 of file scheduler.c.

Referenced by scheduler_tasks().

00186 { 00187 }


Generated on Mon Apr 10 17:23:31 2006 for Atmel by doxygen 1.3.7