#include "config.h"
#include "config_motor.h"
#include "mc_interface.h"
#include "mc_control.h"
#include "mc_drv.h"
Include dependency graph for mc_interface.c:

Go to the source code of this file.
Functions | |
| void | mc_motor_init () |
| use to init programm | |
| void | mc_ramp_up_init (void) |
| void | mci_backward (void) |
| void | mci_forward (void) |
| U16 | mci_get_measured_current (void) |
| Get the current measured in the motor. | |
| U8 | mci_get_measured_speed (void) |
| Measured of speed. | |
| U8 | mci_get_motor_speed (void) |
| U8 | mci_get_potentiometer_value (void) |
| Get the potentiometer value. | |
| Bool | mci_motor_is_running (void) |
| get the motor state | |
| void | mci_run (void) |
| mci_run starts the motor with predefined parameter | |
| void | mci_set_motor_direction (U8 direction) |
| void | mci_set_motor_speed (U8 speed) |
| void | mci_set_speed (U16 speed) |
| void | mci_stop (void) |
| void | mci_store_measured_current (U16 current) |
| Set the variable 'mc_measured_current' for initialization. | |
| void | mci_store_measured_speed (U8 measured_speed) |
| set Measured of speed (for initialization) | |
| void | mci_store_potentiometer_value (U8 potentiometer) |
| Set the 'mc_potentiometer_value' variable with the potentiometer value. | |
Variables | |
| U8 | mci_cmd_speed = 0 |
| User Input parameter to set motor speed. | |
| Bool | mci_direction = CW |
| User Input parameter to set motor direction. | |
| U32 | mci_measured_current = 0 |
| Motor Input parameter to get the motor current. | |
| U8 | mci_measured_speed = 0 |
| Motor Input parameter to get the motor speed. | |
| U8 | mci_potentiometer_value = 0 |
| Motor Input to set the motor speed. | |
| Bool | mci_run_stop = STOP |
| User Input parameter to launch or stop the motor. | |
| void mc_motor_init | ( | void | ) |
use to init programm
| @post | configuration of hardware and sotware |
Definition at line 48 of file mc_interface.c.
References mc_init_HW(), mc_init_SW(), mci_stop(), and mci_store_measured_speed().
Referenced by main(), and mci_run().
00049 { 00050 mc_init_HW(); 00051 mc_init_SW(); 00052 00053 mci_stop(); 00054 mci_store_measured_speed(0); 00055 }
Here is the call graph for this function:

Here is the caller graph for this function:

| void mc_ramp_up_init | ( | void | ) |
Definition at line 35 of file main.c.
References g_speed_monitor_period, HS_001, new_position, ramp_counter, ramp_up, tick_divider_min, and TRUE.
Referenced by main(), and mci_run().
00036 { 00037 ramp_counter = 0; 00038 tick_divider_min = 50; 00039 new_position = HS_001; 00040 ramp_up = TRUE; 00041 g_speed_monitor_period = 0; 00042 }
Here is the caller graph for this function:

| void mci_backward | ( | void | ) |
Definition at line 103 of file mc_interface.c.
References CCW, and mci_direction.
Referenced by ushell_task().
00104 { 00105 mci_direction = CCW; 00106 }
Here is the caller graph for this function:

| void mci_forward | ( | void | ) |
Definition at line 93 of file mc_interface.c.
References CW, and mci_direction.
Referenced by ushell_task().
00094 { 00095 mci_direction = CW; 00096 }
Here is the caller graph for this function:

| U16 mci_get_measured_current | ( | void | ) |
Get the current measured in the motor.
Definition at line 144 of file mc_interface.c.
References mci_measured_current.
Referenced by mc_control_current(), and ushell_task().
00145 { 00146 /* U16 value_to_return; 00147 value_to_return = mci_measured_current>>6; 00148 if (value_to_return > 994) 00149 { 00150 value_to_return = value_to_return - 994; 00151 } 00152 else 00153 { 00154 value_to_return = 994 - value_to_return; 00155 } 00156 return value_to_return;*/ 00157 return mci_measured_current; 00158 }
Here is the caller graph for this function:

| U8 mci_get_measured_speed | ( | void | ) |
Measured of speed.
Definition at line 134 of file mc_interface.c.
References mci_measured_speed.
Referenced by main(), mc_control_speed(), and ushell_task().
00135 { 00136 return mci_measured_speed; 00137 }
Here is the caller graph for this function:

| U8 mci_get_motor_speed | ( | void | ) |
Definition at line 72 of file mc_interface.c.
References mci_cmd_speed.
Referenced by mc_regulation_loop(), and mc_switch_commutation().
00073 { 00074 return mci_cmd_speed; 00075 }
Here is the caller graph for this function:

| U8 mci_get_potentiometer_value | ( | void | ) |
Get the potentiometer value.
Definition at line 175 of file mc_interface.c.
References mci_potentiometer_value.
Referenced by mc_regulation_loop().
00176 { 00177 return mci_potentiometer_value; 00178 }
Here is the caller graph for this function:

| Bool mci_motor_is_running | ( | void | ) |
get the motor state
| @pre | initialization HW and SW |
Definition at line 36 of file mc_interface.c.
References mci_run_stop.
Referenced by mc_switch_commutation().
00037 { 00038 return mci_run_stop; 00039 }
Here is the caller graph for this function:

| void mci_run | ( | void | ) |
mci_run starts the motor with predefined parameter
| @pre | initialization HW and SW |
Definition at line 196 of file mc_interface.c.
References DUTY_RAMP_UP, mc_motor_init(), mc_ramp_up_init(), mc_regulation_loop(), mc_set_Open_Loop(), mci_run_stop, mci_set_motor_speed(), PSC_Run(), and RUN.
Referenced by ushell_task().
00197 { 00198 mc_motor_init(); // launch initialization of the motor 00199 mci_run_stop = RUN; 00200 mci_set_motor_speed(DUTY_RAMP_UP); /* set a speed for the ramp-up */ 00201 mc_set_Open_Loop(); /* set the regulation type */ 00202 mc_regulation_loop(); /* execute the regulation one time */ 00203 mc_ramp_up_init(); 00204 PSC_Run(); 00205 }
Here is the call graph for this function:

Here is the caller graph for this function:

| void mci_set_motor_direction | ( | U8 | direction | ) |
Definition at line 82 of file mc_interface.c.
References mci_direction.
Referenced by mc_control_position().
00083 { 00084 // if ((mci_direction == CW) || (mci_direction == CCW)) mci_direction = direction; 00085 mci_direction = direction; 00086 }
Here is the caller graph for this function:

| void mci_set_motor_speed | ( | U8 | speed | ) |
Definition at line 62 of file mc_interface.c.
References mci_cmd_speed.
Referenced by main(), mci_run(), and mci_set_speed().
00063 { 00064 mci_cmd_speed = speed; 00065 }
Here is the caller graph for this function:

| void mci_set_speed | ( | U16 | speed | ) |
Definition at line 214 of file mc_interface.c.
References mci_set_motor_speed().
Referenced by ushell_task().
00215 { 00216 mci_set_motor_speed((U8)speed); 00217 }
Here is the call graph for this function:

Here is the caller graph for this function:

| void mci_stop | ( | void | ) |
Definition at line 207 of file mc_interface.c.
References mci_run_stop, PSC_Stop(), and STOP.
Referenced by mc_motor_init(), and ushell_task().
00208 { 00209 PSC_Stop(); 00210 mci_run_stop = STOP; 00211 }
Here is the call graph for this function:

Here is the caller graph for this function:

| void mci_store_measured_current | ( | U16 | current | ) |
Set the variable 'mc_measured_current' for initialization.
Definition at line 165 of file mc_interface.c.
References mci_measured_current.
Referenced by ADC_EOC().
00166 { 00167 mci_measured_current = ((63*mci_measured_current)+(64*current))>>6; 00168 }
Here is the caller graph for this function:

| void mci_store_measured_speed | ( | U8 | measured_speed | ) |
set Measured of speed (for initialization)
Definition at line 123 of file mc_interface.c.
References mci_measured_speed.
Referenced by mc_estimation_speed(), mc_motor_init(), and ovfl_timer().
00124 { 00125 mci_measured_speed = measured_speed; 00126 }
Here is the caller graph for this function:

| void mci_store_potentiometer_value | ( | U8 | potentiometer | ) |
Set the 'mc_potentiometer_value' variable with the potentiometer value.
Definition at line 185 of file mc_interface.c.
References mci_potentiometer_value.
Referenced by ADC_EOC().
00186 { 00187 mci_potentiometer_value = potentiometer; 00188 }
Here is the caller graph for this function:

| U8 mci_cmd_speed = 0 |
User Input parameter to set motor speed.
Definition at line 23 of file mc_interface.c.
Referenced by mci_get_motor_speed(), and mci_set_motor_speed().
| Bool mci_direction = CW |
User Input parameter to set motor direction.
Definition at line 21 of file mc_interface.c.
Referenced by mci_backward(), mci_forward(), mci_set_motor_direction(), and ushell_task().
Motor Input parameter to get the motor current.
Definition at line 26 of file mc_interface.c.
Referenced by mci_get_measured_current(), and mci_store_measured_current().
| U8 mci_measured_speed = 0 |
Motor Input parameter to get the motor speed.
Definition at line 25 of file mc_interface.c.
Referenced by mci_get_measured_speed(), and mci_store_measured_speed().
Motor Input to set the motor speed.
Definition at line 27 of file mc_interface.c.
Referenced by mci_get_potentiometer_value(), and mci_store_potentiometer_value().
| Bool mci_run_stop = STOP |
User Input parameter to launch or stop the motor.
Definition at line 22 of file mc_interface.c.
Referenced by main(), mci_motor_is_running(), mci_run(), mci_stop(), and ushell_task().
1.4.7