Comparator 0 Macros
[Comparators Macros]

Collaboration diagram for Comparator 0 Macros:


Detailed Description

Low level macros that permit the use of the Comparator 0 of the product.


Modules

 Turn on the Comparator 0
 Turn on the Comparator 0.
 Comparator 0 Interrupt Enable
 Enable or Disable Comparator 0 Interrupt.
 Comparator 0 Gain Configuration
 Configure the value of the gain of the Comparator 0

Comparator 0 interrupt on output toggle.

 Comparator 0 Negative Input Selection
 Select the Negative Input signal of the Comparator 0.
 Turn off the Comparator 0
 Turn off the Comparator 0.


Generated on Wed Jul 12 16:55:29 2006 for Atmel BLDC Sensorless on ATAVRMC100 by  doxygen 1.4.7