compiler.h File Reference

This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

union  Union16
union  Union32

Defines

#define __IOMACRO_H
#define _MEM_TYPE_BIT_
#define _MEM_TYPE_FAST_
#define _MEM_TYPE_MEDFAST_
#define _MEM_TYPE_MEDSLOW_
#define _MEM_TYPE_SLOW_
#define bit_is_clear(PORT, POSITION)   ((PORT & (1<<POSITION)) == 0 )
#define bit_is_set(PORT, POSITION)   ((PORT & (1<<POSITION)) != 0 )
#define CLR   0
#define CLR_BIT_X(addrx, mask)   (*addrx = (*addrx & ~mask))
#define DISABLE   0
#define DISABLED   0
#define ENABLE   1
#define ENABLED   1
#define FAIL   1
#define FALSE   (0==1)
#define HIGH(U16)   ((Uchar)(U16>>8))
#define htonl(a)   Le32(a)
#define htons(a)   Le16(a)
#define IN_X(addrx)   (*addrx)
#define INTEL_ALIGNMENT   LITTLE_ENDIAN
#define KO   0
#define Le16(b)
#define Le32(b)
#define LITTLE_ENDIAN
#define Long_call(addr)   ((*(void (_ConstType_*)(void))(addr))())
#define LOW(U16)   ((Uchar)U16)
#define LSB(u16)   (((U8* )&u16)[0])
#define LSB0(u32)   MSB3(u32)
#define LSB1(u32)   MSB2(u32)
#define LSB2(u32)   MSB1(u32)
#define LSB3(u32)   MSB0(u32)
#define LSW(u32)   (((U16*)&u32)[0])
#define MOTOROLA_ALIGNMENT   BIG_ENDIAN
#define MSB(u16)   (((U8* )&u16)[1])
#define MSB0(u32)   (((U8* )&u32)[3])
#define MSB1(u32)   (((U8* )&u32)[2])
#define MSB2(u32)   (((U8* )&u32)[1])
#define MSB3(u32)   (((U8* )&u32)[0])
#define MSW(u32)   (((U16*)&u32)[1])
#define ntohl(a)   htonl(a)
#define ntohs(a)   htons(a)
#define NULL   0
#define OFF   0
#define OK   1
#define ON   1
#define OUT_X(addrx, value)   (*addrx = value)
#define PASS   0
#define SET   1
#define SET_BIT_X(addrx, mask)   (*addrx = (*addrx | mask))
#define SET_SFR_BIT(sfr_reg, bit_pos, bit_val)   { sfr_reg &= ~(1<<(bit_pos)); sfr_reg |= ((bit_val)<<(bit_pos));}
#define SFR_B(_NAME, _ADDR)
#define SFR_B2(_NAME1, _NAME2, _ADDR)
#define SFR_B_EXT(_NAME, _ADDR)
#define SFR_W(_NAME, _ADDR)
#define SFR_W_EXT(_NAME, _ADDR)
#define TID_GUARD(proc)   ((__TID__ & 0x7FF0) != ((90 << 8) | ((proc) << 4)))
#define TRUE   (1==1)
#define TST_BIT_X(addrx, mask)   (*addrx & mask)

Typedefs

typedef unsigned char Bool
typedef unsigned char Byte
typedef unsigned long int DWord
typedef float Float16
typedef int Int16
typedef long int Int32
typedef char Int8
typedef char p_uart_ptchar
typedef char r_uart_ptchar
typedef short S16
typedef long S32
typedef signed char S8
typedef U8 Status
typedef Bool Status_bool
typedef unsigned short U16
typedef unsigned long U32
typedef unsigned char U8
typedef unsigned char Uchar
typedef unsigned int Uint16
typedef unsigned long int Uint32
typedef unsigned char Uint8
typedef unsigned int Word


Define Documentation

#define __IOMACRO_H

Definition at line 296 of file compiler.h.

#define _MEM_TYPE_BIT_

Definition at line 54 of file compiler.h.

#define _MEM_TYPE_FAST_

Definition at line 55 of file compiler.h.

#define _MEM_TYPE_MEDFAST_

Definition at line 56 of file compiler.h.

#define _MEM_TYPE_MEDSLOW_

Definition at line 57 of file compiler.h.

#define _MEM_TYPE_SLOW_

Definition at line 58 of file compiler.h.

#define bit_is_clear ( PORT,
POSITION   )     ((PORT & (1<<POSITION)) == 0 )

Definition at line 278 of file compiler.h.

#define bit_is_set ( PORT,
POSITION   )     ((PORT & (1<<POSITION)) != 0 )

Definition at line 288 of file compiler.h.

#define CLR   0

Definition at line 228 of file compiler.h.

#define CLR_BIT_X ( addrx,
mask   )     (*addrx = (*addrx & ~mask))

Definition at line 237 of file compiler.h.

#define DISABLE   0

Definition at line 218 of file compiler.h.

#define DISABLED   0

Definition at line 217 of file compiler.h.

#define ENABLE   1

Definition at line 215 of file compiler.h.

#define ENABLED   1

Definition at line 216 of file compiler.h.

#define FAIL   1

Definition at line 43 of file compiler.h.

#define FALSE   (0==1)

Definition at line 219 of file compiler.h.

Referenced by main(), mc_hall_a(), mystrncmp(), parse_cmd(), timer1_periodic_interrupt(), ushell_task(), and ushell_task_init().

#define HIGH ( U16   )     ((Uchar)(U16>>8))

Definition at line 234 of file compiler.h.

Referenced by PSC0_Init(), PSC1_Init(), and PSC2_Init().

#define htonl (  )     Le32(a)

Definition at line 204 of file compiler.h.

#define htons (  )     Le16(a)

Definition at line 202 of file compiler.h.

#define IN_X ( addrx   )     (*addrx)

Definition at line 239 of file compiler.h.

#define INTEL_ALIGNMENT   LITTLE_ENDIAN

Definition at line 153 of file compiler.h.

#define KO   0

Definition at line 222 of file compiler.h.

Referenced by mc_estimation_speed().

#define Le16 (  ) 

Value:

(  ((U16)(     (b) &   0xFF) << 8)  \
   |  (     ((U16)(b) & 0xFF00) >> 8)  \
   )

Definition at line 186 of file compiler.h.

#define Le32 (  ) 

Value:

(  ((U32)(     (b) &       0xFF) << 24)  \
   |  ((U32)((U16)(b) &     0xFF00) <<  8)  \
   |  (     ((U32)(b) &   0xFF0000) >>  8)  \
   |  (     ((U32)(b) & 0xFF000000) >> 24)  \
   )

Definition at line 190 of file compiler.h.

#define LITTLE_ENDIAN

Definition at line 23 of file compiler.h.

#define Long_call ( addr   )     ((*(void (_ConstType_*)(void))(addr))())

Definition at line 256 of file compiler.h.

#define LOW ( U16   )     ((Uchar)U16)

Definition at line 233 of file compiler.h.

Referenced by PSC0_Init(), PSC1_Init(), and PSC2_Init().

#define LSB ( u16   )     (((U8* )&u16)[0])

Definition at line 159 of file compiler.h.

Referenced by parse_cmd().

#define LSB0 ( u32   )     MSB3(u32)

Definition at line 166 of file compiler.h.

#define LSB1 ( u32   )     MSB2(u32)

Definition at line 167 of file compiler.h.

#define LSB2 ( u32   )     MSB1(u32)

Definition at line 168 of file compiler.h.

#define LSB3 ( u32   )     MSB0(u32)

Definition at line 169 of file compiler.h.

#define LSW ( u32   )     (((U16*)&u32)[0])

Definition at line 161 of file compiler.h.

#define MOTOROLA_ALIGNMENT   BIG_ENDIAN

Definition at line 154 of file compiler.h.

#define MSB ( u16   )     (((U8* )&u16)[1])

Definition at line 158 of file compiler.h.

Referenced by parse_cmd().

#define MSB0 ( u32   )     (((U8* )&u32)[3])

Definition at line 162 of file compiler.h.

#define MSB1 ( u32   )     (((U8* )&u32)[2])

Definition at line 163 of file compiler.h.

#define MSB2 ( u32   )     (((U8* )&u32)[1])

Definition at line 164 of file compiler.h.

#define MSB3 ( u32   )     (((U8* )&u32)[0])

Definition at line 165 of file compiler.h.

#define MSW ( u32   )     (((U16*)&u32)[1])

Definition at line 160 of file compiler.h.

#define ntohl (  )     htonl(a)

Definition at line 205 of file compiler.h.

#define ntohs (  )     htons(a)

Definition at line 203 of file compiler.h.

#define NULL   0

Definition at line 226 of file compiler.h.

#define OFF   0

Definition at line 224 of file compiler.h.

#define OK   1

Definition at line 223 of file compiler.h.

Referenced by mc_estimation_speed().

#define ON   1

Definition at line 225 of file compiler.h.

#define OUT_X ( addrx,
value   )     (*addrx = value)

Definition at line 238 of file compiler.h.

#define PASS   0

Definition at line 42 of file compiler.h.

#define SET   1

Definition at line 229 of file compiler.h.

#define SET_BIT_X ( addrx,
mask   )     (*addrx = (*addrx | mask))

Definition at line 236 of file compiler.h.

#define SET_SFR_BIT ( sfr_reg,
bit_pos,
bit_val   )     { sfr_reg &= ~(1<<(bit_pos)); sfr_reg |= ((bit_val)<<(bit_pos));}

Definition at line 268 of file compiler.h.

#define SFR_B ( _NAME,
_ADDR   ) 

Value:

SFR_B_BITS(_NAME, _ADDR, \
                                    Bit0,Bit1,Bit2,Bit3,Bit4,Bit5,Bit6,Bit7)

Definition at line 409 of file compiler.h.

#define SFR_B2 ( _NAME1,
_NAME2,
_ADDR   ) 

Value:

SFR_B2_BITS(_NAME1, _NAME2, _ADDR, \
                                    Bit0,Bit1,Bit2,Bit3,Bit4,Bit5,Bit6,Bit7)

Definition at line 411 of file compiler.h.

#define SFR_B_EXT ( _NAME,
_ADDR   ) 

Value:

SFR_B_BITS_EXT(_NAME, _ADDR, \
                                    Bit0,Bit1,Bit2,Bit3,Bit4,Bit5,Bit6,Bit7)

Definition at line 413 of file compiler.h.

#define SFR_W ( _NAME,
_ADDR   ) 

Value:

SFR_W_BITS(_NAME, _ADDR, \
                                    Bit0,Bit1,Bit2,Bit3,Bit4,Bit5,Bit6,Bit7, \
                                    Bit8,Bit9,Bit10,Bit11,Bit12,Bit13,Bit14,Bit15)

Definition at line 416 of file compiler.h.

#define SFR_W_EXT ( _NAME,
_ADDR   ) 

Value:

SFR_W_BITS_EXT(_NAME, _ADDR, \
                                    Bit0,Bit1,Bit2,Bit3,Bit4,Bit5,Bit6,Bit7, \
                                    Bit8,Bit9,Bit10,Bit11,Bit12,Bit13,Bit14,Bit15)

Definition at line 420 of file compiler.h.

#define TID_GUARD ( proc   )     ((__TID__ & 0x7FF0) != ((90 << 8) | ((proc) << 4)))

Definition at line 298 of file compiler.h.

#define TRUE   (1==1)

Definition at line 220 of file compiler.h.

Referenced by main(), mc_hall_a(), mc_hall_b(), mc_hall_c(), mc_ramp_up_init(), mystrncmp(), parse_cmd(), timer1_periodic_interrupt(), and uart_init().

#define TST_BIT_X ( addrx,
mask   )     (*addrx & mask)

Definition at line 235 of file compiler.h.


Typedef Documentation

typedef unsigned char Bool

Definition at line 37 of file compiler.h.

typedef unsigned char Byte

Definition at line 72 of file compiler.h.

typedef unsigned long int DWord

Definition at line 74 of file compiler.h.

typedef float Float16

Definition at line 26 of file compiler.h.

typedef int Int16

Definition at line 69 of file compiler.h.

typedef long int Int32

Definition at line 70 of file compiler.h.

typedef char Int8

Definition at line 68 of file compiler.h.

typedef char p_uart_ptchar

Definition at line 100 of file compiler.h.

typedef char r_uart_ptchar

Definition at line 101 of file compiler.h.

typedef short S16

Definition at line 32 of file compiler.h.

typedef long S32

Definition at line 33 of file compiler.h.

typedef signed char S8

Definition at line 31 of file compiler.h.

typedef U8 Status

Definition at line 40 of file compiler.h.

typedef Bool Status_bool

Definition at line 41 of file compiler.h.

typedef unsigned short U16

Definition at line 29 of file compiler.h.

typedef unsigned long U32

Definition at line 30 of file compiler.h.

typedef unsigned char U8

Definition at line 28 of file compiler.h.

typedef unsigned char Uchar

Definition at line 61 of file compiler.h.

typedef unsigned int Uint16

Definition at line 65 of file compiler.h.

typedef unsigned long int Uint32

Definition at line 66 of file compiler.h.

typedef unsigned char Uint8

Definition at line 64 of file compiler.h.

typedef unsigned int Word

Definition at line 73 of file compiler.h.


Generated on Wed Jul 12 16:55:12 2006 for Atmel BLDC Sensorless on ATAVRMC100 by  doxygen 1.4.7