AVR443 Sensor-based control of three phase Brushless DC Motor Documentation
This documents the software for application note AVR443. This is an example of how to use an ATmega48/88/168 to control a three phase BLDC motor with hall sensors.
This software was compiled with IAR Embedded Workbench, 4.12A. Details about compiler settings can be found in "related pages".
The code is targeting ATmega48/88/168. The concepts used can also be applied when using other AVRs, though some rewriting of the code will be required.
For more info about Atmel AVR visit http://www.atmel.com/products/AVR/
For application notes visit http://www.atmel.com/dyn/products/app_notes.asp?family_id=607
Support mail: avr@atmel.com
Generated on Tue Sep 18 08:53:11 2007 for AVR443 Sensor-based control of three phase Brushless DC Motor by
1.4.7