Go to the source code of this file.
Defines | |
| #define | ABORT_CHAR CTRL_C |
| #define | BKSPACE_CHAR 0x08 |
| #define | CMD_BACKWARD 0x05 |
| #define | CMD_FORWARD 0x04 |
| #define | CMD_GET_ID 0x07 |
| #define | CMD_GET_STATUS0 0x08 |
| #define | CMD_GET_STATUS1 0x09 |
| #define | CMD_HELP 0x01 |
| #define | CMD_NONE 0x00 |
| #define | CMD_RUN 0x02 |
| #define | CMD_SET_SPEED 0x06 |
| #define | CMD_STOP 0x03 |
| #define | CR 0x0D |
| #define | CTRL_C 0x03 |
| #define | CTRL_Q 0x11 |
| #define | LF 0x0A |
| #define | MSG_ER_CMD_NOT_FOUND "Unknown Command" |
| #define | MSG_HELP "\r\ru : run\r\st : stop\r\fw : forward\r\bw : backward\r\ss : set speed\r\gi : get id\" |
| #define | MSG_PROMPT "\r>" |
| #define | MSG_WELCOME "\rATMEL Motor Control Interface" |
| #define | QUIT_APPEND CTRL_Q |
| #define | STR_BACKWARD "bw" |
| #define | STR_FORWARD "fw" |
| #define | STR_GET_ID "gi" |
| #define | STR_GET_STATUS0 "g0" |
| #define | STR_GET_STATUS1 "g1" |
| #define | STR_HELP "help" |
| #define | STR_RUN "ru" |
| #define | STR_SET_SPEED "ss" |
| #define | STR_STOP "st" |
Functions | |
| void | build_cmd (void) |
| void | parse_cmd (void) |
| void | ushell_task (void) |
| void | ushell_task_init (void) |
| #define ABORT_CHAR CTRL_C |
| #define BKSPACE_CHAR 0x08 |
| #define CMD_BACKWARD 0x05 |
| #define CMD_FORWARD 0x04 |
| #define CMD_GET_ID 0x07 |
| #define CMD_GET_STATUS0 0x08 |
| #define CMD_GET_STATUS1 0x09 |
| #define CMD_HELP 0x01 |
| #define CMD_NONE 0x00 |
| #define CMD_RUN 0x02 |
| #define CMD_SET_SPEED 0x06 |
| #define CMD_STOP 0x03 |
| #define CR 0x0D |
| #define CTRL_C 0x03 |
Definition at line 38 of file ushell_task.h.
| #define CTRL_Q 0x11 |
Definition at line 37 of file ushell_task.h.
| #define LF 0x0A |
Definition at line 36 of file ushell_task.h.
| #define MSG_ER_CMD_NOT_FOUND "Unknown Command" |
Definition at line 57 of file ushell_task.h.
| #define MSG_HELP "\r\ru : run\r\st : stop\r\fw : forward\r\bw : backward\r\ss : set speed\r\gi : get id\" |
Definition at line 58 of file ushell_task.h.
| #define MSG_PROMPT "\r>" |
Definition at line 55 of file ushell_task.h.
| #define MSG_WELCOME "\rATMEL Motor Control Interface" |
Definition at line 56 of file ushell_task.h.
| #define QUIT_APPEND CTRL_Q |
Definition at line 41 of file ushell_task.h.
| #define STR_BACKWARD "bw" |
Definition at line 48 of file ushell_task.h.
| #define STR_FORWARD "fw" |
Definition at line 47 of file ushell_task.h.
| #define STR_GET_ID "gi" |
Definition at line 50 of file ushell_task.h.
| #define STR_GET_STATUS0 "g0" |
Definition at line 51 of file ushell_task.h.
| #define STR_GET_STATUS1 "g1" |
Definition at line 52 of file ushell_task.h.
| #define STR_HELP "help" |
Definition at line 46 of file ushell_task.h.
| #define STR_RUN "ru" |
Definition at line 44 of file ushell_task.h.
| #define STR_SET_SPEED "ss" |
Definition at line 49 of file ushell_task.h.
| #define STR_STOP "st" |
Definition at line 45 of file ushell_task.h.
| void build_cmd | ( | void | ) |
get the full command line to be interpreted.
| none |
Definition at line 164 of file ushell_task.c.
References ABORT_CHAR, BKSPACE_CHAR, cmd_str, CR, i_str, parse_cmd(), uart_getchar(), and uart_test_hit().
00165 { 00166 U8 c; 00167 00168 if (uart_test_hit()) //Something new of the UART ? 00169 { 00170 c=uart_getchar(); 00171 switch (c) 00172 { 00173 case CR: 00174 cmd_str[i_str]=0; //Add NULL char 00175 parse_cmd(); //Decode the command 00176 i_str=0; 00177 break; 00178 case ABORT_CHAR: //^c abort cmd 00179 i_str=0; 00180 printf("\r#"); 00181 break; 00182 case BKSPACE_CHAR: //backspace 00183 if(i_str>0) 00184 { 00185 putchar(c); 00186 putchar(' '); 00187 putchar(c); 00188 } 00189 if(i_str>=1) 00190 { 00191 i_str--; 00192 } 00193 break; 00194 00195 default: 00196 cmd_str[i_str++]=c; //append to cmd line 00197 break; 00198 } 00199 } 00200 }

| void parse_cmd | ( | void | ) |
decodes full command line into command type and arguments This function allows to set the cmd_type to the command type decoded with its respective arguments par_str1 and par_str2
| none |
Definition at line 212 of file ushell_task.c.
References cmd, CMD_BACKWARD, CMD_FORWARD, CMD_GET_ID, CMD_GET_STATUS0, CMD_GET_STATUS1, CMD_HELP, CMD_RUN, CMD_SET_SPEED, CMD_STOP, cmd_str, cmd_type, FALSE, i_str, LSB, MSB, msg_er_cmd_not_found, msg_prompt, par_str1, par_str2, str_backward, str_forward, str_get_id, str_get_status0, str_get_status1, str_help, str_run, str_set_speed, str_stop, and TRUE.
00213 { 00214 U8 i=0; 00215 U8 j; 00216 00217 //Get command type 00218 for(i=0;cmd_str[i]!=' ' && i<=i_str;i++); 00219 cmd=TRUE; 00220 00221 //Decode command type 00222 00223 if ( mystrncmp(cmd_str,str_run,i-1)) 00224 { cmd_type=CMD_RUN; } 00225 else if ( mystrncmp(cmd_str,str_stop,i-1)) 00226 { cmd_type=CMD_STOP; } 00227 else if ( mystrncmp(cmd_str,str_help,i-1)) 00228 { cmd_type=CMD_HELP; } 00229 else if ( mystrncmp(cmd_str,str_forward,i-1)) 00230 { cmd_type=CMD_FORWARD; } 00231 else if ( mystrncmp(cmd_str,str_backward,i-1)) 00232 { cmd_type=CMD_BACKWARD; } 00233 else if ( mystrncmp(cmd_str,str_set_speed,i-1)) 00234 { cmd_type=CMD_SET_SPEED; } 00235 else if ( mystrncmp(cmd_str,str_get_id,i-1)) 00236 { cmd_type=CMD_GET_ID; } 00237 else if ( mystrncmp(cmd_str,str_get_status0,i-1)) 00238 { cmd_type=CMD_GET_STATUS0; } 00239 else if ( mystrncmp(cmd_str,str_get_status1,i-1)) 00240 { cmd_type=CMD_GET_STATUS1; } 00241 else 00242 { 00243 if(i_str) 00244 { 00245 print_msg(msg_er_cmd_not_found); 00246 } 00247 print_msg(msg_prompt); 00248 cmd=FALSE; 00249 return; 00250 } 00251 00252 //Get first arg (if any) 00253 if(++i<i_str) 00254 { 00255 j=0; 00256 for(;(cmd_str[i]!=' ')&&(i<i_str);i++) 00257 { 00258 LSB(par_str1[j])=cmd_str[i]; 00259 MSB(par_str1[j])=0; 00260 j++; 00261 } 00262 LSB(par_str1[j])=0;MSB(par_str1[j])=0; 00263 } 00264 else { return; } 00265 00266 //Get second arg (if any) 00267 if(++i<i_str) 00268 { 00269 j=0; 00270 for(;(cmd_str[i]!=' ')&&(i<i_str);i++) 00271 { 00272 LSB(par_str2[j])=cmd_str[i]; 00273 MSB(par_str2[j])=0; 00274 j++; 00275 } 00276 LSB(par_str2[j])=0;MSB(par_str2[j])=0; 00277 } 00278 else { return; } 00279 00280 }
| void ushell_task | ( | void | ) |
Entry point of the explorer task management This function links perform ushell task decoding to access file system functions.
| none |
Definition at line 99 of file ushell_task.c.
References BOARD_ID, build_cmd(), cmd, CMD_BACKWARD, CMD_FORWARD, CMD_GET_ID, CMD_GET_STATUS0, CMD_GET_STATUS1, CMD_HELP, CMD_NONE, CMD_RUN, CMD_SET_SPEED, CMD_STOP, cmd_type, convert_param1(), FALSE, mci_backward(), mci_direction, mci_forward(), mci_get_measured_current(), mci_get_measured_speed(), mci_run(), mci_run_stop, mci_set_speed(), mci_stop(), msg_er_cmd_not_found, msg_help, msg_prompt, param1, print_hex16(), REV_ID, and SOFT_ID.
00100 { 00101 U8 status = 0; 00102 00103 if(cmd==FALSE) 00104 { 00105 build_cmd(); 00106 } 00107 else 00108 { 00109 switch (cmd_type) 00110 { 00111 case CMD_HELP: 00112 print_msg(msg_help); 00113 break; 00114 case CMD_RUN: 00115 mci_run(); 00116 break; 00117 case CMD_STOP: 00118 mci_stop(); 00119 break; 00120 case CMD_FORWARD: 00121 mci_forward(); 00122 break; 00123 case CMD_BACKWARD: 00124 mci_backward(); 00125 break; 00126 case CMD_SET_SPEED: 00127 convert_param1(); 00128 mci_set_speed(param1); 00129 break; 00130 case CMD_GET_ID: 00131 print_hex16(BOARD_ID); 00132 putchar(' '); 00133 print_hex16(SOFT_ID); 00134 putchar(' '); 00135 print_hex16(REV_ID); 00136 break; 00137 case CMD_GET_STATUS0: 00138 status = (mci_direction<<3)|(mci_run_stop<<2); 00139 print_hex16(status); 00140 putchar(' '); 00141 print_hex16(mci_get_measured_speed()); 00142 putchar(' '); 00143 print_hex16(mci_get_measured_current()); 00144 break; 00145 case CMD_GET_STATUS1: 00146 print_hex16(0xDEA); 00147 putchar(' '); 00148 print_hex16(0x123); 00149 break; 00150 default: //Unknown command 00151 print_msg(msg_er_cmd_not_found); 00152 } 00153 cmd_type=CMD_NONE; 00154 cmd=FALSE; 00155 print_msg(msg_prompt); 00156 } 00157 }

| void ushell_task_init | ( | void | ) |
This function initializes the hardware/software ressources required for ushell task.
| none |
Definition at line 73 of file ushell_task.c.
References cmd, CMD_NONE, cmd_type, FALSE, msg_prompt, msg_welcome, uart_getchar(), uart_init(), and uart_putchar.
00074 { 00075 uart_init(); 00076 #ifdef __GNUC__ 00077 fdevopen((int (*)(char, FILE*))(uart_putchar),(int (*)(FILE*))uart_getchar); //for printf redirection 00078 #endif 00079 print_msg(msg_welcome); 00080 print_msg(msg_prompt); 00081 cmd=FALSE; 00082 cmd_type=CMD_NONE; 00083 00084 00085 }

1.5.3