| AVR Z-LINKŪ | |||||
Classes | |
| class | NewAssociationIndication |
| Defines a NewAssociationIndication instance. More... | |
| interface | NewAssociationIndicationListener |
| This interface defines the function that any NewAssociationIndicationListener must implement. More... | |
| class | NewDataIndication |
| Defines a NewDataIndication instance. More... | |
| interface | NewDataIndicationListener |
| This interface defines the function that any NewDataIndicationListener must implement. More... | |
| class | NewDisassociationIndication |
| Class that defines the NewDisassociationIndication object. The NewDisassociationIndication notifies the NewDisassociation listener that one of the radios in the peer-to-peer link wishes to disconnect. More... | |
| interface | NewDisassociationIndicationListener |
| This interface defines the function that any NewDisassociationIndicationListener must implement. More... | |
| class | RadioInterface |
| The radio interface is the next higher layer of the SerialStream. This layer defines the AT-Command interface to the radio. More... | |
| class | RadioInterfaceStartException |
| Class that defines the exception thrown by the RadioInterface in the case of an error during start-up of the radio. More... | |
| class | TimeOut |
| This class defines a TimerTask that is used to ensure that the radio answers any request/command within a specified time. More... | |
Generated on Sat Dec 2 16:14:07 2006 for AVR414 User's Guide - ATAVRRZ502 - Accessory Kit by 1.4.7
|