AVR Z-LINKŪ


Package gui


Classes

class  ChatWindow
 ChatWindow is a class that defines the graphical interface to display the live traffic. Incomming messages will be appended to the conversation ("Chat") and the end user can type in new messages. More...
class  ChatWindowEvent
 Defines a ChatWindowEvent instance. More...
interface  ChatWindowEventListener
 Defines a ChatWindowEventListener interface. More...
class  ConfigurationDialog
 The ConfigurationDialog is a extension of the JDialog. More...
class  Dialogs
 Group of JDialogs used by the GUI. More...
class  MainFrame
 The MainFrame is the background component (JFrame) and where tabing is enabled. This is what the user will see directly after start-up. More...
class  MainFrameEvent
 MainFrameEvents are sent to MainFrameEventListeners to notify them that something new has happened. More...
interface  MainFrameEventListener
 MainFrameEventLIstener interface. More...
@DOC_TITLE@
Generated on Sat Dec 2 16:14:07 2006 for AVR414 User's Guide - ATAVRRZ502 - Accessory Kit by doxygen 1.4.7