AVR Z-LINKŪ


serialInterface.SerialStream Class Reference

List of all members.

Detailed Description

This class defines serial streams that can be used for writing and reading to/from serial ports.

Application note:
AVR414: User's Guide - ATAVRRZ502 - Accessory Kit
Author:
Atmel Corporation: http://www.atmel.com
Support email: avr@atmel.com
Name
vkbakken
Revision
1.5
RCSfile
code_header_template_CVS_DOXYGEN.txt,v
Date
2006/04/07 12:40:07

Definition at line 29 of file SerialStream.java.

Public Member Functions

void addSerialStreamEventListener (SerialStreamListener ssListener)
 This function adds a new SerialStreamEventListener to the queue of event listeners.
void disableSerialStreamEvents ()
 This function disables SerialStream event generation.
void enableSerialStreamEvents ()
 This function enables SerialStream event generation.
String getData ()
 This function is used to get data from the output stream.
SerialPort getSerialPortUsed ()
 Return the SerialPort instance to which the io streams are connected.
void removeSerialStreamListener (SerialStreamListener ssListener)
 This function deletes a SerialStreamListener from the queue of event listeners.
void resetReceiver ()
 This function resets the receiver.
void sendData (String data)
 This function is used to append data to the output stream.
String sendDataBlocking (String data)
 This is the blocking version of sendData.
void serialEvent (SerialPortEvent spe)
 Function that any SerialPortEventListener must implement. It is called whenever new events are available.
 SerialStream (SerialPort portToAppendStream) throws SerialStreamException
 This is the SerialStream constructor. Creates a new serial stream if possible.

Protected Member Functions

void fireSearialStreamEvent (SerialStreamEvent SerialStreamEvent)
 When this function is called a new SerialStreamEvent is injected into the dispatcher queue to be handled by the associated SerialStreamListener.
@DOC_TITLE@
Generated on Sat Dec 2 16:14:07 2006 for AVR414 User's Guide - ATAVRRZ502 - Accessory Kit by doxygen 1.4.7