| AVR Z-LINKŪ | |||||
Definition in file utilities.c.
#include <stdint.h>
#include <stdbool.h>
#include "compiler.h"
#include "utilities.h"
Include dependency graph for utilities.c:

Go to the source code of this file.
Functions | |
| bool | htoi16 (uint8_t *hex, uint16_t *ret) |
| Convert two byte hex value [0x0000 to 0xFFFF] to integer. | |
| bool | htoi8 (uint8_t *hex, uint8_t *ret) |
| Convert two byte hex value [0x00 to 0xFF] to integer. | |
| bool | stringCompare (const uint8_t *str, const uint8_t __flash *fstr) |
| Will compare two strings and ensure that they are identical. | |
| bool htoi16 | ( | uint8_t * | hex, | |
| uint16_t * | ret | |||
| ) |
Convert two byte hex value [0x0000 to 0xFFFF] to integer.
| hex | Ascii representation of two byte hex value. | |
| ret | Pointer to place the integer representation at. |
Definition at line 150 of file utilities.c.
Referenced by handleNewCommand().
00150 { 00151 00152 uint8_t i = 0x00; 00153 uint16_t radix = 1; 00154 *ret = 0x0000; 00155 00156 //Run through and check that the length is valid. 00157 while( *hex != '\0' ){ 00158 00159 //Return with false with the ascii char is not in 00160 //the [0->F] range. 00161 if( !( ( ( *hex >= '0' ) && ( *hex <= '9' ) ) || 00162 ( ( *hex >= 'A' ) && ( *hex <= 'F' ) ) ) ){ 00163 00164 return false; 00165 } 00166 00167 hex++; 00168 i++; 00169 } 00170 00171 //Only Four or less digits. Valid conversion. 00172 if( i <= 0x04 ){ 00173 00174 hex--; 00175 00176 //Do the actual conversion. 00177 for( ; i > 0; i-- ){ 00178 00179 // 0->9 00180 if( ( *hex >= '0' ) && ( *hex <= '9' ) ){ 00181 00182 *ret += radix * ( *hex - '0' ); 00183 } 00184 00185 //A->F 00186 else{ 00187 00188 *ret += radix * ( *hex - 'A' + 10 ); 00189 } 00190 00191 hex--; 00192 radix = radix << 4; 00193 } 00194 00195 return true; 00196 } 00197 00198 //Return with an error. 00199 else{ 00200 00201 return false; 00202 } 00203 }
| bool htoi8 | ( | uint8_t * | hex, | |
| uint8_t * | ret | |||
| ) |
Convert two byte hex value [0x00 to 0xFF] to integer.
| hex | Ascii representation of two byte hex value. | |
| ret | Pointer to place the integer representation at. |
Definition at line 85 of file utilities.c.
Referenced by handleNewCommand().
00085 { 00086 00087 uint8_t i = 0x00; 00088 uint8_t radix = 1; 00089 *ret = 0x00; 00090 00091 //Run through and check that the length is valid. 00092 while( *hex != '\0' ){ 00093 00094 //Return with false with the ascii char is not in 00095 //the [0->F] range. 00096 if( !( ( ( *hex >= '0' ) && ( *hex <= '9' ) ) || 00097 ( ( *hex >= 'A' ) && ( *hex <= 'F' ) ) ) ){ 00098 00099 return false; 00100 } 00101 00102 hex++; 00103 i++; 00104 } 00105 00106 //Only two or less digits. Valid conversion. 00107 if( i <= 0x02 ){ 00108 00109 hex--; 00110 00111 //Do the actual conversion. 00112 for( ; i > 0; i-- ){ 00113 00114 // 0->9 00115 if( ( *hex >= '0' ) && ( *hex <= '9' ) ){ 00116 00117 *ret += radix * ( *hex - '0' ); 00118 } 00119 00120 //A->F 00121 else{ 00122 00123 *ret += radix * ( *hex - 'A' + 10 ); 00124 } 00125 00126 hex--; 00127 radix = radix << 4; // Multiply by 16. 00128 } 00129 00130 return true; 00131 } 00132 00133 //Return with an error. 00134 else{ 00135 00136 return false; 00137 } 00138 }
| bool stringCompare | ( | const uint8_t * | str, | |
| const uint8_t __flash * | fstr | |||
| ) |
Will compare two strings and ensure that they are identical.
str will be compared against fstr to see if they are identical. They must be of same length and contentent to be identical.
| str | String one. | |
| fstr | String to compare with. |
Definition at line 47 of file utilities.c.
References END_OF_STRING.
Referenced by handleNewCommand().
00047 { 00048 00049 //Run until one of the strings are terminated. 00050 while( !( ( *str == END_OF_STRING ) || ( *fstr == END_OF_STRING ) ) ){ 00051 00052 //If they are not equal before END_OF_STRING, return false. 00053 if( *str != *fstr ){ 00054 00055 break; 00056 } 00057 00058 str++; 00059 fstr++; 00060 } 00061 00062 //Both strings equal and of same length. 00063 if( ( ( *str == END_OF_STRING ) && ( *fstr == END_OF_STRING ) ) ){ 00064 00065 return true; 00066 } 00067 00068 //Equal, unequal or of different legth. 00069 else{ 00070 00071 return false; 00072 } 00073 }
Generated on Sat Dec 2 16:05:51 2006 for AVR414 User's Guide - ATAVRRZ502 - Accessory Kit by 1.4.7
|