| AVR Z-LINKŪ | |||||
Definition in file serialPortHAL.c.
#include "serialPortHAL.h"
Include dependency graph for serialPortHAL.c:

Go to the source code of this file.
Functions | |
| bool | dataAvailable (void) |
| Function that is used to poll if new data is available. | |
| static uint8_t | errToHex (uint8_t hexNibble) |
| Returns the rxError_t member of the rxDataBlock_t struct. | |
| unsigned char * | getATCommand (void) |
| Returns a pointer to the read AT-Command. | |
| rxError_t | getError (void) |
| Returns the rxError_t member of the rxDataBlock_t struct. | |
| unsigned char * | getParameterNumber (paramter_t parameterNumber) |
| Returns a pointer to the specified parameter. | |
| ISR (USART0_RX_vect) | |
| Universal receive interrupt service routine for both USART0 and the FTDI USB chip. | |
| void | rxReset (void) |
| This function is used to reset the receive interrupt and associated variables. | |
| void | sendAssociationNotification (void) |
| Send notification over the serial link that an end-device has associated successfully. | |
| void | sendDataNotification (uint8_t length, unsigned char *data) |
| Send notification when new data has been received. | |
| void | sendDisAssociationNotification (void) |
| Send notification over the serial link when the the other peer has requested to leave (disassociate). | |
| void | sendERROR (const chatError_t err) |
| Send an error message over the serial link. | |
| void | sendFlashString (const unsigned char __flash *string) |
| Send a flash string over the serial link (USART or USB). | |
| void | sendOK (void) |
| Send the "OK" string over the serial link. | |
| void | sendString (const unsigned char *string) |
| Send a string over the serial link (USART or USB). | |
| static void | sendStringWithLength (const unsigned char *string, const uint8_t strLength) |
| Internal (static) method used by sendDataNotification() to send a string with a given length. | |
| static void | sendSymbol (const unsigned char symbol) |
| Send one symbol on the serial line. | |
| void | serialInterfaceInitialization (void) |
| This function handles the initialization of the serial interface. | |
Variables | |
| const unsigned char __flash | ASSOCIATION_NOTIFICATION [] = "+N" |
| String sent over the serial interface to notify tha a device has successfully been associated to the coordinator. | |
| const unsigned char __flash | CRNL [] = "\r\n" |
| Carrige Return New Line. | |
| const unsigned char __flash | DISASSOCIATION_NOTIFICATION [] = "+D" |
| String sent over the serial interface to notify that the associated end-device has successfully left the network. | |
| const unsigned char __flash | ERROR [] = "ERROR: 0x" |
| String sent over the serial interface whenever an error occurs. Used by the sendERROR() function. | |
| const uint8_t __flash | hexTable [] = "0123456789ABCDEF" |
| Look-up table used by errToHex() to do hex conversions. | |
| const unsigned char __flash | NEW_DATA_NOTIFICATION [] = "+T: " |
| String sent over the serial interface to notify that new data has been received. | |
| const unsigned char __flash | OK [] = "OK\r\n" |
| String sent over the serial interface whenever an AT-Command terminates successfully. | |
| rxDataBlock_t | rxData |
| rxState_t | rxState |
| bool dataAvailable | ( | void | ) |
Function that is used to poll if new data is available.
Definition at line 161 of file serialPortHAL.c.
References rxDataBlock_t::receptionComplete, and rxData.
Referenced by main().
00161 { 00162 00163 return rxData.receptionComplete; 00164 }
| static uint8_t errToHex | ( | uint8_t | hexNibble | ) | [static] |
Returns the rxError_t member of the rxDataBlock_t struct.
Definition at line 292 of file serialPortHAL.c.
References hexTable.
Referenced by sendERROR().
00292 { 00293 00294 return hexTable[ hexNibble ]; 00295 }
| unsigned char* getATCommand | ( | void | ) |
Returns a pointer to the read AT-Command.
Definition at line 142 of file serialPortHAL.c.
References rxDataBlock_t::ATCommand, and rxData.
Referenced by handleNewCommand().
| rxError_t getError | ( | void | ) |
Returns the rxError_t member of the rxDataBlock_t struct.
Definition at line 151 of file serialPortHAL.c.
References rxDataBlock_t::error, and rxData.
| unsigned char* getParameterNumber | ( | paramter_t | parameterNumber | ) |
Returns a pointer to the specified parameter.
| parameterNumber | What parameter to be returned. |
Definition at line 173 of file serialPortHAL.c.
References NULL_PARAMETER, NUMBER_OF_PARAMETERS, rxDataBlock_t::parameter, and rxData.
Referenced by handleNewCommand().
00173 { 00174 00175 if( parameterNumber < NUMBER_OF_PARAMETERS ){ 00176 00177 return rxData.parameter[ parameterNumber ]; 00178 } 00179 00180 00181 else{ 00182 00183 return NULL_PARAMETER; 00184 } 00185 }
| ISR | ( | USART0_RX_vect | ) |
Universal receive interrupt service routine for both USART0 and the FTDI USB chip.
This routine is called whenever a new byte is available to be read. This service routine does also implement a sort of pre parsing since the received stream of bytes comes in a known pattern (AT-Commands). Where data is read from is controlled through the UART or FTDI flag. So the only difference is the interrupt vector and where to read data from.
Definition at line 397 of file serialPortHAL.c.
References rxDataBlock_t::ATCommand, BUFFER_OVERFLOW, COLLECT_PARAMETERS, EOC, EOC_DELIMITER, rxDataBlock_t::error, FTDI_Fifo, ISR(), LENGTH_OF_COMMAND, LENGTH_OF_PARAMETER_BUFFER, NUMBER_OF_PARAMETERS, rxDataBlock_t::numberOfReceivedParameters, PARAM_PREAMBLE, rxDataBlock_t::parameter, PARAMETER_DELIMITER, PARAMETER_PREAMBLE_A, PARAMETER_PREAMBLE_B, rxDataBlock_t::parameters, RECEIVER_OFF, rxDataBlock_t::receptionComplete, rxDataBlock_t::rx_i, rxData, rxState, SOC, UNKNOWN_EOC_SEQUENCE, UNKNOWN_RX_STATE, and UNKNOWN_SEQUENCE.
Referenced by ISR().
00397 { 00398 00399 uint8_t receivedData; 00400 00401 receivedData = ( uint8_t )UDR0; //Collect data. 00402 #else 00403 ISR( INT7_vect ){ 00404 00405 unsigned char receivedData; 00406 00407 receivedData = ( uint8_t )*FTDI_Fifo; //Collect data. 00408 #endif 00409 00410 switch( rxState ){ 00411 00412 case SOC: 00413 00414 if( rxData.rx_i <= LENGTH_OF_COMMAND ){ 00415 00416 if( receivedData == PARAMETER_PREAMBLE_A ){ 00417 00418 rxData.ATCommand[ rxData.rx_i ] = '\0'; 00419 rxState = PARAM_PREAMBLE; 00420 } 00421 00422 else if( receivedData == EOC_DELIMITER ){ 00423 00424 rxData.ATCommand[ rxData.rx_i ] = '\0'; 00425 rxState = EOC; 00426 } 00427 00428 else{ 00429 00430 rxData.ATCommand[ rxData.rx_i++ ] = receivedData; 00431 } 00432 } 00433 00434 else{ 00435 00436 RECEIVER_OFF; 00437 rxData.error = BUFFER_OVERFLOW; 00438 rxData.receptionComplete = true; 00439 } 00440 00441 break; 00442 00443 case PARAM_PREAMBLE: 00444 00445 if( receivedData == PARAMETER_PREAMBLE_B ){ 00446 00447 rxData.rx_i = 0; 00448 rxData.parameter[ rxData.numberOfReceivedParameters++ ] = \ 00449 &rxData.parameters[ rxData.rx_i ]; 00450 rxState = COLLECT_PARAMETERS; 00451 } 00452 00453 else{ 00454 00455 RECEIVER_OFF; 00456 rxData.error = UNKNOWN_SEQUENCE; 00457 rxData.receptionComplete = true; 00458 } 00459 00460 break; 00461 00462 case COLLECT_PARAMETERS: 00463 00464 00465 if( ( rxData.rx_i < LENGTH_OF_PARAMETER_BUFFER )&& 00466 ( rxData.numberOfReceivedParameters < NUMBER_OF_PARAMETERS ) ) 00467 { 00468 00469 if( receivedData == PARAMETER_DELIMITER ){ 00470 00471 rxData.parameters[ rxData.rx_i++ ] = '\0'; 00472 rxData.parameter[ rxData.numberOfReceivedParameters++ ] = \ 00473 &rxData.parameters[ rxData.rx_i ]; 00474 } 00475 00476 00477 else if( receivedData == EOC_DELIMITER ){ 00478 00479 rxData.parameters[ rxData.rx_i ] = '\0'; 00480 rxState = EOC; 00481 } 00482 00483 else{ 00484 00485 rxData.parameters[ rxData.rx_i++ ] = receivedData; 00486 } 00487 } 00488 00489 else{ 00490 00491 RECEIVER_OFF; 00492 rxData.error = BUFFER_OVERFLOW; 00493 rxData.receptionComplete = true; 00494 } 00495 break; 00496 00497 case EOC: 00498 00499 RECEIVER_OFF; 00500 00501 if( receivedData != '\n' ){ 00502 00503 rxData.error = UNKNOWN_EOC_SEQUENCE; 00504 } 00505 00506 rxData.receptionComplete = true; 00507 break; 00508 00509 default: 00510 00511 RECEIVER_OFF; 00512 rxData.error = UNKNOWN_RX_STATE; 00513 rxData.receptionComplete = true; 00514 break; 00515 } 00516 }
Here is the call graph for this function:

| void rxReset | ( | void | ) |
This function is used to reset the receive interrupt and associated variables.
Definition at line 111 of file serialPortHAL.c.
References rxDataBlock_t::ATCommand, rxDataBlock_t::error, NO_ERROR, rxDataBlock_t::numberOfReceivedParameters, rxDataBlock_t::parameters, RECEIVER_OFF, RECEIVER_ON, rxDataBlock_t::receptionComplete, rxDataBlock_t::rx_i, rxData, rxState, and SOC.
Referenced by main().
00111 { 00112 00113 unsigned char dummy = 0x00; 00114 00115 RECEIVER_OFF; 00116 00117 rxState = SOC; 00118 00119 rxData.rx_i = dummy; 00120 rxData.ATCommand[ rxData.rx_i ] = dummy; 00121 rxData.parameters[ rxData.rx_i ] = dummy; 00122 rxData.numberOfReceivedParameters = dummy; 00123 rxData.receptionComplete = false; 00124 rxData.error = NO_ERROR; 00125 00126 #ifdef UART 00127 //Following loop is used to ensure that the rx FIFO is flushed. 00128 //Sometimes it gets cloged up with old data. 00129 for( ; UCSR0A & ( 1 << RXC0 ); ){ 00130 00131 dummy = UDR0; 00132 } 00133 #endif 00134 00135 RECEIVER_ON; 00136 }
| void sendAssociationNotification | ( | void | ) |
Send notification over the serial link that an end-device has associated successfully.
Message format: <+N
>
Definition at line 303 of file serialPortHAL.c.
References ASSOCIATION_NOTIFICATION, CRNL, and sendFlashString().
Referenced by usr_mlme_comm_status_ind().
00303 { 00304 00305 sendFlashString( ASSOCIATION_NOTIFICATION ); 00306 sendFlashString( CRNL ); 00307 00308 return; 00309 }
Here is the call graph for this function:

| void sendDataNotification | ( | uint8_t | length, | |
| unsigned char * | data | |||
| ) |
Send notification when new data has been received.
Message format: <+T: [length],[data payload]
>
| length | Length of data in bytes. | |
| data | Pointer to data. |
Definition at line 333 of file serialPortHAL.c.
References CRNL, NEW_DATA_NOTIFICATION, sendFlashString(), sendString(), sendStringWithLength(), and sendSymbol().
Referenced by usr_mcps_data_ind().
00333 { 00334 00335 uint8_t i, ii, dataLength; 00336 unsigned char valueReversed[ 3 ]; 00337 unsigned char asciiValue[ 4 ]; 00338 00339 dataLength = length; 00340 00341 //Make sure that only 3 iterations are made. 00342 for( i = ii = 0; (ii < 3) && ( dataLength != 0 ) ; ii++ ){ 00343 00344 i = dataLength % 10; 00345 dataLength = dataLength / 10; 00346 00347 valueReversed[ ii ] = i + '0'; 00348 } 00349 00350 asciiValue[ ii ] = '\0'; //Terminate string 00351 00352 //Reverse the order of digits. 00353 for( i = 0, ii; ii > 0 ; ii--, i++ ){ 00354 00355 asciiValue[ i ] = valueReversed[ ii - 1 ]; 00356 } 00357 00358 00359 sendFlashString( NEW_DATA_NOTIFICATION ); 00360 sendString( asciiValue ); 00361 //sendStringWithLength( asciiValue, length ); //Dummy...hardcoded. 00362 sendSymbol( ',' ); 00363 sendStringWithLength( data, length ); 00364 sendFlashString( CRNL ); 00365 00366 return; 00367 }
Here is the call graph for this function:

| void sendDisAssociationNotification | ( | void | ) |
Send notification over the serial link when the the other peer has requested to leave (disassociate).
Message format: <+D
>
Definition at line 316 of file serialPortHAL.c.
References CRNL, DISASSOCIATION_NOTIFICATION, and sendFlashString().
00316 { 00317 00318 sendFlashString( DISASSOCIATION_NOTIFICATION ); 00319 sendFlashString( CRNL ); 00320 00321 return; 00322 }
Here is the call graph for this function:

| void sendERROR | ( | const chatError_t | err | ) |
Send an error message over the serial link.
The sent string will be "ERROR: " and then one of the follwing hex values:
| err | Error type to return with. Must be a valid number for the chatError_t type. |
Definition at line 274 of file serialPortHAL.c.
References CRNL, ERROR, errToHex(), sendFlashString(), and sendSymbol().
Referenced by handleNewCommand(), sendMsg(), usr_mcps_data_conf(), usr_mlme_associate_conf(), usr_mlme_reset_conf(), usr_mlme_scan_conf(), usr_mlme_set_conf(), and usr_mlme_start_conf().
00274 { 00275 00276 sendFlashString( ERROR ); 00277 00278 //Convert from err to ascii hex: 00279 sendSymbol( errToHex( (err & 0xF0) >> 4 ) ); //MSB 00280 sendSymbol( errToHex( err & 0x0F ) ); //LSB 00281 00282 sendFlashString( CRNL ); 00283 00284 return; 00285 }
Here is the call graph for this function:

| void sendFlashString | ( | const unsigned char __flash * | string | ) |
Send a flash string over the serial link (USART or USB).
| string | string to be sent. |
Definition at line 228 of file serialPortHAL.c.
References sendSymbol().
Referenced by sendAssociationNotification(), sendDataNotification(), sendDisAssociationNotification(), sendERROR(), and sendOK().
00228 { 00229 00230 for( ; *string != '\0'; ){ 00231 00232 sendSymbol( *string++ ); 00233 } 00234 00235 return; 00236 }
Here is the call graph for this function:

| void sendOK | ( | void | ) |
Send the "OK" string over the serial link.
Definition at line 242 of file serialPortHAL.c.
References OK, and sendFlashString().
Referenced by usr_mcps_data_conf(), usr_mlme_associate_conf(), usr_mlme_reset_conf(), and usr_mlme_set_conf().
00242 { 00243 00244 sendFlashString( OK ); 00245 00246 return; 00247 }
Here is the call graph for this function:

| void sendString | ( | const unsigned char * | string | ) |
Send a string over the serial link (USART or USB).
| string | string to be sent. |
Definition at line 213 of file serialPortHAL.c.
References sendSymbol().
Referenced by sendDataNotification().
00213 { 00214 00215 for( ; *string != '\0'; ){ 00216 00217 sendSymbol( *string++ ); 00218 } 00219 00220 return; 00221 }
Here is the call graph for this function:

| static void sendStringWithLength | ( | const unsigned char * | string, | |
| const uint8_t | strLength | |||
| ) | [static] |
Internal (static) method used by sendDataNotification() to send a string with a given length.
| string | String to send bytes from. | |
| strLength | Number of bytes to send. |
Definition at line 376 of file serialPortHAL.c.
References sendSymbol().
Referenced by sendDataNotification().
00376 { 00377 00378 uint8_t i; 00379 00380 for( i = 0; i < strLength; i++ ){ 00381 00382 sendSymbol( *string++ ); 00383 } 00384 00385 return; 00386 }
Here is the call graph for this function:

| static void sendSymbol | ( | const unsigned char | symbol | ) | [static] |
Send one symbol on the serial line.
This function passes one symbol (8 bits) to the USART module on the AVR or the FTDI USB chip.
| symbol | Symbol to be sent. |
Definition at line 197 of file serialPortHAL.c.
References ftdiSendSymbol(), and uartSendSymbol().
Referenced by sendDataNotification(), sendERROR(), sendFlashString(), sendString(), and sendStringWithLength().
00197 { 00198 00199 #ifdef UART 00200 00201 uartSendSymbol( symbol ); 00202 #else 00203 ftdiSendSymbol( symbol ); 00204 #endif 00205 }
Here is the call graph for this function:

| void serialInterfaceInitialization | ( | void | ) |
This function handles the initialization of the serial interface.
What serial interface that actually will be initialized is controlled by the UART or FTDI flag. If the UART flag is defined USART0 is defined with a sybol size of 8 bits, no parity and one stop bit. If FTDI is defined the FTDI USB chip will be setup the same way.
Definition at line 97 of file serialPortHAL.c.
References BR_38400, ftdiInitialization(), and uartInitialization().
Referenced by applicationInit().
00097 { 00098 00099 #ifdef UART 00100 00101 uartInitialization( BR_38400 ); 00102 #else 00103 ftdiInitialization( ); 00104 #endif 00105 }
Here is the call graph for this function:

| const unsigned char __flash ASSOCIATION_NOTIFICATION[] = "+N" |
String sent over the serial interface to notify tha a device has successfully been associated to the coordinator.
Definition at line 52 of file serialPortHAL.c.
Referenced by sendAssociationNotification().
| const unsigned char __flash CRNL[] = "\r\n" |
Carrige Return New Line.
Definition at line 72 of file serialPortHAL.c.
Referenced by sendAssociationNotification(), sendDataNotification(), sendDisAssociationNotification(), and sendERROR().
| const unsigned char __flash DISASSOCIATION_NOTIFICATION[] = "+D" |
String sent over the serial interface to notify that the associated end-device has successfully left the network.
Definition at line 59 of file serialPortHAL.c.
Referenced by sendDisAssociationNotification().
| const unsigned char __flash ERROR[] = "ERROR: 0x" |
String sent over the serial interface whenever an error occurs. Used by the sendERROR() function.
Definition at line 45 of file serialPortHAL.c.
Referenced by sendERROR().
| const uint8_t __flash hexTable[] = "0123456789ABCDEF" |
Look-up table used by errToHex() to do hex conversions.
Definition at line 78 of file serialPortHAL.c.
Referenced by errToHex().
| const unsigned char __flash NEW_DATA_NOTIFICATION[] = "+T: " |
String sent over the serial interface to notify that new data has been received.
Definition at line 66 of file serialPortHAL.c.
Referenced by sendDataNotification().
| const unsigned char __flash OK[] = "OK\r\n" |
String sent over the serial interface whenever an AT-Command terminates successfully.
Definition at line 38 of file serialPortHAL.c.
Referenced by sendOK().
Definition at line 30 of file serialPortHAL.c.
Referenced by dataAvailable(), getATCommand(), getError(), getParameterNumber(), ISR(), and rxReset().
Generated on Sat Dec 2 16:05:51 2006 for AVR414 User's Guide - ATAVRRZ502 - Accessory Kit by 1.4.7
|