AVR Z-LINKŪ


AVR414: User's Guide - ATAVRRZ502 - Accessory Kit.

Contents

Introduction

The AVR414 application note serves as an user's guide for the ATAVRRZ502 Accessory Kit. An evaluation application is furnished with this kit. This application defines a thin layer on top of the IEEE 802.15.4 library available from Atmel that makes it possible to send data between two peers. The IEEE 802.15.4 standard defines a radio transceiver and protocol stack for wireless personal area networks (WPANs) with relative low data rate (250 kbps).

Both hardware and software building blocks are needed to realize the evaluation application of AVR414. These blocks are briefly presented in the following list. The picture below can also be used as a cross-reference.

Building Blocks:

AVR414Overview.png

AVR414 from a system point of view.

The focus for this documentation is the code written in the C programming language for the AVR.

@DOC_TITLE@
Generated on Sat Dec 2 16:05:51 2006 for AVR414 User's Guide - ATAVRRZ502 - Accessory Kit by doxygen 1.4.7