AVR Z-LINKŪ


AVR414 User's Guide - ATAVRRZ502 - Accessory Kit File List

Here is a list of all files with brief descriptions:
atParser.c [code]This file implements the textual AT interface
atParser.h [code]Header file for the atParser.c
callbacks.c [code]This files implements all the necessary callback functions
chat.h [code]Definition of states and error codes etc
compiler.h [code]File containing some "glue" so that the IAR compiler and GCC can be used interchangeably
documentation.h [code]This file is not a part of the header files referenced by the source code. However it defines the only a part of the doxygen documentation
ftdi.c [code]This files contains the functions for initializing and sending data using the FTDI USB fifo on the STK541 board
ftdi.h [code]Header file for the FTDI USB fifo
main.c [code]File containing the main loop
serialPortHAL.c [code]This defines hardware abstraction level, so that the it is invisible to the next higher layer if the USART0 or FTDI USB chip is used for serial communication
serialPortHAL.h [code]This file defines the serial interface. Either USART or USB. Controlled by the UART/FTDI flags on line 28/29
usart.c [code]This files contains the functions for initializing and sending data using the USART0 of the AVR microcontroller
usart.h [code]This is the header file for the usart.c
utilities.c [code]This files contains the implementation for some of the support functions used by this application
utilities.h [code]Header files that defines interface to the defined support functions
@DOC_TITLE@
Generated on Sat Dec 2 16:05:51 2006 for AVR414 User's Guide - ATAVRRZ502 - Accessory Kit by doxygen 1.4.7