| Remote Access Control | |||||
This file contains the prototypes for common functions needed by the Remote Keyless Entry application. The implementation is found in the common.c file.
Copyright (c) 2006, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL ``AS IS'' AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file common.h.
#include <ioavr.h>
#include <inavr.h>
Include dependency graph for common.h:

This graph shows which files directly or indirectly include this file:

Go to the source code of this file.
Typedefs | |
| typedef uint8_t | byte |
| typedef short | int16_t |
| typedef long | int32_t |
| typedef signed char | int8_t |
| typedef unsigned short | uint16_t |
| typedef unsigned long | uint32_t |
| typedef unsigned char | uint8_t |
Functions | |
| void | addConstantFromEEPROM (byte *bytes, const byte __eeprom *constant, byte count) |
| void | copyBytes (byte *destination, const byte *source, byte count) |
| void | copyBytesFromEEPROM (byte *destination, const byte __eeprom *source, byte count) |
| void | copyBytesToEEPROM (byte __eeprom *destination, const byte *source, byte count) |
XOR 'count' bytes from 'constant' buffer in EEPROM into 'bytes' buffer in SRAM.
Definition at line 67 of file common.c.
Referenced by calcCMAC(), calcKeySchedule(), and cipherLookup().
00069 { 00070 // Copy to temporary variables for optimization. 00071 byte * tempDestination = bytes; 00072 byte tempCount = count; 00073 byte tempValue; 00074 EEAR = (unsigned short int) constant; 00075 00076 do { 00077 EECR |= (1<<EERE); 00078 ++EEAR; 00079 tempValue = *tempDestination ^ EEDR; // Add in GF(2), ie. XOR. 00080 *tempDestination++ = tempValue; 00081 } while( --tempCount ); 00082 }
Copy 'count' bytes from 'source' buffer to 'destination' buffer in SRAM.
Definition at line 53 of file common.c.
Referenced by calcCMAC(), and calcKeySchedule().
00054 { 00055 // Copy to temporary variables for optimization. 00056 byte * tempDest = destination; 00057 const byte * tempSrc = source; 00058 byte tempCount = count; 00059 00060 do { 00061 *tempDest++ = *tempSrc++; 00062 } while( --tempCount ); 00063 }
Copy 'count' bytes from 'source' buffer in EEPROM to 'destination' buffer in SRAM.
Definition at line 106 of file common.c.
Referenced by calcKeySchedule(), and transmitTeachMessage().
00108 { 00109 // Copy to temporary variables for optimization. 00110 byte * tempDest = destination; 00111 byte tempCount = count; 00112 EEAR = (unsigned short int) source; 00113 00114 do { 00115 EECR |= (1<<EERE); 00116 ++EEAR; 00117 *tempDest++ = EEDR; 00118 } while( --tempCount ); 00119 }
Copy 'count' bytes from 'source' buffer in SRAM to 'destination' buffer in EEPROM.
Definition at line 86 of file common.c.
Referenced by calcCMACSubkey(), and calcKeySchedule().
00088 { 00089 // Copy to temporary variables for optimization. 00090 const byte * tempSrc = source; 00091 byte tempCount = count; 00092 do {} while( EECR & (1<<EEWE) ); 00093 EEAR = (uint16_t) destination; 00094 00095 do { 00096 EEDR = *tempSrc++; 00097 EECR |= (1<<EEMWE); 00098 EECR |= (1<<EEWE); 00099 do {} while( EECR & (1<<EEWE) ); 00100 ++EEAR; 00101 } while( --tempCount ); 00102 }
Generated on Fri Aug 8 11:03:23 2008 for AVR411 Secure Rolling Code Algorithm (Transmitter) by 1.4.7
|