GPIO software driver interface for AVR UC3. More...
#include "gpio.h"Go to the source code of this file.
Defines | |
| #define | GPIO AVR32_GPIO |
| GPIO module instance. | |
Functions | |
Peripheral Bus Interface | |
| int | gpio_enable_module (const gpio_map_t gpiomap, uint32_t size) |
| Enables specific module modes for a set of pins. | |
| int | gpio_enable_module_pin (uint32_t pin, uint32_t function) |
| Enables a specific module mode for a pin. | |
| void | gpio_enable_gpio (const gpio_map_t gpiomap, uint32_t size) |
| Enables the GPIO mode of a set of pins. | |
| void | gpio_enable_gpio_pin (uint32_t pin) |
| Enables the GPIO mode of a pin. | |
| void | gpio_enable_pin_pull_up (uint32_t pin) |
| Enables the pull-up resistor of a pin. | |
| void | gpio_disable_pin_pull_up (uint32_t pin) |
| Disables the pull-up resistor of a pin. | |
| void | gpio_configure_pin (uint32_t pin, uint32_t flags) |
| Configuration functionality on a pin. | |
| void | gpio_configure_group (uint32_t port, uint32_t mask, uint32_t flags) |
| Configuration functionality on a port. | |
| int | gpio_get_pin_value (uint32_t pin) |
| Returns the value of a pin. | |
| int | gpio_get_gpio_pin_output_value (uint32_t pin) |
| Returns the output value set for a GPIO pin. | |
| int | gpio_get_gpio_open_drain_pin_output_value (uint32_t pin) |
| Returns the output value set for a GPIO pin using open drain. | |
| void | gpio_set_gpio_pin (uint32_t pin) |
| Drives a GPIO pin to 1. | |
| void | gpio_set_pin_high (uint32_t pin) |
| Drives a GPIO pin to 1. | |
| void | gpio_set_group_high (uint32_t port, uint32_t mask) |
| Drives a GPIO port to 1. | |
| void | gpio_set_pin_low (uint32_t pin) |
| Drives a GPIO pin to 0. | |
| void | gpio_clr_gpio_pin (uint32_t pin) |
| Drives a GPIO pin to 0. | |
| void | gpio_set_group_low (uint32_t port, uint32_t mask) |
| Drives a GPIO port to 0. | |
| void | gpio_tgl_gpio_pin (uint32_t pin) |
| Toggles a GPIO pin. | |
| void | gpio_toggle_pin (uint32_t pin) |
| Toggles a GPIO pin. | |
| void | gpio_toggle_group (uint32_t port, uint32_t mask) |
| Toggles a GPIO group. | |
| void | gpio_set_gpio_open_drain_pin (uint32_t pin) |
| Drives a GPIO pin to 1 using open drain. | |
| void | gpio_clr_gpio_open_drain_pin (uint32_t pin) |
| Drives a GPIO pin to 0 using open drain. | |
| void | gpio_tgl_gpio_open_drain_pin (uint32_t pin) |
| Toggles a GPIO pin using open drain. | |
| void | gpio_enable_pin_glitch_filter (uint32_t pin) |
| Enables the glitch filter of a pin. | |
| void | gpio_disable_pin_glitch_filter (uint32_t pin) |
| Disables the glitch filter of a pin. | |
| static int | gpio_configure_edge_detector (uint32_t pin, uint32_t mode) |
| Configure the edge detector of an input pin. | |
| int | gpio_enable_pin_interrupt (uint32_t pin, uint32_t mode) |
| Enables the interrupt of a pin with the specified settings. | |
| void | gpio_disable_pin_interrupt (uint32_t pin) |
| Disables the interrupt of a pin. | |
| int | gpio_get_pin_interrupt_flag (uint32_t pin) |
| Gets the interrupt flag of a pin. | |
| void | gpio_clear_pin_interrupt_flag (uint32_t pin) |
| Clears the interrupt flag of a pin. | |
GPIO software driver interface for AVR UC3.
Definition in file gpio.c.
| #define GPIO AVR32_GPIO |
GPIO module instance.
Definition at line 51 of file gpio.c.
Referenced by gpio_clear_pin_interrupt_flag(), gpio_clr_gpio_open_drain_pin(), gpio_clr_gpio_pin(), gpio_configure_edge_detector(), gpio_configure_group(), gpio_configure_pin(), gpio_disable_pin_glitch_filter(), gpio_disable_pin_interrupt(), gpio_disable_pin_pull_up(), gpio_enable_gpio_pin(), gpio_enable_module_pin(), gpio_enable_pin_glitch_filter(), gpio_enable_pin_interrupt(), gpio_enable_pin_pull_up(), gpio_get_gpio_open_drain_pin_output_value(), gpio_get_gpio_pin_output_value(), gpio_get_pin_interrupt_flag(), gpio_get_pin_value(), gpio_set_gpio_open_drain_pin(), gpio_set_gpio_pin(), gpio_set_group_high(), gpio_set_group_low(), gpio_set_pin_high(), gpio_set_pin_low(), gpio_tgl_gpio_open_drain_pin(), gpio_tgl_gpio_pin(), gpio_toggle_group(), and gpio_toggle_pin().
| void gpio_clear_pin_interrupt_flag | ( | uint32_t | pin | ) |
| void gpio_clr_gpio_open_drain_pin | ( | uint32_t | pin | ) |
Drives a GPIO pin to 0 using open drain.
| pin | The pin number. |
Definition at line 502 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrc = 1 << (pin & 0x1F); // Value to be driven on the I/O line: 0.
gpio_port->oders = 1 << (pin & 0x1F); // The GPIO output driver is enabled for that pin.
gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
}
| void gpio_clr_gpio_pin | ( | uint32_t | pin | ) |
Drives a GPIO pin to 0.
| pin | The pin number. |
Definition at line 459 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrc = 1 << (pin & 0x1F); // Value to be driven on the I/O line: 0.
gpio_port->oders = 1 << (pin & 0x1F); // The GPIO output driver is enabled for that pin.
gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
}
| static int gpio_configure_edge_detector | ( | uint32_t | pin, | |
| uint32_t | mode | |||
| ) | [static] |
Configure the edge detector of an input pin.
| pin | The pin number. | |
| mode | The edge detection mode (GPIO_PIN_CHANGE, GPIO_RISING_EDGE or GPIO_FALLING_EDGE). |
Definition at line 543 of file gpio.c.
References GPIO, GPIO_FALLING_EDGE, GPIO_PIN_CHANGE, and GPIO_RISING_EDGE.
Referenced by gpio_enable_pin_interrupt().
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
// Configure the edge detector.
switch (mode)
{
case GPIO_PIN_CHANGE:
gpio_port->imr0c = 1 << (pin & 0x1F);
gpio_port->imr1c = 1 << (pin & 0x1F);
break;
case GPIO_RISING_EDGE:
gpio_port->imr0s = 1 << (pin & 0x1F);
gpio_port->imr1c = 1 << (pin & 0x1F);
break;
case GPIO_FALLING_EDGE:
gpio_port->imr0c = 1 << (pin & 0x1F);
gpio_port->imr1s = 1 << (pin & 0x1F);
break;
default:
return GPIO_INVALID_ARGUMENT;
}
return GPIO_SUCCESS;
}
| void gpio_configure_group | ( | uint32_t | port, | |
| uint32_t | mask, | |||
| uint32_t | flags | |||
| ) |
Configuration functionality on a port.
| port | The port number. | |
| mask | The mask. | |
| flags | The configuration. |
Definition at line 336 of file gpio.c.
References GPIO, GPIO_BOTHEDGES, GPIO_DIR_OUTPUT, GPIO_DRIVE_HIGH, GPIO_DRIVE_LOW, GPIO_FALLING, GPIO_INIT_HIGH, GPIO_INTERRUPT, GPIO_OPEN_DRAIN, GPIO_PULL_DOWN, GPIO_PULL_UP, and GPIO_RISING.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[port];
/* Both pull-up and pull-down set means buskeeper */
#if defined(AVR32_GPIO_200_H_INCLUDED) || defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
if (flags & GPIO_PULL_DOWN)
gpio_port->pders = mask;
else
gpio_port->pderc = mask;
#endif
if (flags & GPIO_PULL_UP)
gpio_port->puers = mask;
else
gpio_port->puerc = mask;
/* Enable open-drain mode if requested */
#if defined(AVR32_GPIO_200_H_INCLUDED) || defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
if (flags & GPIO_OPEN_DRAIN)
gpio_port->odmers = mask;
else
gpio_port->odmerc = mask;
if (flags & GPIO_OPEN_DRAIN)
gpio_port->pders = mask;
else
gpio_port->pderc = mask;
#endif
#if defined(AVR32_GPIO_200_H_INCLUDED) || defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
/* Select drive strength */
if (flags & GPIO_DRIVE_LOW)
gpio_port->odcr0s = mask;
else
gpio_port->odcr0c = mask;
if (flags & GPIO_DRIVE_HIGH)
gpio_port->odcr1s = mask;
else
gpio_port->odcr1c = mask;
#endif
/* Select interrupt level for group */
if (flags & GPIO_INTERRUPT) {
if (flags & GPIO_BOTHEDGES)
{
gpio_port->imr0c = mask;
gpio_port->imr1c = mask;
}
else if (flags & GPIO_RISING)
{
gpio_port->imr0s = mask;
gpio_port->imr1c = mask;
}
else if (flags & GPIO_FALLING)
{
gpio_port->imr0c = mask;
gpio_port->imr1s = mask;
}
}
/* Select direction and initial pin state */
if (flags & GPIO_DIR_OUTPUT) {
if (flags & GPIO_INIT_HIGH)
gpio_port->ovrs = mask;
else
gpio_port->ovrc = mask;
gpio_port->oders = mask;
} else {
gpio_port->oderc = mask;
}
/* Enable GPIO */
gpio_port->gpers = mask;
}
| void gpio_configure_pin | ( | uint32_t | pin, | |
| uint32_t | flags | |||
| ) |
Configuration functionality on a pin.
| pin | The pin number. | |
| flags | The configuration. |
Definition at line 261 of file gpio.c.
References GPIO, GPIO_BOTHEDGES, GPIO_DIR_OUTPUT, GPIO_DRIVE_HIGH, GPIO_DRIVE_LOW, GPIO_FALLING, GPIO_INIT_HIGH, GPIO_INTERRUPT, GPIO_OPEN_DRAIN, GPIO_PULL_DOWN, GPIO_PULL_UP, and GPIO_RISING.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
/* Both pull-up and pull-down set means buskeeper */
#if defined(AVR32_GPIO_200_H_INCLUDED) || defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
if (flags & GPIO_PULL_DOWN)
gpio_port->pders = 1 << (pin & 0x1F);
else
gpio_port->pderc = 1 << (pin & 0x1F);
#endif
if (flags & GPIO_PULL_UP)
gpio_port->puers = 1 << (pin & 0x1F);
else
gpio_port->puerc = 1 << (pin & 0x1F);
/* Enable open-drain mode if requested */
#if defined(AVR32_GPIO_200_H_INCLUDED) || defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
if (flags & GPIO_OPEN_DRAIN)
gpio_port->odmers = 1 << (pin & 0x1F);
else
gpio_port->odmerc = 1 << (pin & 0x1F);
if (flags & GPIO_OPEN_DRAIN)
gpio_port->pders = 1 << (pin & 0x1F);
else
gpio_port->pderc = 1 << (pin & 0x1F);
#endif
#if defined(AVR32_GPIO_200_H_INCLUDED) || defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
/* Select drive strength */
if (flags & GPIO_DRIVE_LOW)
gpio_port->odcr0s = 1 << (pin & 0x1F);
else
gpio_port->odcr0c = 1 << (pin & 0x1F);
if (flags & GPIO_DRIVE_HIGH)
gpio_port->odcr1s = 1 << (pin & 0x1F);
else
gpio_port->odcr1c = 1 << (pin & 0x1F);
#endif
/* Select interrupt level for group */
if (flags & GPIO_INTERRUPT) {
if (flags & GPIO_BOTHEDGES)
{
gpio_port->imr0c = 1 << (pin & 0x1F);
gpio_port->imr1c = 1 << (pin & 0x1F);
}
else if (flags & GPIO_RISING)
{
gpio_port->imr0s = 1 << (pin & 0x1F);
gpio_port->imr1c = 1 << (pin & 0x1F);
}
else if (flags & GPIO_FALLING)
{
gpio_port->imr0c = 1 << (pin & 0x1F);
gpio_port->imr1s = 1 << (pin & 0x1F);
}
}
/* Select direction and initial pin state */
if (flags & GPIO_DIR_OUTPUT) {
if (flags & GPIO_INIT_HIGH)
gpio_port->ovrs = 1 << (pin & 0x1F);
else
gpio_port->ovrc = 1 << (pin & 0x1F);
gpio_port->oders = 1 << (pin & 0x1F);
} else {
gpio_port->oderc = 1 << (pin & 0x1F);
}
/* Enable GPIO */
gpio_port->gpers = 1 << (pin & 0x1F);
}
| void gpio_disable_pin_glitch_filter | ( | uint32_t | pin | ) |
| void gpio_disable_pin_interrupt | ( | uint32_t | pin | ) |
| void gpio_disable_pin_pull_up | ( | uint32_t | pin | ) |
| void gpio_enable_gpio | ( | const gpio_map_t | gpiomap, | |
| uint32_t | size | |||
| ) |
Enables the GPIO mode of a set of pins.
| gpiomap | The pin map. | |
| size | The number of pins in gpiomap. |
Definition at line 150 of file gpio.c.
References gpio_enable_gpio_pin(), and gpio_map_t::pin.
{
uint32_t i;
for (i = 0; i < size; i++)
{
gpio_enable_gpio_pin(gpiomap->pin);
gpiomap++;
}
}
| void gpio_enable_gpio_pin | ( | uint32_t | pin | ) |
Enables the GPIO mode of a pin.
| pin | The pin number. Refer to the product header file `uc3x.h' (where x is the part number; e.g. x = a0512) for pin definitions. E.g., to enable the GPIO mode of PX21, AVR32_PIN_PX21 can be used. Module pins such as AVR32_PWM_3_PIN for PWM channel 3 can also be used to release module pins for GPIO. |
Definition at line 162 of file gpio.c.
References GPIO.
Referenced by gpio_enable_gpio().
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->oderc = 1 << (pin & 0x1F);
gpio_port->gpers = 1 << (pin & 0x1F);
}
| int gpio_enable_module | ( | const gpio_map_t | gpiomap, | |
| uint32_t | size | |||
| ) |
Enables specific module modes for a set of pins.
| gpiomap | The pin map. | |
| size | The number of pins in gpiomap. |
Definition at line 59 of file gpio.c.
References gpio_map_t::function, gpio_enable_module_pin(), and gpio_map_t::pin.
{
int status = GPIO_SUCCESS;
uint32_t i;
for (i = 0; i < size; i++)
{
status |= gpio_enable_module_pin(gpiomap->pin, gpiomap->function);
gpiomap++;
}
return status;
}
| int gpio_enable_module_pin | ( | uint32_t | pin, | |
| uint32_t | function | |||
| ) |
Enables a specific module mode for a pin.
| pin | The pin number. Refer to the product header file `uc3x.h' (where x is the part number; e.g. x = a0512) for module pins. E.g., to enable a PWM channel output, the pin number can be AVR32_PWM_3_PIN for PWM channel 3. | |
| function | The pin function. Refer to the product header file `uc3x.h' (where x is the part number; e.g. x = a0512) for module pin functions. E.g., to enable a PWM channel output, the pin function can be AVR32_PWM_3_FUNCTION for PWM channel 3. |
Definition at line 74 of file gpio.c.
References GPIO.
Referenced by gpio_enable_module().
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
// Enable the correct function.
switch (function)
{
case 0: // A function.
gpio_port->pmr0c = 1 << (pin & 0x1F);
gpio_port->pmr1c = 1 << (pin & 0x1F);
#if defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
gpio_port->pmr2c = 1 << (pin & 0x1F);
#endif
break;
case 1: // B function.
gpio_port->pmr0s = 1 << (pin & 0x1F);
gpio_port->pmr1c = 1 << (pin & 0x1F);
#if defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
gpio_port->pmr2c = 1 << (pin & 0x1F);
#endif
break;
case 2: // C function.
gpio_port->pmr0c = 1 << (pin & 0x1F);
gpio_port->pmr1s = 1 << (pin & 0x1F);
#if defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
gpio_port->pmr2c = 1 << (pin & 0x1F);
#endif
break;
case 3: // D function.
gpio_port->pmr0s = 1 << (pin & 0x1F);
gpio_port->pmr1s = 1 << (pin & 0x1F);
#if defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
gpio_port->pmr2c = 1 << (pin & 0x1F);
#endif
break;
#if defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
case 4: // E function.
gpio_port->pmr0c = 1 << (pin & 0x1F);
gpio_port->pmr1c = 1 << (pin & 0x1F);
gpio_port->pmr2s = 1 << (pin & 0x1F);
break;
case 5: // F function.
gpio_port->pmr0s = 1 << (pin & 0x1F);
gpio_port->pmr1c = 1 << (pin & 0x1F);
gpio_port->pmr2s = 1 << (pin & 0x1F);
break;
case 6: // G function.
gpio_port->pmr0c = 1 << (pin & 0x1F);
gpio_port->pmr1s = 1 << (pin & 0x1F);
gpio_port->pmr2s = 1 << (pin & 0x1F);
break;
case 7: // H function.
gpio_port->pmr0s = 1 << (pin & 0x1F);
gpio_port->pmr1s = 1 << (pin & 0x1F);
gpio_port->pmr2s = 1 << (pin & 0x1F);
break;
#endif
default:
return GPIO_INVALID_ARGUMENT;
}
// Disable GPIO control.
gpio_port->gperc = 1 << (pin & 0x1F);
return GPIO_SUCCESS;
}
| void gpio_enable_pin_glitch_filter | ( | uint32_t | pin | ) |
Enables the glitch filter of a pin.
When the glitch filter is enabled, a glitch with duration of less than 1 clock cycle is automatically rejected, while a pulse with duration of 2 clock cycles or more is accepted. For pulse durations between 1 clock cycle and 2 clock cycles, the pulse may or may not be taken into account, depending on the precise timing of its occurrence. Thus for a pulse to be guaranteed visible it must exceed 2 clock cycles, whereas for a glitch to be reliably filtered out, its duration must not exceed 1 clock cycle. The filter introduces 2 clock cycles latency.
| pin | The pin number. |
Definition at line 522 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->gfers = 1 << (pin & 0x1F);
}
| int gpio_enable_pin_interrupt | ( | uint32_t | pin, | |
| uint32_t | mode | |||
| ) |
Enables the interrupt of a pin with the specified settings.
| pin | The pin number. | |
| mode | The trigger mode (GPIO_PIN_CHANGE, GPIO_RISING_EDGE or GPIO_FALLING_EDGE). |
Definition at line 573 of file gpio.c.
References GPIO, gpio_configure_edge_detector(), and GPIO_INVALID_ARGUMENT.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
// Enable the glitch filter.
gpio_port->gfers = 1 << (pin & 0x1F);
// Configure the edge detector.
if(GPIO_INVALID_ARGUMENT == gpio_configure_edge_detector(pin, mode))
return(GPIO_INVALID_ARGUMENT);
// Enable interrupt.
gpio_port->iers = 1 << (pin & 0x1F);
return GPIO_SUCCESS;
}
| void gpio_enable_pin_pull_up | ( | uint32_t | pin | ) |
Enables the pull-up resistor of a pin.
| pin | The pin number. |
Definition at line 197 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->puers = 1 << (pin & 0x1F);
#if defined(AVR32_GPIO_200_H_INCLUDED) || defined(AVR32_GPIO_210_H_INCLUDED) || defined(AVR32_GPIO_211_H_INCLUDED)
gpio_port->pderc = 1 << (pin & 0x1F);
#endif
}
| int gpio_get_gpio_open_drain_pin_output_value | ( | uint32_t | pin | ) |
Returns the output value set for a GPIO pin using open drain.
| pin | The pin number. |
Definition at line 425 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
return ((gpio_port->oder >> (pin & 0x1F)) & 1) ^ 1;
}
| int gpio_get_gpio_pin_output_value | ( | uint32_t | pin | ) |
Returns the output value set for a GPIO pin.
| pin | The pin number. |
Definition at line 418 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
return (gpio_port->ovr >> (pin & 0x1F)) & 1;
}
| int gpio_get_pin_interrupt_flag | ( | uint32_t | pin | ) |
| int gpio_get_pin_value | ( | uint32_t | pin | ) |
| void gpio_set_gpio_open_drain_pin | ( | uint32_t | pin | ) |
Drives a GPIO pin to 1 using open drain.
| pin | The pin number. |
Definition at line 493 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->oderc = 1 << (pin & 0x1F); // The GPIO output driver is disabled for that pin.
gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
}
| void gpio_set_gpio_pin | ( | uint32_t | pin | ) |
Drives a GPIO pin to 1.
| pin | The pin number. |
Definition at line 432 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrs = 1 << (pin & 0x1F); // Value to be driven on the I/O line: 1.
gpio_port->oders = 1 << (pin & 0x1F); // The GPIO output driver is enabled for that pin.
gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
}
| void gpio_set_group_high | ( | uint32_t | port, | |
| uint32_t | mask | |||
| ) |
| void gpio_set_group_low | ( | uint32_t | port, | |
| uint32_t | mask | |||
| ) |
| void gpio_set_pin_high | ( | uint32_t | pin | ) |
Drives a GPIO pin to 1.
| pin | The pin number. |
Definition at line 440 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrs = 1 << (pin & 0x1F); // Value to be driven on the I/O line: 1.
}
| void gpio_set_pin_low | ( | uint32_t | pin | ) |
Drives a GPIO pin to 0.
| pin | The pin number. |
Definition at line 453 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrc = 1 << (pin & 0x1F); // Value to be driven on the I/O line: 0.
}
| void gpio_tgl_gpio_open_drain_pin | ( | uint32_t | pin | ) |
Toggles a GPIO pin using open drain.
| pin | The pin number. |
Definition at line 512 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrc = 1 << (pin & 0x1F); // Value to be driven on the I/O line if the GPIO output driver is enabled: 0.
gpio_port->odert = 1 << (pin & 0x1F); // The GPIO output driver is toggled for that pin.
gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
}
| void gpio_tgl_gpio_pin | ( | uint32_t | pin | ) |
Toggles a GPIO pin.
| pin | The pin number. |
Definition at line 473 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrt = 1 << (pin & 0x1F); // Toggle the I/O line.
gpio_port->oders = 1 << (pin & 0x1F); // The GPIO output driver is enabled for that pin.
gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
}
| void gpio_toggle_group | ( | uint32_t | port, | |
| uint32_t | mask | |||
| ) |
| void gpio_toggle_pin | ( | uint32_t | pin | ) |
Toggles a GPIO pin.
| pin | The pin number. |
Definition at line 481 of file gpio.c.
References GPIO.
{
volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
gpio_port->ovrt = 1 << (pin & 0x1F); // Toggle the I/O line.
}
1.7.1