stringz.h File Reference


Detailed Description

Preprocessor stringizing utils.

Author:
Atmel Corporation: http://www.atmel.com
Support and FAQ: http://support.atmel.no/

Definition in file stringz.h.

This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Defines

#define ASTRINGZ(x)   STRINGZ(x)
 Absolute stringize.
#define STRINGZ(x)   #x
 Stringize.


Define Documentation

#define ASTRINGZ (  )     STRINGZ(x)

Absolute stringize.

Stringize a preprocessing token, this token being allowed to be #defined.

No restriction of use if the token is #defined.

For example, writing ASTRINGZ(PIN0) anywhere with PIN0 #defined as A0 is equivalent to writing "A0".

Definition at line 69 of file stringz.h.

#define STRINGZ (  )     #x

Stringize.

Stringize a preprocessing token, this token being allowed to be #defined.

May be used only within macros with the token passed as an argument if the token is #defined.

For example, writing STRINGZ(PIN) within a macro #defined by PIN_NAME(PIN) and invoked as PIN_NAME(PIN0) with PIN0 #defined as A0 is equivalent to writing "A0".

Definition at line 58 of file stringz.h.


Generated on Wed May 7 14:40:11 2008 for AVR32114 Using the AVR32 LCD Controller by  doxygen 1.5.3-20071008