Definition in file pm.h.
#include <avr32/io.h>
#include "compiler.h"
#include "preprocessor.h"
Go to the source code of this file.
Defines | |
| #define | SLEEP(mode) {__asm__ __volatile__ ("sleep "STRINGZ(mode));} |
| Sets the MCU in the specified sleep mode. | |
Functions | |
| void | pm_cksel (volatile avr32_pm_t *pm, unsigned int pbadiv, unsigned int pbasel, unsigned int pbbdiv, unsigned int pbbsel, unsigned int hsbdiv, unsigned int hsbsel) |
| This function will select all the power manager clocks. | |
| void | pm_disable_clk0 (volatile avr32_pm_t *pm) |
| This function will disable the oscillator 0. | |
| void | pm_disable_clk1 (volatile avr32_pm_t *pm) |
| This function will disable the oscillator 1. | |
| void | pm_disable_clk32 (volatile avr32_pm_t *pm) |
| This function will disable the oscillator 32. | |
| void | pm_enable_clk0 (volatile avr32_pm_t *pm, unsigned int startup) |
| This function will enable the oscillator 0 to be used with a startup time. | |
| void | pm_enable_clk0_no_wait (volatile avr32_pm_t *pm, unsigned int startup) |
| This function will enable the oscillator 0 to be used with no startup time. | |
| void | pm_enable_clk1 (volatile avr32_pm_t *pm, unsigned int startup) |
| This function will enable the oscillator 1 to be used with a startup time. | |
| void | pm_enable_clk1_no_wait (volatile avr32_pm_t *pm, unsigned int startup) |
| This function will enable the oscillator 1 to be used with no startup time. | |
| void | pm_enable_clk32 (volatile avr32_pm_t *pm, unsigned int startup) |
| This function will enable the oscillator 32 to be used with a startup time. | |
| void | pm_enable_clk32_no_wait (volatile avr32_pm_t *pm, unsigned int startup) |
| This function will enable the oscillator 32 to be used with no startup time. | |
| void | pm_enable_osc0_crystal (volatile avr32_pm_t *pm, unsigned int fosc0) |
| This function will enable the crystal mode of the oscillator 0. | |
| void | pm_enable_osc0_ext_clock (volatile avr32_pm_t *pm) |
| This function will enable the external clock mode of the oscillator 0. | |
| void | pm_enable_osc1_crystal (volatile avr32_pm_t *pm, unsigned int fosc1) |
| This function will enable the crystal mode of the oscillator 1. | |
| void | pm_enable_osc1_ext_clock (volatile avr32_pm_t *pm) |
| This function will enable the external clock mode of the oscillator 1. | |
| void | pm_enable_osc32_crystal (volatile avr32_pm_t *pm) |
| This function will enable the crystal mode of the 32-kHz oscillator. | |
| void | pm_enable_osc32_ext_clock (volatile avr32_pm_t *pm) |
| This function will enable the external clock mode of the 32-kHz oscillator. | |
| void | pm_gc_disable (volatile avr32_pm_t *pm, unsigned int gc) |
| This function will disable a generic clock. | |
| void | pm_gc_enable (volatile avr32_pm_t *pm, unsigned int gc) |
| This function will enable a generic clock. | |
| void | pm_gc_setup (volatile avr32_pm_t *pm, unsigned int gc, unsigned int osc_or_pll, unsigned int pll_osc, unsigned int diven, unsigned int div) |
| This function will setup a generic clock. | |
| __inline__ unsigned int | pm_get_reset_cause (volatile avr32_pm_t *pm) |
| Gets the MCU reset cause. | |
| void | pm_pll_disable (volatile avr32_pm_t *pm, unsigned int pll) |
| This function will disable a PLL. | |
| void | pm_pll_enable (volatile avr32_pm_t *pm, unsigned int pll) |
| This function will enable a PLL. | |
| unsigned int | pm_pll_get_option (volatile avr32_pm_t *pm, unsigned int pll) |
| This function will get a PLL option. | |
| void | pm_pll_set_option (volatile avr32_pm_t *pm, unsigned int pll, unsigned int pll_freq, unsigned int pll_div2, unsigned int pll_wbwdisable) |
| This function will set a PLL option. | |
| void | pm_pll_setup (volatile avr32_pm_t *pm, unsigned int pll, unsigned int mul, unsigned int div, unsigned int osc, unsigned int lockcount) |
| This function will setup a PLL. | |
| void | pm_switch_to_clock (volatile avr32_pm_t *pm, unsigned long clock) |
| This function will switch the power manager main clock. | |
| void | pm_switch_to_osc0 (volatile avr32_pm_t *pm, unsigned int fosc0, unsigned int startup) |
| Switch main clock to clock Osc0 (crystal mode). | |
| void | pm_wait_for_clk0_ready (volatile avr32_pm_t *pm) |
| This function will wait until the Osc0 clock is ready. | |
| void | pm_wait_for_clk1_ready (volatile avr32_pm_t *pm) |
| This function will wait until the Osc1 clock is ready. | |
| void | pm_wait_for_clk32_ready (volatile avr32_pm_t *pm) |
| This function will wait until the osc32 clock is ready. | |
| void | pm_wait_for_pll0_locked (volatile avr32_pm_t *pm) |
| This function will wait for PLL0 locked. | |
| void | pm_wait_for_pll1_locked (volatile avr32_pm_t *pm) |
| This function will wait for PLL1 locked. | |
| #define SLEEP | ( | mode | ) | {__asm__ __volatile__ ("sleep "STRINGZ(mode));} |
Sets the MCU in the specified sleep mode.
| mode | Sleep mode:
|
Definition at line 64 of file pm.h.
Referenced by main().
| void pm_cksel | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | pbadiv, | |||
| unsigned int | pbasel, | |||
| unsigned int | pbbdiv, | |||
| unsigned int | pbbsel, | |||
| unsigned int | hsbdiv, | |||
| unsigned int | hsbsel | |||
| ) |
This function will select all the power manager clocks.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| pbadiv | Peripheral Bus A clock divisor enable | |
| pbasel | Peripheral Bus A select | |
| pbbdiv | Peripheral Bus B clock divisor enable | |
| pbbsel | Peripheral Bus B select | |
| hsbdiv | High Speed Bus clock divisor enable (CPU clock = HSB clock) | |
| hsbsel | High Speed Bus select (CPU clock = HSB clock ) |
Definition at line 321 of file pm.c.
References u_avr32_pm_cksel_t::cksel, and u_avr32_pm_cksel_t::CKSEL.
Referenced by main().
00328 { 00329 u_avr32_pm_cksel_t u_avr32_pm_cksel = {0}; 00330 00331 u_avr32_pm_cksel.CKSEL.cpusel = hsbsel; 00332 u_avr32_pm_cksel.CKSEL.cpudiv = hsbdiv; 00333 u_avr32_pm_cksel.CKSEL.hsbsel = hsbsel; 00334 u_avr32_pm_cksel.CKSEL.hsbdiv = hsbdiv; 00335 u_avr32_pm_cksel.CKSEL.pbasel = pbasel; 00336 u_avr32_pm_cksel.CKSEL.pbadiv = pbadiv; 00337 u_avr32_pm_cksel.CKSEL.pbbsel = pbbsel; 00338 u_avr32_pm_cksel.CKSEL.pbbdiv = pbbdiv; 00339 00340 pm->cksel = u_avr32_pm_cksel.cksel; 00341 00342 // Wait for ckrdy bit and then clear it 00343 while (!(pm->poscsr & AVR32_PM_POSCSR_CKRDY_MASK)); 00344 }
| void pm_disable_clk0 | ( | volatile avr32_pm_t * | pm | ) |
| void pm_disable_clk1 | ( | volatile avr32_pm_t * | pm | ) |
| void pm_disable_clk32 | ( | volatile avr32_pm_t * | pm | ) |
| void pm_enable_clk0 | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | startup | |||
| ) |
This function will enable the oscillator 0 to be used with a startup time.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| startup | Clock 0 startup time. Time is expressed in term of RCOsc periods (3-bit value) |
Definition at line 169 of file pm.c.
References pm_enable_clk0_no_wait(), and pm_wait_for_clk0_ready().
Referenced by pm_switch_to_osc0().
00170 { 00171 pm_enable_clk0_no_wait(pm, startup); 00172 pm_wait_for_clk0_ready(pm); 00173 }
| void pm_enable_clk0_no_wait | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | startup | |||
| ) |
This function will enable the oscillator 0 to be used with no startup time.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| startup | Clock 0 startup time. Time is expressed in term of RCOsc periods (3-bit value) but not checked. |
Definition at line 182 of file pm.c.
References u_avr32_pm_oscctrl0_t::oscctrl0, and u_avr32_pm_oscctrl0_t::OSCCTRL0.
Referenced by pm_enable_clk0().
00183 { 00184 // Read register 00185 u_avr32_pm_oscctrl0_t u_avr32_pm_oscctrl0 = {pm->oscctrl0}; 00186 // Modify 00187 u_avr32_pm_oscctrl0.OSCCTRL0.startup = startup; 00188 // Write back 00189 pm->oscctrl0 = u_avr32_pm_oscctrl0.oscctrl0; 00190 00191 pm->mcctrl |= AVR32_PM_MCCTRL_OSC0EN_MASK; 00192 }
| void pm_enable_clk1 | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | startup | |||
| ) |
This function will enable the oscillator 1 to be used with a startup time.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| startup | Clock 1 startup time. Time is expressed in term of RCOsc periods (3-bit value) |
Definition at line 230 of file pm.c.
References pm_enable_clk1_no_wait(), and pm_wait_for_clk1_ready().
00231 { 00232 pm_enable_clk1_no_wait(pm, startup); 00233 pm_wait_for_clk1_ready(pm); 00234 }
| void pm_enable_clk1_no_wait | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | startup | |||
| ) |
This function will enable the oscillator 1 to be used with no startup time.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| startup | Clock 1 startup time. Time is expressed in term of RCOsc periods (3-bit value) but not checked. |
Definition at line 243 of file pm.c.
References u_avr32_pm_oscctrl1_t::oscctrl1, and u_avr32_pm_oscctrl1_t::OSCCTRL1.
Referenced by pm_enable_clk1().
00244 { 00245 // Read register 00246 u_avr32_pm_oscctrl1_t u_avr32_pm_oscctrl1 = {pm->oscctrl1}; 00247 // Modify 00248 u_avr32_pm_oscctrl1.OSCCTRL1.startup = startup; 00249 // Write back 00250 pm->oscctrl1 = u_avr32_pm_oscctrl1.oscctrl1; 00251 00252 pm->mcctrl |= AVR32_PM_MCCTRL_OSC1EN_MASK; 00253 }
| void pm_enable_clk32 | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | startup | |||
| ) |
This function will enable the oscillator 32 to be used with a startup time.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| startup | Clock 32 kHz startup time. Time is expressed in term of RCOsc periods (3-bit value) |
Definition at line 290 of file pm.c.
References pm_enable_clk32_no_wait(), and pm_wait_for_clk32_ready().
00291 { 00292 pm_enable_clk32_no_wait(pm, startup); 00293 pm_wait_for_clk32_ready(pm); 00294 }
| void pm_enable_clk32_no_wait | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | startup | |||
| ) |
This function will enable the oscillator 32 to be used with no startup time.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| startup | Clock 32 kHz startup time. Time is expressed in term of RCOsc periods (3-bit value) but not checked. |
Definition at line 303 of file pm.c.
References u_avr32_pm_oscctrl32_t::oscctrl32, and u_avr32_pm_oscctrl32_t::OSCCTRL32.
Referenced by pm_enable_clk32(), and rtc_init().
00304 { 00305 // Read register 00306 u_avr32_pm_oscctrl32_t u_avr32_pm_oscctrl32 = {pm->oscctrl32}; 00307 // Modify 00308 u_avr32_pm_oscctrl32.OSCCTRL32.osc32en = 1; 00309 u_avr32_pm_oscctrl32.OSCCTRL32.startup = startup; 00310 // Write back 00311 pm->oscctrl32 = u_avr32_pm_oscctrl32.oscctrl32; 00312 }
| void pm_enable_osc0_crystal | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | fosc0 | |||
| ) |
This function will enable the crystal mode of the oscillator 0.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| fosc0 | Oscillator 0 crystal frequency (Hz) |
Definition at line 162 of file pm.c.
References pm_set_osc0_mode().
Referenced by pm_switch_to_osc0().
00163 { 00164 pm_set_osc0_mode(pm, (fosc0 < 8000000) ? AVR32_PM_OSCCTRL0_MODE_CRYSTAL_G2 : 00165 AVR32_PM_OSCCTRL0_MODE_CRYSTAL_G3); 00166 }
| void pm_enable_osc0_ext_clock | ( | volatile avr32_pm_t * | pm | ) |
This function will enable the external clock mode of the oscillator 0.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 156 of file pm.c.
References pm_set_osc0_mode().
00157 { 00158 pm_set_osc0_mode(pm, AVR32_PM_OSCCTRL0_MODE_EXT_CLOCK); 00159 }
| void pm_enable_osc1_crystal | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | fosc1 | |||
| ) |
This function will enable the crystal mode of the oscillator 1.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| fosc1 | Oscillator 1 crystal frequency (Hz) |
Definition at line 223 of file pm.c.
References pm_set_osc1_mode().
00224 { 00225 pm_set_osc1_mode(pm, (fosc1 < 8000000) ? AVR32_PM_OSCCTRL1_MODE_CRYSTAL_G2 : 00226 AVR32_PM_OSCCTRL1_MODE_CRYSTAL_G3); 00227 }
| void pm_enable_osc1_ext_clock | ( | volatile avr32_pm_t * | pm | ) |
This function will enable the external clock mode of the oscillator 1.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 217 of file pm.c.
References pm_set_osc1_mode().
00218 { 00219 pm_set_osc1_mode(pm, AVR32_PM_OSCCTRL1_MODE_EXT_CLOCK); 00220 }
| void pm_enable_osc32_crystal | ( | volatile avr32_pm_t * | pm | ) |
This function will enable the crystal mode of the 32-kHz oscillator.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 284 of file pm.c.
References pm_set_osc32_mode().
Referenced by rtc_init().
00285 { 00286 pm_set_osc32_mode(pm, AVR32_PM_OSCCTRL32_MODE_CRYSTAL); 00287 }
| void pm_enable_osc32_ext_clock | ( | volatile avr32_pm_t * | pm | ) |
This function will enable the external clock mode of the 32-kHz oscillator.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 278 of file pm.c.
References pm_set_osc32_mode().
00279 { 00280 pm_set_osc32_mode(pm, AVR32_PM_OSCCTRL32_MODE_EXT_CLOCK); 00281 }
| void pm_gc_disable | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | gc | |||
| ) |
| void pm_gc_enable | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | gc | |||
| ) |
| void pm_gc_setup | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | gc, | |||
| unsigned int | osc_or_pll, | |||
| unsigned int | pll_osc, | |||
| unsigned int | diven, | |||
| unsigned int | div | |||
| ) |
This function will setup a generic clock.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| gc | generic clock number (0 for gc0...) | |
| osc_or_pll | Use OSC (=0) or PLL (=1) | |
| pll_osc | Select Osc0/PLL0 or Osc1/PLL1 | |
| diven | Generic clock divisor enable | |
| div | Generic clock divisor |
Definition at line 347 of file pm.c.
References u_avr32_pm_gcctrl_t::gcctrl, and u_avr32_pm_gcctrl_t::GCCTRL.
00353 { 00354 u_avr32_pm_gcctrl_t u_avr32_pm_gcctrl = {0}; 00355 00356 u_avr32_pm_gcctrl.GCCTRL.oscsel = pll_osc; 00357 u_avr32_pm_gcctrl.GCCTRL.pllsel = osc_or_pll; 00358 u_avr32_pm_gcctrl.GCCTRL.diven = diven; 00359 u_avr32_pm_gcctrl.GCCTRL.div = div; 00360 00361 pm->gcctrl[gc] = u_avr32_pm_gcctrl.gcctrl; 00362 }
| __inline__ unsigned int pm_get_reset_cause | ( | volatile avr32_pm_t * | pm | ) |
| void pm_pll_disable | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | pll | |||
| ) |
| void pm_pll_enable | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | pll | |||
| ) |
| unsigned int pm_pll_get_option | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | pll | |||
| ) |
| void pm_pll_set_option | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | pll, | |||
| unsigned int | pll_freq, | |||
| unsigned int | pll_div2, | |||
| unsigned int | pll_wbwdisable | |||
| ) |
This function will set a PLL option.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| pll | PLL number(0 for PLL0, 1 for PLL1) | |
| pll_freq | Set to 1 for VCO frequency range 80-180MHz, set to 0 for VCO frequency range 160-240Mhz. | |
| pll_div2 | Divide the PLL output frequency by 2 (this settings does not change the FVCO value) | |
| pll_wbwdisable | 1 Disable the Wide-Bandith Mode (Wide-Bandwith mode allow a faster startup time and out-of-lock time). 0 to enable the Wide-Bandith Mode. |
Definition at line 397 of file pm.c.
References u_avr32_pm_pll_t::pll, and u_avr32_pm_pll_t::PLL.
00402 { 00403 u_avr32_pm_pll_t u_avr32_pm_pll = {pm->pll[pll]}; 00404 u_avr32_pm_pll.PLL.pllopt = pll_freq | (pll_div2 << 1) | (pll_wbwdisable << 2); 00405 pm->pll[pll] = u_avr32_pm_pll.pll; 00406 }
| void pm_pll_setup | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | pll, | |||
| unsigned int | mul, | |||
| unsigned int | div, | |||
| unsigned int | osc, | |||
| unsigned int | lockcount | |||
| ) |
This function will setup a PLL.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| pll | PLL number(0 for PLL0, 1 for PLL1) | |
| mul | ||
| div | ||
| osc | ||
| lockcount |
Definition at line 379 of file pm.c.
References u_avr32_pm_pll_t::pll, and u_avr32_pm_pll_t::PLL.
00385 { 00386 u_avr32_pm_pll_t u_avr32_pm_pll = {0}; 00387 00388 u_avr32_pm_pll.PLL.pllosc = osc; 00389 u_avr32_pm_pll.PLL.plldiv = div; 00390 u_avr32_pm_pll.PLL.pllmul = mul; 00391 u_avr32_pm_pll.PLL.pllcount = lockcount; 00392 00393 pm->pll[pll] = u_avr32_pm_pll.pll; 00394 }
| void pm_switch_to_clock | ( | volatile avr32_pm_t * | pm, | |
| unsigned long | clock | |||
| ) |
This function will switch the power manager main clock.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| clock | Clock to be switched on. AVR32_PM_MCSEL_SLOW for RCOsc, AVR32_PM_MCSEL_OSC0 for Osc0, AVR32_PM_MCSEL_PLL0 for PLL0. |
Definition at line 448 of file pm.c.
References u_avr32_pm_mcctrl_t::mcctrl, and u_avr32_pm_mcctrl_t::MCCTRL.
Referenced by pm_switch_to_osc0().
00449 { 00450 // Read 00451 u_avr32_pm_mcctrl_t u_avr32_pm_mcctrl = {pm->mcctrl}; 00452 // Modify 00453 u_avr32_pm_mcctrl.MCCTRL.mcsel = clock; 00454 // Write back 00455 pm->mcctrl = u_avr32_pm_mcctrl.mcctrl; 00456 }
| void pm_switch_to_osc0 | ( | volatile avr32_pm_t * | pm, | |
| unsigned int | fosc0, | |||
| unsigned int | startup | |||
| ) |
Switch main clock to clock Osc0 (crystal mode).
| pm | Base address of the Power Manager (i.e. &AVR32_PM) | |
| fosc0 | Oscillator 0 crystal frequency (Hz) | |
| startup | Crystal 0 startup time. Time is expressed in term of RCOsc periods (3-bit value) |
Definition at line 459 of file pm.c.
References pm_enable_clk0(), pm_enable_osc0_crystal(), and pm_switch_to_clock().
Referenced by main().
00460 { 00461 pm_enable_osc0_crystal(pm, fosc0); // Enable the Osc0 in crystal mode 00462 pm_enable_clk0(pm, startup); // Crystal startup time - This parameter is critical and depends on the characteristics of the crystal 00463 pm_switch_to_clock(pm, AVR32_PM_MCSEL_OSC0); // Then switch main clock to Osc0 00464 }
| void pm_wait_for_clk0_ready | ( | volatile avr32_pm_t * | pm | ) |
This function will wait until the Osc0 clock is ready.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 195 of file pm.c.
Referenced by pm_enable_clk0().
| void pm_wait_for_clk1_ready | ( | volatile avr32_pm_t * | pm | ) |
This function will wait until the Osc1 clock is ready.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 256 of file pm.c.
Referenced by pm_enable_clk1().
| void pm_wait_for_clk32_ready | ( | volatile avr32_pm_t * | pm | ) |
This function will wait until the osc32 clock is ready.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 315 of file pm.c.
Referenced by pm_enable_clk32().
| void pm_wait_for_pll0_locked | ( | volatile avr32_pm_t * | pm | ) |
This function will wait for PLL0 locked.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 430 of file pm.c.
00431 { 00432 while (!(pm->poscsr & AVR32_PM_POSCSR_LOCK0_MASK)); 00433 00434 // Bypass the lock signal of the PLL 00435 pm->pll[0] |= AVR32_PM_PLL0_PLLBPL_MASK; 00436 }
| void pm_wait_for_pll1_locked | ( | volatile avr32_pm_t * | pm | ) |
This function will wait for PLL1 locked.
| pm | Base address of the Power Manager (i.e. &AVR32_PM) |
Definition at line 439 of file pm.c.
00440 { 00441 while (!(pm->poscsr & AVR32_PM_POSCSR_LOCK1_MASK)); 00442 00443 // Bypass the lock signal of the PLL 00444 pm->pll[1] |= AVR32_PM_PLL1_PLLBPL_MASK; 00445 }
1.5.3-20071008