Graph Legend

This page explains how to interpret the graphs that are generated by doxygen.

Consider the following example:

/*! Invisible class because of truncation */
class Invisible { };

/*! Truncated class, inheritance relation is hidden */
class Truncated : public Invisible { };

/* Class not documented with doxygen comments */
class Undocumented { };

/*! Class that is inherited using public inheritance */
class PublicBase : public Truncated { };

/*! A template class */
template<class T> class Templ { };

/*! Class that is inherited using protected inheritance */
class ProtectedBase { };

/*! Class that is inherited using private inheritance */
class PrivateBase { };

/*! Class that is used by the Inherited class */
class Used { };

/*! Super class that inherits a number of other classes */
class Inherited : public PublicBase,
                  protected ProtectedBase,
                  private PrivateBase,
                  public Undocumented,
                  public Templ<int>
{
  private:
    Used *m_usedClass;
};
If the MAX_DOT_GRAPH_HEIGHT tag in the configuration file is set to 240 this will result in the following graph:

graph_legend.png

The boxes in the above graph have the following meaning:

The arrows have the following meaning:
Generated on Wed May 7 14:40:11 2008 for AVR32114 Using the AVR32 LCD Controller by  doxygen 1.5.3-20071008