gpio.c File Reference


Detailed Description

GPIO driver for AVR32 UC3.

This file defines a useful set of functions for the GPIO.

Author:
Atmel Corporation: http://www.atmel.com
Support and FAQ: http://support.atmel.no/

Definition in file gpio.c.

#include "gpio.h"

Include dependency graph for gpio.c:

Go to the source code of this file.

Defines

#define GPIO   AVR32_GPIO
 GPIO module instance.

Functions

void gpio_clear_pin_interrupt_flag (unsigned int pin)
 Clears the interrupt flag of a pin.
void gpio_clr_gpio_pin (unsigned int pin)
 Drives a GPIO pin to 0.
void gpio_disable_pin_glitch_filter (unsigned int pin)
 Disables the glitch filter of a pin.
void gpio_disable_pin_interrupt (unsigned int pin)
 Disables the interrupt of a pin.
void gpio_disable_pin_open_drain (unsigned int pin)
 Disables the open-drain mode of a pin.
void gpio_disable_pin_pull_up (unsigned int pin)
 Disables the pull-up resistor of a pin.
void gpio_enable_gpio (const gpio_map_t gpiomap, unsigned int size)
 Enables the GPIO mode of a set of pins.
void gpio_enable_gpio_pin (unsigned int pin)
 Enables the GPIO mode of a pin.
int gpio_enable_module (const gpio_map_t gpiomap, unsigned int size)
 Enables specific module modes for a set of pins.
int gpio_enable_module_pin (unsigned int pin, unsigned int function)
 Enables a specific module mode for a pin.
void gpio_enable_pin_glitch_filter (unsigned int pin)
 Enables the glitch filter of a pin.
int gpio_enable_pin_interrupt (unsigned int pin, unsigned int mode)
 Enables the interrupt of a pin with the specified settings.
void gpio_enable_pin_open_drain (unsigned int pin)
 Enables the open-drain mode of a pin.
void gpio_enable_pin_pull_up (unsigned int pin)
 Enables the pull-up resistor of a pin.
int gpio_get_gpio_pin_output_value (unsigned int pin)
 Returns the output value set for a GPIO pin.
int gpio_get_pin_interrupt_flag (unsigned int pin)
 Gets the interrupt flag of a pin.
int gpio_get_pin_value (unsigned int pin)
 Returns the value of a pin.
void gpio_set_gpio_pin (unsigned int pin)
 Drives a GPIO pin to 1.
void gpio_tgl_gpio_pin (unsigned int pin)
 Toggles a GPIO pin.


Define Documentation

#define GPIO   AVR32_GPIO

GPIO module instance.

Definition at line 51 of file gpio.c.

Referenced by gpio_clear_pin_interrupt_flag(), gpio_clr_gpio_pin(), gpio_disable_pin_glitch_filter(), gpio_disable_pin_interrupt(), gpio_disable_pin_open_drain(), gpio_disable_pin_pull_up(), gpio_enable_gpio_pin(), gpio_enable_module_pin(), gpio_enable_pin_glitch_filter(), gpio_enable_pin_interrupt(), gpio_enable_pin_open_drain(), gpio_enable_pin_pull_up(), gpio_get_gpio_pin_output_value(), gpio_get_pin_interrupt_flag(), gpio_get_pin_value(), gpio_set_gpio_pin(), and gpio_tgl_gpio_pin().


Function Documentation

void gpio_clear_pin_interrupt_flag ( unsigned int  pin  ) 

Clears the interrupt flag of a pin.

Parameters:
pin The pin number.

Definition at line 258 of file gpio.c.

References GPIO.

00259 {
00260   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00261   gpio_port->ifrc = 1 << (pin & 0x1F);
00262 }

void gpio_clr_gpio_pin ( unsigned int  pin  ) 

Drives a GPIO pin to 0.

Parameters:
pin The pin number.

Definition at line 174 of file gpio.c.

References GPIO.

Referenced by main().

00175 {
00176   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00177 
00178   gpio_port->ovrc  = 1 << (pin & 0x1F); // Value to be driven on the I/O line: 0.
00179   gpio_port->oders = 1 << (pin & 0x1F); // The GPIO output driver is enabled for that pin.
00180   gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
00181 }

void gpio_disable_pin_glitch_filter ( unsigned int  pin  ) 

Disables the glitch filter of a pin.

Parameters:
pin The pin number.

Definition at line 201 of file gpio.c.

References GPIO.

00202 {
00203   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00204   gpio_port->gferc = 1 << (pin & 0x1F);
00205 }

void gpio_disable_pin_interrupt ( unsigned int  pin  ) 

Disables the interrupt of a pin.

Parameters:
pin The pin number.

Definition at line 244 of file gpio.c.

References GPIO.

00245 {
00246   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00247   gpio_port->ierc = 1 << (pin & 0x1F);
00248 }

void gpio_disable_pin_open_drain ( unsigned int  pin  ) 

Disables the open-drain mode of a pin.

Parameters:
pin The pin number.

Definition at line 129 of file gpio.c.

References GPIO.

00130 {
00131   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00132   gpio_port->odmerc = 1 << (pin & 0x1F);
00133 }

void gpio_disable_pin_pull_up ( unsigned int  pin  ) 

Disables the pull-up resistor of a pin.

Parameters:
pin The pin number.

Definition at line 143 of file gpio.c.

References GPIO.

00144 {
00145   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00146   gpio_port->puerc = 1 << (pin & 0x1F);
00147 }

void gpio_enable_gpio ( const gpio_map_t  gpiomap,
unsigned int  size 
)

Enables the GPIO mode of a set of pins.

Parameters:
gpiomap The pin map.
size The number of pins in gpiomap.

Definition at line 102 of file gpio.c.

References gpio_enable_gpio_pin(), and gpio_map_t::pin.

00103 {
00104   unsigned int i;
00105 
00106   for (i = 0; i < size; i++)
00107   {
00108     gpio_enable_gpio_pin(gpiomap->pin);
00109     gpiomap++;
00110   }
00111 }

Here is the call graph for this function:

void gpio_enable_gpio_pin ( unsigned int  pin  ) 

Enables the GPIO mode of a pin.

Parameters:
pin The pin number.
Refer to the product header file `uc3x.h' (where x is the part number; e.g. x = a0512) for pin definitions. E.g., to enable the GPIO mode of PX21, AVR32_PIN_PX21 can be used. Module pins such as AVR32_PWM_PWM_3_PIN for PWM channel 3 can also be used to release module pins for GPIO.

Definition at line 114 of file gpio.c.

References GPIO.

Referenced by gpio_enable_gpio().

00115 {
00116   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00117   gpio_port->oderc = 1 << (pin & 0x1F);
00118   gpio_port->gpers = 1 << (pin & 0x1F);
00119 }

int gpio_enable_module ( const gpio_map_t  gpiomap,
unsigned int  size 
)

Enables specific module modes for a set of pins.

Parameters:
gpiomap The pin map.
size The number of pins in gpiomap.
Returns:
GPIO_SUCCESS or GPIO_INVALID_ARGUMENT.

Definition at line 54 of file gpio.c.

References gpio_map_t::function, gpio_enable_module_pin(), GPIO_SUCCESS, and gpio_map_t::pin.

00055 {
00056   int status = GPIO_SUCCESS;
00057   unsigned int i;
00058 
00059   for (i = 0; i < size; i++)
00060   {
00061     status |= gpio_enable_module_pin(gpiomap->pin, gpiomap->function);
00062     gpiomap++;
00063   }
00064 
00065   return status;
00066 }

Here is the call graph for this function:

int gpio_enable_module_pin ( unsigned int  pin,
unsigned int  function 
)

Enables a specific module mode for a pin.

Parameters:
pin The pin number.
Refer to the product header file `uc3x.h' (where x is the part number; e.g. x = a0512) for module pins. E.g., to enable a PWM channel output, the pin number can be AVR32_PWM_PWM_3_PIN for PWM channel 3.
function The pin function.
Refer to the product header file `uc3x.h' (where x is the part number; e.g. x = a0512) for module pin functions. E.g., to enable a PWM channel output, the pin function can be AVR32_PWM_PWM_3_FUNCTION for PWM channel 3.
Returns:
GPIO_SUCCESS or GPIO_INVALID_ARGUMENT.

Definition at line 69 of file gpio.c.

References GPIO, GPIO_INVALID_ARGUMENT, and GPIO_SUCCESS.

Referenced by gpio_enable_module().

00070 {
00071   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00072 
00073   // Enable the correct function.
00074   switch (function)
00075   {
00076   case 0: // A function.
00077     gpio_port->pmr0c = 1 << (pin & 0x1F);
00078     gpio_port->pmr1c = 1 << (pin & 0x1F);
00079     break;
00080 
00081   case 1: // B function.
00082     gpio_port->pmr0s = 1 << (pin & 0x1F);
00083     gpio_port->pmr1c = 1 << (pin & 0x1F);
00084     break;
00085 
00086   case 2: // C function.
00087     gpio_port->pmr0c = 1 << (pin & 0x1F);
00088     gpio_port->pmr1s = 1 << (pin & 0x1F);
00089     break;
00090 
00091   default:
00092     return GPIO_INVALID_ARGUMENT;
00093   }
00094 
00095   // Disable GPIO control.
00096   gpio_port->gperc = 1 << (pin & 0x1F);
00097 
00098   return GPIO_SUCCESS;
00099 }

void gpio_enable_pin_glitch_filter ( unsigned int  pin  ) 

Enables the glitch filter of a pin.

When the glitch filter is enabled, a glitch with duration of less than 1 clock cycle is automatically rejected, while a pulse with duration of 2 clock cycles or more is accepted. For pulse durations between 1 clock cycle and 2 clock cycles, the pulse may or may not be taken into account, depending on the precise timing of its occurrence. Thus for a pulse to be guaranteed visible it must exceed 2 clock cycles, whereas for a glitch to be reliably filtered out, its duration must not exceed 1 clock cycle. The filter introduces 2 clock cycles latency.

Parameters:
pin The pin number.

Definition at line 194 of file gpio.c.

References GPIO.

00195 {
00196   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00197   gpio_port->gfers = 1 << (pin & 0x1F);
00198 }

int gpio_enable_pin_interrupt ( unsigned int  pin,
unsigned int  mode 
)

Enables the interrupt of a pin with the specified settings.

Parameters:
pin The pin number.
mode The trigger mode (GPIO_PIN_CHANGE, GPIO_RISING_EDGE or GPIO_FALLING_EDGE).
Returns:
GPIO_SUCCESS or GPIO_INVALID_ARGUMENT.

Definition at line 208 of file gpio.c.

References GPIO, GPIO_FALLING_EDGE, GPIO_INVALID_ARGUMENT, GPIO_PIN_CHANGE, GPIO_RISING_EDGE, and GPIO_SUCCESS.

00209 {
00210   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00211 
00212   // Enable the glitch filter.
00213   gpio_port->gfers = 1 << (pin & 0x1F);
00214 
00215   // Configure the edge detector.
00216   switch (mode)
00217   {
00218   case GPIO_PIN_CHANGE:
00219     gpio_port->imr0c = 1 << (pin & 0x1F);
00220     gpio_port->imr1c = 1 << (pin & 0x1F);
00221     break;
00222 
00223   case GPIO_RISING_EDGE:
00224     gpio_port->imr0s = 1 << (pin & 0x1F);
00225     gpio_port->imr1c = 1 << (pin & 0x1F);
00226     break;
00227 
00228   case GPIO_FALLING_EDGE:
00229     gpio_port->imr0c = 1 << (pin & 0x1F);
00230     gpio_port->imr1s = 1 << (pin & 0x1F);
00231     break;
00232 
00233   default:
00234     return GPIO_INVALID_ARGUMENT;
00235   }
00236 
00237   // Enable interrupt.
00238   gpio_port->iers = 1 << (pin & 0x1F);
00239 
00240   return GPIO_SUCCESS;
00241 }

void gpio_enable_pin_open_drain ( unsigned int  pin  ) 

Enables the open-drain mode of a pin.

Parameters:
pin The pin number.

Definition at line 122 of file gpio.c.

References GPIO.

00123 {
00124   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00125   gpio_port->odmers = 1 << (pin & 0x1F);
00126 }

void gpio_enable_pin_pull_up ( unsigned int  pin  ) 

Enables the pull-up resistor of a pin.

Parameters:
pin The pin number.

Definition at line 136 of file gpio.c.

References GPIO.

00137 {
00138   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00139   gpio_port->puers = 1 << (pin & 0x1F);
00140 }

int gpio_get_gpio_pin_output_value ( unsigned int  pin  ) 

Returns the output value set for a GPIO pin.

Parameters:
pin The pin number.
Returns:
The pin output value.

Definition at line 157 of file gpio.c.

References GPIO.

00158 {
00159   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00160   return (gpio_port->ovr >> (pin & 0x1F)) & 1;
00161 }

int gpio_get_pin_interrupt_flag ( unsigned int  pin  ) 

Gets the interrupt flag of a pin.

Parameters:
pin The pin number.
Returns:
The pin interrupt flag.

Definition at line 251 of file gpio.c.

References GPIO.

00252 {
00253   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00254   return (gpio_port->ifr >> (pin & 0x1F)) & 1;
00255 }

int gpio_get_pin_value ( unsigned int  pin  ) 

Returns the value of a pin.

Parameters:
pin The pin number.
Returns:
The pin value.

Definition at line 150 of file gpio.c.

References GPIO.

Referenced by main().

00151 {
00152   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00153   return (gpio_port->pvr >> (pin & 0x1F)) & 1;
00154 }

void gpio_set_gpio_pin ( unsigned int  pin  ) 

Drives a GPIO pin to 1.

Parameters:
pin The pin number.

Definition at line 164 of file gpio.c.

References GPIO.

Referenced by main().

00165 {
00166   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00167 
00168   gpio_port->ovrs  = 1 << (pin & 0x1F); // Value to be driven on the I/O line: 1.
00169   gpio_port->oders = 1 << (pin & 0x1F); // The GPIO output driver is enabled for that pin.
00170   gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
00171 }

void gpio_tgl_gpio_pin ( unsigned int  pin  ) 

Toggles a GPIO pin.

Parameters:
pin The pin number.

Definition at line 184 of file gpio.c.

References GPIO.

00185 {
00186   volatile avr32_gpio_port_t *gpio_port = &GPIO.port[pin >> 5];
00187 
00188   gpio_port->ovrt  = 1 << (pin & 0x1F); // Toggle the I/O line.
00189   gpio_port->oders = 1 << (pin & 0x1F); // The GPIO output driver is enabled for that pin.
00190   gpio_port->gpers = 1 << (pin & 0x1F); // The GPIO module controls that pin.
00191 }


Generated on Wed May 7 14:40:10 2008 for AVR32114 Using the AVR32 LCD Controller by  doxygen 1.5.3-20071008