Defines | |
| #define | Usb_send_event(x) (g_usb_event |= (1<<x)) |
| #define | Usb_ack_event(x) (g_usb_event &= ~(1<<x)) |
| #define | Usb_clear_all_event() (g_usb_event = 0) |
| #define | Is_usb_event(x) ((g_usb_event & (1<<x)) ? TRUE : FALSE) |
| #define | Is_not_usb_event(x) ((g_usb_event & (1<<x)) ? FALSE: TRUE) |
| #define | Is_host_emergency_exit() (Is_usb_id_device()||(device_state==DEVICE_DISCONNECTED)) |
| #define | Is_usb_device() (g_usb_mode==USB_MODE_DEVICE ? TRUE : FALSE) |
| #define | Is_usb_host() (g_usb_mode==USB_MODE_HOST ? TRUE : FALSE) |
| #define | Otg_send_event(x) (g_otg_event |= (1<<x)) |
| #define | Otg_ack_event(x) (g_otg_event &= ~(1<<x)) |
| #define | Otg_clear_all_event() (g_otg_event = 0) |
| #define | Is_otg_event(x) ((g_otg_event & (1<<x)) ? TRUE : FALSE) |
| #define | Is_not_otg_event(x) ((g_otg_event & (1<<x)) ? FALSE: TRUE) |
| #define | EVT_USB_POWERED 1 |
| #define | EVT_USB_UNPOWERED 2 |
| #define | EVT_USB_DEVICE_FUNCTION 3 |
| #define | EVT_USB_HOST_FUNCTION 4 |
| #define | EVT_USB_SUSPEND 5 |
| #define | EVT_USB_WAKE_UP 6 |
| #define | EVT_USB_RESUME 7 |
| #define | EVT_USB_RESET 8 |
| #define | EVT_HOST_SOF 9 |
| #define | EVT_HOST_HWUP 10 |
| #define | EVT_HOST_DISCONNECTION 11 |
| #define | EVT_HOST_REMOTE_WAKEUP 12 |
| #define | EVT_OTG_HNP_ERROR 1 |
| #define | EVT_OTG_HNP_SUCCESS 2 |
| #define | EVT_OTG_SRP_RECEIVED 3 |
| #define | EVT_OTG_DEV_UNSUPPORTED 4 |
| #define | EVT_OTG_DEVICE_CONNECTED 5 |
| #define Usb_send_event | ( | x | ) | (g_usb_event |= (1<<x)) |
Definition at line 60 of file usb_task.h.
Referenced by usb_device_task(), and usb_general_interrupt().
| #define Usb_ack_event | ( | x | ) | (g_usb_event &= ~(1<<x)) |
Definition at line 61 of file usb_task.h.
Referenced by host_send_control(), host_send_data(), usb_device_task(), and usb_host_task().
| #define Usb_clear_all_event | ( | ) | (g_usb_event = 0) |
| #define Is_usb_event | ( | x | ) | ((g_usb_event & (1<<x)) ? TRUE : FALSE) |
Definition at line 63 of file usb_task.h.
Referenced by host_send_data(), usb_device_task(), and usb_host_task().
| #define Is_not_usb_event | ( | x | ) | ((g_usb_event & (1<<x)) ? FALSE: TRUE) |
| #define Is_host_emergency_exit | ( | ) | (Is_usb_id_device()||(device_state==DEVICE_DISCONNECTED)) |
Definition at line 65 of file usb_task.h.
Referenced by host_get_data(), host_send_control(), host_send_data(), and usb_host_task().
| #define Is_usb_device | ( | ) | (g_usb_mode==USB_MODE_DEVICE ? TRUE : FALSE) |
Definition at line 66 of file usb_task.h.
| #define Is_usb_host | ( | ) | (g_usb_mode==USB_MODE_HOST ? TRUE : FALSE) |
Definition at line 67 of file usb_task.h.
| #define Otg_send_event | ( | x | ) | (g_otg_event |= (1<<x)) |
Definition at line 69 of file usb_task.h.
| #define Otg_ack_event | ( | x | ) | (g_otg_event &= ~(1<<x)) |
| #define Otg_clear_all_event | ( | ) | (g_otg_event = 0) |
Definition at line 71 of file usb_task.h.
| #define Is_otg_event | ( | x | ) | ((g_otg_event & (1<<x)) ? TRUE : FALSE) |
| #define Is_not_otg_event | ( | x | ) | ((g_otg_event & (1<<x)) ? FALSE: TRUE) |
Definition at line 73 of file usb_task.h.
| #define EVT_USB_POWERED 1 |
| #define EVT_USB_UNPOWERED 2 |
| #define EVT_USB_DEVICE_FUNCTION 3 |
| #define EVT_USB_HOST_FUNCTION 4 |
| #define EVT_USB_SUSPEND 5 |
Definition at line 79 of file usb_task.h.
Referenced by usb_device_task(), and usb_general_interrupt().
| #define EVT_USB_WAKE_UP 6 |
| #define EVT_USB_RESUME 7 |
Definition at line 81 of file usb_task.h.
Referenced by usb_device_task(), and usb_general_interrupt().
| #define EVT_USB_RESET 8 |
Definition at line 82 of file usb_task.h.
Referenced by usb_device_task(), and usb_general_interrupt().
| #define EVT_HOST_SOF 9 |
Definition at line 83 of file usb_task.h.
Referenced by host_send_control(), host_send_data(), usb_general_interrupt(), and usb_host_task().
| #define EVT_HOST_HWUP 10 |
Definition at line 84 of file usb_task.h.
Referenced by usb_general_interrupt(), and usb_host_task().
| #define EVT_HOST_DISCONNECTION 11 |
| #define EVT_HOST_REMOTE_WAKEUP 12 |
Definition at line 86 of file usb_task.h.
| #define EVT_OTG_HNP_ERROR 1 |
| #define EVT_OTG_HNP_SUCCESS 2 |
Definition at line 89 of file usb_task.h.
| #define EVT_OTG_SRP_RECEIVED 3 |
Definition at line 90 of file usb_task.h.
| #define EVT_OTG_DEV_UNSUPPORTED 4 |
| #define EVT_OTG_DEVICE_CONNECTED 5 |
1.5.3