Data Structures | |
| struct | S_usb_setup_data |
| Usb Setup Data. More... | |
| struct | S_usb_endpoint |
| struct | S_usb_interface |
| struct | S_usb_device |
| struct | S_usb_tree |
Defines | |
| #define | REQUEST_TYPE_POS 0 |
| #define | REQUEST_POS 1 |
| #define | VALUE_HIGH_POS 2 |
| #define | VALUE_LOW_POS 3 |
| #define | INDEX_HIGH_POS 4 |
| #define | INDEX_LOW_POS 5 |
| #define | LENGTH_HIGH_POS 6 |
| #define | LENGTH_LOW_POS 7 |
| #define | UNCOMPLETE_READ_POS 8 |
| #define | DATA_ADDR_HIGH_POS 9 |
| #define | DATA_ADDR_LOW_POS 10 |
| #define | CONTROL_GOOD 0 |
| #define | CONTROL_DATA_TOGGLE 0x01 |
| #define | CONTROL_DATA_PID 0x02 |
| #define | CONTROL_PID 0x04 |
| #define | CONTROL_TIMEOUT 0x08 |
| #define | CONTROL_CRC16 0x10 |
| #define | CONTROL_STALL 0x20 |
| #define | CONTROL_NO_DEVICE 0x40 |
| Set of defines for offset in data stage. | |
| #define | OFFSET_FIELD_MAXPACKETSIZE 7 |
| #define | OFFSET_FIELD_MSB_VID 9 |
| #define | OFFSET_FIELD_LSB_VID 8 |
| #define | OFFSET_FIELD_MSB_PID 11 |
| #define | OFFSET_FIELD_LSB_PID 10 |
| #define | OFFSET_DESCRIPTOR_LENGHT 0 |
| #define | OFFSET_FIELD_DESCRIPTOR_TYPE 1 |
| #define | OFFSET_FIELD_TOTAL_LENGHT 2 |
| #define | OFFSET_FIELD_BMATTRIBUTES 7 |
| #define | OFFSET_FIELD_MAXPOWER 8 |
| #define | OFFSET_FIELD_NB_INTERFACE 4 |
| OFFSET for INTERFACE DESCRIPTORS. | |
| #define | OFFSET_FIELD_CLASS 5 |
| #define | OFFSET_FIELD_SUB_CLASS 6 |
| #define | OFFSET_FIELD_PROTOCOL 7 |
| #define | OFFSET_FIELD_INTERFACE_NB 2 |
| #define | OFFSET_FIELD_ALT 3 |
| #define | OFFSET_FIELS_NB_OF_EP 4 |
| #define | OFFSET_FIELD_EP_ADDR 2 |
| #define | OFFSET_FIELD_EP_TYPE 3 |
| #define | OFFSET_FIELD_EP_SIZE 4 |
| #define | OFFSET_FIELD_EP_INTERVAL 6 |
| #define | HOST_FALSE 0 |
| #define | HOST_TRUE 1 |
| #define | host_clear_endpoint_feature(ep) |
| host_clear_endpoint_feature | |
| #define | host_get_configuration() |
| host_get_configuration | |
| #define | host_set_configuration(cfg_nb) |
| host_set_configuration | |
| #define | host_set_interface(interface_nb, alt_setting) |
| host_set_interface | |
| #define | host_get_device_descriptor_uncomplete() |
| host_get_device_descriptor_uncomplete | |
| #define | host_get_device_descriptor() |
| host_get_device_descriptor | |
| #define | host_get_configuration_descriptor() |
| host_get_configuration_descriptor | |
| #define | host_get_descriptor_uncomplete() |
| #define | host_set_address(addr) |
| host_set_address | |
| #define | host_set_feature_remote_wakeup() |
| host_set_feature_remote_wakeup | |
| #define | host_ms_get_max_lun() |
| host_ms_get_max_lun | |
| #define | Get_VID() (usb_tree.device[selected_device].vid) |
| Get_VID. | |
| #define | Get_PID() (usb_tree.device[selected_device].pid) |
| Get_PID. | |
| #define | Get_ep0_size() (usb_tree.device[selected_device].ep_ctrl_size) |
| Get_ep0_size. | |
| #define | Get_maxpower() (usb_tree.device[selected_device].maxpower) |
| Get_maxpower. | |
| #define | Get_class(s_interface) (usb_tree.device[selected_device].interface[s_interface].class) |
| #define | Get_subclass(s_interface) (usb_tree.device[selected_device].interface[s_interface].subclass) |
| #define | Get_protocol(s_interface) (usb_tree.device[selected_device].interface[s_interface].protocol) |
| #define | Get_ep_addr(s_interface, n_ep) (usb_tree.device[selected_device].interface[s_interface].ep[n_ep].ep_addr) |
| #define | Get_nb_ep(s_interface) (usb_tree.device[selected_device].interface[s_interface].nb_ep) |
| #define | Get_alts_s(s_interface) (usb_tree.device[selected_device].interface[s_interface].altset_nb) |
| #define | Get_interface_number(s_interface) (usb_tree.device[selected_device].interface[s_interface].interface_nb) |
| #define | Get_nb_supported_interface() (usb_tree.device[selected_device].nb_interface) |
| #define | Is_device_self_powered() ((usb_tree.device[selected_device].bmattributes & USB_CONFIG_ATTRIBUTES_SELFPOWERED) ? TRUE : FALSE) |
| #define | Get_nb_device() (usb_tree.nb_device) |
| #define | Is_device_supports_remote_wakeup() ((usb_tree.device[selected_device].bmattributes & USB_CONFIG_ATTRIBUTES_REMOTEWAKEUP) ? TRUE : FALSE) |
| #define | Host_select_device(i) (host_select_device(i)) |
| #define | Host_get_nb_device() ((U16)(usb_tree.nb_device)) |
Functions | |
| U8 | host_send_control (U8 *) |
| host_send_control. | |
| U8 | host_check_VID_PID (void) |
| host_check_VID_PID | |
| U8 | host_check_class (void) |
| host_check_class | |
| U8 | host_auto_configure_endpoint () |
| U8 | get_interface_descriptor_offset (U8 interface, U8 alt) |
| get_interface_descriptor_offset | |
| U8 | host_get_hwd_pipe_nb (U8 ep_addr) |
| void | init_usb_tree (void) |
| init_usb_tree | |
| void | remove_device_entry (U8 device_index) |
| remove_device_entry | |
| void | host_select_device (U8 i) |
| void | freeze_user_periodic_pipe (void) |
| void | unfreeze_user_periodic_pipe (void) |
Variables | |
| U8 | user_periodic_pipe |
| S_usb_tree | usb_tree |
| The main structure that represents the usb tree connected to the host controller. | |
| S_usb_setup_data | usb_request |
| For control requests management over pipe 0. | |
| U8 | data_stage [SIZEOF_DATA_STAGE] |
| Public : U8 data_stage[SIZEOF_DATA_STAGE]; Internal RAM buffer for USB data stage content This buffer is required to setup host enumeration process Its contains the device descriptors received. | |
| U8 | device_status |
| U8 | selected_device |
| U8 | ctrl_pipe_size |
| #define REQUEST_TYPE_POS 0 |
Definition at line 137 of file usb_host_enum.h.
| #define REQUEST_POS 1 |
Definition at line 138 of file usb_host_enum.h.
| #define VALUE_HIGH_POS 2 |
Definition at line 139 of file usb_host_enum.h.
| #define VALUE_LOW_POS 3 |
Definition at line 140 of file usb_host_enum.h.
| #define INDEX_HIGH_POS 4 |
Definition at line 141 of file usb_host_enum.h.
| #define INDEX_LOW_POS 5 |
Definition at line 142 of file usb_host_enum.h.
| #define LENGTH_HIGH_POS 6 |
Definition at line 143 of file usb_host_enum.h.
| #define LENGTH_LOW_POS 7 |
Definition at line 144 of file usb_host_enum.h.
| #define UNCOMPLETE_READ_POS 8 |
Definition at line 145 of file usb_host_enum.h.
| #define DATA_ADDR_HIGH_POS 9 |
Definition at line 146 of file usb_host_enum.h.
| #define DATA_ADDR_LOW_POS 10 |
Definition at line 147 of file usb_host_enum.h.
| #define CONTROL_GOOD 0 |
Definition at line 149 of file usb_host_enum.h.
Referenced by host_send_control(), and usb_host_task().
| #define CONTROL_DATA_TOGGLE 0x01 |
Definition at line 150 of file usb_host_enum.h.
| #define CONTROL_DATA_PID 0x02 |
Definition at line 151 of file usb_host_enum.h.
| #define CONTROL_PID 0x04 |
Definition at line 152 of file usb_host_enum.h.
| #define CONTROL_TIMEOUT 0x08 |
| #define CONTROL_CRC16 0x10 |
Definition at line 154 of file usb_host_enum.h.
| #define CONTROL_STALL 0x20 |
| #define CONTROL_NO_DEVICE 0x40 |
| #define OFFSET_FIELD_MAXPACKETSIZE 7 |
| #define OFFSET_FIELD_MSB_VID 9 |
| #define OFFSET_FIELD_LSB_VID 8 |
| #define OFFSET_FIELD_MSB_PID 11 |
| #define OFFSET_FIELD_LSB_PID 10 |
| #define OFFSET_DESCRIPTOR_LENGHT 0 |
Definition at line 166 of file usb_host_enum.h.
Referenced by get_interface_descriptor_offset(), and host_auto_configure_endpoint().
| #define OFFSET_FIELD_DESCRIPTOR_TYPE 1 |
Definition at line 167 of file usb_host_enum.h.
Referenced by get_interface_descriptor_offset(), host_auto_configure_endpoint(), and host_check_class().
| #define OFFSET_FIELD_TOTAL_LENGHT 2 |
| #define OFFSET_FIELD_BMATTRIBUTES 7 |
| #define OFFSET_FIELD_MAXPOWER 8 |
| #define OFFSET_FIELD_NB_INTERFACE 4 |
OFFSET for INTERFACE DESCRIPTORS.
Definition at line 175 of file usb_host_enum.h.
Referenced by get_interface_descriptor_offset().
| #define OFFSET_FIELD_CLASS 5 |
| #define OFFSET_FIELD_SUB_CLASS 6 |
| #define OFFSET_FIELD_PROTOCOL 7 |
| #define OFFSET_FIELD_INTERFACE_NB 2 |
Definition at line 180 of file usb_host_enum.h.
Referenced by get_interface_descriptor_offset(), and host_check_class().
| #define OFFSET_FIELD_ALT 3 |
Definition at line 181 of file usb_host_enum.h.
Referenced by get_interface_descriptor_offset(), and host_check_class().
| #define OFFSET_FIELS_NB_OF_EP 4 |
| #define OFFSET_FIELD_EP_ADDR 2 |
| #define OFFSET_FIELD_EP_TYPE 3 |
| #define OFFSET_FIELD_EP_SIZE 4 |
| #define OFFSET_FIELD_EP_INTERVAL 6 |
| #define HOST_FALSE 0 |
Definition at line 189 of file usb_host_enum.h.
Referenced by get_interface_descriptor_offset(), host_auto_configure_endpoint(), host_check_class(), host_check_VID_PID(), host_get_data_interrupt(), host_send_data_interrupt(), and usb_host_task().
| #define HOST_TRUE 1 |
Definition at line 190 of file usb_host_enum.h.
Referenced by host_auto_configure_endpoint(), host_check_class(), host_check_VID_PID(), host_get_data_interrupt(), host_send_data_interrupt(), and usb_host_task().
| #define host_clear_endpoint_feature | ( | ep | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_SET_STAND_ENDPOINT,\ usb_request.bRequest = SETUP_CLEAR_FEATURE,\ usb_request.wValue = FEATURE_ENDPOINT_HALT << 8,\ usb_request.wIndex = ep,\ usb_request.wLength = 0,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a clear endpoint request
| U8 | ep (the target endpoint nb) |
Definition at line 203 of file usb_host_enum.h.
| #define host_get_configuration | ( | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_GET_STAND_DEVICE,\ usb_request.bRequest = SETUP_GET_CONFIGURATION,\ usb_request.wValue = 0,\ usb_request.wIndex = 0,\ usb_request.wLength = 1,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a get configuration request
| none |
Definition at line 219 of file usb_host_enum.h.
| #define host_set_configuration | ( | cfg_nb | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_SET_STAND_DEVICE,\ usb_request.bRequest = SETUP_SET_CONFIGURATION,\ usb_request.wValue = cfg_nb,\ usb_request.wIndex = 0,\ usb_request.wLength = 0,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a set configuration request
| U8 | configuration numer to activate |
Definition at line 235 of file usb_host_enum.h.
Referenced by usb_host_task().
| #define host_set_interface | ( | interface_nb, | |||
| alt_setting | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_SET_STAND_DEVICE,\ usb_request.bRequest = USB_SETUP_SET_STAND_INTERFACE,\ usb_request.wValue = alt_setting,\ usb_request.wIndex = interface_nb,\ usb_request.wLength = 0,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a set interface request to specify a specific alt setting for an interface
| U8 | interface_nb (the interface) U8 alt_setting (the alternate setting to activate) |
Definition at line 253 of file usb_host_enum.h.
| #define host_get_device_descriptor_uncomplete | ( | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_GET_STAND_DEVICE,\ usb_request.bRequest = SETUP_GET_DESCRIPTOR,\ usb_request.wValue = DESCRIPTOR_DEVICE << 8,\ usb_request.wIndex = 0,\ usb_request.wLength = 64,\ usb_request.uncomplete_read = TRUE,\ host_send_control(data_stage))
this function send a get device desriptor request. The descriptor table received is stored in data_stage array. The received descriptors is limited to the control pipe lenght
| none |
Definition at line 274 of file usb_host_enum.h.
Referenced by usb_host_task().
| #define host_get_device_descriptor | ( | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_GET_STAND_DEVICE,\ usb_request.bRequest = SETUP_GET_DESCRIPTOR,\ usb_request.wValue = DESCRIPTOR_DEVICE << 8,\ usb_request.wIndex = 0,\ usb_request.wLength = 18,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a get device desriptor request. The descriptor table received is stored in data_stage array.
| none |
Definition at line 294 of file usb_host_enum.h.
Referenced by usb_host_task().
| #define host_get_configuration_descriptor | ( | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_GET_STAND_DEVICE,\ usb_request.bRequest = SETUP_GET_DESCRIPTOR,\ usb_request.wValue = DESCRIPTOR_CONFIGURATION << 8,\ usb_request.wIndex = 0,\ usb_request.wLength = 255,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a get device configuration request. The configuration descriptor table received is stored in data_stage array.
| none |
Definition at line 313 of file usb_host_enum.h.
Referenced by usb_host_task().
| #define host_get_descriptor_uncomplete | ( | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_GET_STAND_DEVICE,\ usb_request.bRequest = SETUP_GET_DESCRIPTOR,\ usb_request.wValue = 0,\ usb_request.wIndex = 0,\ usb_request.wLength = 64,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
Definition at line 321 of file usb_host_enum.h.
| #define host_set_address | ( | addr | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_SET_STAND_DEVICE,\ usb_request.bRequest = SETUP_SET_ADDRESS,\ usb_request.wValue = (U16)addr,\ usb_request.wIndex = 0,\ usb_request.wLength = 0,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a set address request.
| U8 | address (the addr attributed to the device) |
Definition at line 339 of file usb_host_enum.h.
Referenced by usb_host_task().
| #define host_set_feature_remote_wakeup | ( | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_SET_STAND_DEVICE,\ usb_request.bRequest = SETUP_SET_FEATURE,\ usb_request.wValue = 1,\ usb_request.wIndex = 1,\ usb_request.wLength = 0,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send a set feature device remote wakeup
| none |
Definition at line 356 of file usb_host_enum.h.
Referenced by usb_host_task().
| #define host_ms_get_max_lun | ( | ) |
Value:
(usb_request.bmRequestType = USB_SETUP_GET_CLASS_INTER,\ usb_request.bRequest = SETUP_MASS_STORAGE_GET_MAX_LUN,\ usb_request.wValue = 0,\ usb_request.wIndex = 0,\ usb_request.wLength = 1,\ usb_request.uncomplete_read = FALSE,\ host_send_control(data_stage))
this function send the mass storage specific request "get max lun"
| none |
Definition at line 375 of file usb_host_enum.h.
| #define Get_VID | ( | ) | (usb_tree.device[selected_device].vid) |
Get_VID.
this function returns the VID of the device connected
| none |
Definition at line 393 of file usb_host_enum.h.
Referenced by host_check_VID_PID().
| #define Get_PID | ( | ) | (usb_tree.device[selected_device].pid) |
Get_PID.
this function returns the PID of the device connected
| none |
Definition at line 405 of file usb_host_enum.h.
Referenced by host_check_VID_PID().
| #define Get_ep0_size | ( | ) | (usb_tree.device[selected_device].ep_ctrl_size) |
Get_ep0_size.
this function returns the size of the control endpoint for the selected device
| none |
Definition at line 417 of file usb_host_enum.h.
| #define Get_maxpower | ( | ) | (usb_tree.device[selected_device].maxpower) |
Get_maxpower.
this function returns the maximum power consumption ot the connected device (unit is 2mA)
| none |
Definition at line 429 of file usb_host_enum.h.
| #define Get_class | ( | s_interface | ) | (usb_tree.device[selected_device].interface[s_interface].class) |
this function returns the USB class associated to the specified interface
| U8 | s_interface: the supported interface number |
Definition at line 438 of file usb_host_enum.h.
Referenced by host_template_task(), and usb_host_task().
| #define Get_subclass | ( | s_interface | ) | (usb_tree.device[selected_device].interface[s_interface].subclass) |
this function returns the USB subclass associated to the specified interface
| U8 | s_interface: the supported interface number |
Definition at line 447 of file usb_host_enum.h.
Referenced by host_template_task(), and usb_host_task().
| #define Get_protocol | ( | s_interface | ) | (usb_tree.device[selected_device].interface[s_interface].protocol) |
this function returns the USB protocol associated to the specified interface
| U8 | s_interface: the supported interface number |
Definition at line 456 of file usb_host_enum.h.
Referenced by host_template_task(), and usb_host_task().
| #define Get_ep_addr | ( | s_interface, | |||
| n_ep | ) | (usb_tree.device[selected_device].interface[s_interface].ep[n_ep].ep_addr) |
this function returns endpoint address associated to the specified interface and endpoint number in this interface.
| U8 | s_interface: the supported interface number | |
| U8 | n_ep: the endpoint number in this interface |
Definition at line 467 of file usb_host_enum.h.
Referenced by host_template_task().
| #define Get_nb_ep | ( | s_interface | ) | (usb_tree.device[selected_device].interface[s_interface].nb_ep) |
this function returns number of endpoints associated to a supported interface.
| U8 | s_interface: the supported interface number |
Definition at line 477 of file usb_host_enum.h.
| #define Get_alts_s | ( | s_interface | ) | (usb_tree.device[selected_device].interface[s_interface].altset_nb) |
this function returns number of the alternate setting field associated to a supported interface.
| U8 | s_interface: the supported interface number |
Definition at line 487 of file usb_host_enum.h.
| #define Get_interface_number | ( | s_interface | ) | (usb_tree.device[selected_device].interface[s_interface].interface_nb) |
this function returns number of the interface number associated to a supported interface.
| U8 | s_interface: the supported interface number |
Definition at line 497 of file usb_host_enum.h.
| #define Get_nb_supported_interface | ( | ) | (usb_tree.device[selected_device].nb_interface) |
this function returns the number of interface supported in the device connected
| none |
Definition at line 506 of file usb_host_enum.h.
Referenced by host_template_task().
| #define Is_device_self_powered | ( | ) | ((usb_tree.device[selected_device].bmattributes & USB_CONFIG_ATTRIBUTES_SELFPOWERED) ? TRUE : FALSE) |
this function returns true if the device connected is self powered
| none |
Definition at line 515 of file usb_host_enum.h.
| #define Get_nb_device | ( | ) | (usb_tree.nb_device) |
this function returns the number of devices connected in the USB tree
| none |
Definition at line 524 of file usb_host_enum.h.
| #define Is_device_supports_remote_wakeup | ( | ) | ((usb_tree.device[selected_device].bmattributes & USB_CONFIG_ATTRIBUTES_REMOTEWAKEUP) ? TRUE : FALSE) |
this function returns true if the device supports remote wake_up
| none |
Definition at line 533 of file usb_host_enum.h.
Referenced by usb_host_task().
Definition at line 536 of file usb_host_enum.h.
Referenced by init_usb_tree(), unfreeze_user_periodic_pipe(), and usb_host_task().
| #define Host_get_nb_device | ( | ) | ((U16)(usb_tree.nb_device)) |
Definition at line 541 of file usb_host_enum.h.
host_send_control.
This function is the generic Pipe 0 management function This function is used to send and receive control request over pipe 0
| data_pointer |
Definition at line 531 of file usb_host_enum.c.
References S_usb_setup_data::bmRequestType, S_usb_setup_data::bRequest, c, CONTROL_GOOD, CONTROL_STALL, CONTROL_TIMEOUT, S_usb_tree::device, S_usb_device::device_address, S_usb_device::ep_ctrl_size, EVT_HOST_SOF, FALSE, freeze_user_periodic_pipe(), Host_ack_all_errors, Host_ack_control_in, Host_ack_control_out, Host_ack_in_received, Host_ack_setup, Host_ack_stall, Host_configure_address, Host_data_length_U8, Host_disable_sof_interrupt, Host_enable_sof_interrupt, Host_error_status, Host_freeze_pipe, Host_read_byte, Host_reset_pipe, Host_select_pipe, Host_send_control_in, Host_send_control_out, Host_send_setup, Host_set_token_in, Host_set_token_out, Host_set_token_setup, Host_standard_in_mode, Host_unfreeze_pipe, Host_write_byte, Is_host_control_in_received, Is_host_control_out_sent, Is_host_emergency_exit, Is_host_pipe_error, Is_host_setup_sent, Is_host_sof_interrupt_enabled, Is_host_stall, Is_not_usb_event, LSB, MSB, selected_device, TRUE, S_usb_setup_data::uncomplete_read, unfreeze_user_periodic_pipe(), Usb_ack_event, USB_SETUP_DIR_DEVICE_TO_HOST, S_usb_setup_data::wIndex, S_usb_setup_data::wLength, and S_usb_setup_data::wValue.
00532 { 00533 U16 data_length; 00534 U8 sav_int_sof_enable; 00535 U8 c; 00536 U8 ep_size_max; 00537 00538 #if (USB_HUB_SUPPORT==ENABLE && USER_PERIODIC_PIPE==ENABLE) 00539 freeze_user_periodic_pipe(); 00540 #endif 00541 00542 ep_size_max = usb_tree.device[selected_device].ep_ctrl_size; 00543 Host_configure_address(usb_tree.device[selected_device].device_address); 00544 00545 Usb_ack_event(EVT_HOST_SOF); 00546 sav_int_sof_enable=Is_host_sof_interrupt_enabled(); 00547 Host_enable_sof_interrupt(); // SOF software detection is in interrupt sub-routine 00548 while(Is_not_usb_event(EVT_HOST_SOF)) // Wait 1 sof 00549 { 00550 if (Is_host_emergency_exit()) 00551 { 00552 c=CONTROL_TIMEOUT; 00553 Host_freeze_pipe(); 00554 Host_reset_pipe(0); 00555 goto host_send_control_end; 00556 } 00557 } 00558 if (sav_int_sof_enable==FALSE) 00559 { 00560 Host_disable_sof_interrupt(); 00561 } 00562 00563 Host_select_pipe(0); 00564 Host_set_token_setup(); 00565 Host_ack_setup(); 00566 Host_unfreeze_pipe(); 00567 // Build the setup request fields 00568 Host_write_byte(usb_request.bmRequestType); 00569 Host_write_byte(usb_request.bRequest); 00570 Host_write_byte(LSB(usb_request.wValue)); 00571 Host_write_byte(MSB(usb_request.wValue)); 00572 Host_write_byte(LSB(usb_request.wIndex)); 00573 Host_write_byte(MSB(usb_request.wIndex)); 00574 Host_write_byte(LSB(usb_request.wLength)); 00575 Host_write_byte(MSB(usb_request.wLength)); 00576 00577 Host_send_setup(); 00578 while(Is_host_setup_sent() == FALSE) // wait for SETUP ack 00579 { 00580 if (Is_host_emergency_exit()) 00581 { 00582 c=CONTROL_TIMEOUT; 00583 Host_freeze_pipe(); 00584 Host_reset_pipe(0); 00585 goto host_send_control_end; 00586 } 00587 if(Is_host_pipe_error()) // Any error ? 00588 { 00589 c = Host_error_status(); 00590 Host_ack_all_errors(); 00591 goto host_send_control_end; // Send error status 00592 } 00593 } 00594 // Setup token sent now send In or OUT token 00595 // Before just wait one SOF 00596 Usb_ack_event(EVT_HOST_SOF); 00597 sav_int_sof_enable=Is_host_sof_interrupt_enabled(); 00598 Host_enable_sof_interrupt(); 00599 Host_freeze_pipe(); 00600 data_length = usb_request.wLength; 00601 while(Is_not_usb_event(EVT_HOST_SOF)) // Wait 1 sof 00602 { 00603 if (Is_host_emergency_exit()) 00604 { 00605 c=CONTROL_TIMEOUT; 00606 Host_freeze_pipe(); 00607 Host_reset_pipe(0); 00608 goto host_send_control_end; 00609 } 00610 } 00611 if (sav_int_sof_enable==FALSE) 00612 { Host_disable_sof_interrupt(); } // Restore SOF interrupt enable 00613 00614 // IN request management --------------------------------------------- 00615 if(usb_request.bmRequestType & USB_SETUP_DIR_DEVICE_TO_HOST) 00616 { 00617 Host_standard_in_mode(); 00618 Host_set_token_in(); 00619 Host_ack_control_in(); 00620 while(data_length != 0) 00621 { 00622 Host_unfreeze_pipe(); 00623 while(!Is_host_control_in_received()) 00624 { 00625 if (Is_host_emergency_exit()) 00626 { 00627 c=CONTROL_TIMEOUT; 00628 Host_freeze_pipe(); 00629 Host_reset_pipe(0); 00630 goto host_send_control_end; 00631 } 00632 if(Is_host_pipe_error()) 00633 { 00634 c = Host_error_status(); 00635 Host_ack_all_errors(); 00636 goto host_send_control_end; 00637 } 00638 if(Is_host_stall()) 00639 { 00640 c=CONTROL_STALL; 00641 Host_ack_stall(); 00642 goto host_send_control_end; 00643 } 00644 } 00645 c = Host_data_length_U8(); 00646 if (c == ep_size_max) 00647 { 00648 data_length -= c; 00649 if (usb_request.uncomplete_read == TRUE) // uncomplete_read 00650 { 00651 data_length = 0; 00652 } 00653 } 00654 else 00655 { 00656 data_length = 0; 00657 } 00658 while (c!=0) 00659 { 00660 *data_pointer = Host_read_byte(); 00661 data_pointer++; 00662 c--; 00663 } 00664 Host_freeze_pipe(); 00665 Host_ack_control_in(); 00666 Host_send_control_in(); 00667 } // end of IN data stage 00668 00669 Host_set_token_out(); 00670 Host_ack_control_out(); 00671 Host_unfreeze_pipe(); 00672 Host_send_control_out(); 00673 while(!Is_host_control_out_sent()) 00674 { 00675 if (Is_host_emergency_exit()) 00676 { 00677 c=CONTROL_TIMEOUT; 00678 Host_freeze_pipe(); 00679 Host_reset_pipe(0); 00680 goto host_send_control_end; 00681 } 00682 if(Is_host_pipe_error()) 00683 { 00684 c = Host_error_status(); 00685 Host_ack_all_errors(); 00686 goto host_send_control_end; 00687 } 00688 if(Is_host_stall()) 00689 { 00690 c=CONTROL_STALL; 00691 Host_ack_stall(); 00692 goto host_send_control_end; 00693 } 00694 } 00695 Host_ack_control_out(); 00696 c=(CONTROL_GOOD); 00697 goto host_send_control_end; 00698 } 00699 00700 // OUT request management --------------------------------------------- 00701 else // Data stage OUT (bmRequestType==0) 00702 { 00703 Host_set_token_out(); 00704 Host_ack_control_out(); 00705 while(data_length != 0) 00706 { 00707 Host_unfreeze_pipe(); 00708 c = ep_size_max; 00709 if ( ep_size_max > data_length) 00710 { 00711 c = (U8)data_length; 00712 data_length = 0; 00713 } 00714 else 00715 { 00716 data_length -= c; 00717 } 00718 while (c!=0) 00719 { 00720 Host_write_byte(*data_pointer); 00721 data_pointer++; 00722 c--; 00723 } 00724 Host_send_control_out(); 00725 while (!Is_host_control_out_sent()) 00726 { 00727 if (Is_host_emergency_exit()) 00728 { 00729 c=CONTROL_TIMEOUT; 00730 Host_freeze_pipe(); 00731 Host_reset_pipe(0); 00732 goto host_send_control_end; 00733 } 00734 if(Is_host_pipe_error()) 00735 { 00736 c = Host_error_status(); 00737 Host_ack_all_errors(); 00738 goto host_send_control_end; 00739 } 00740 if(Is_host_stall()) 00741 { 00742 c=CONTROL_STALL; 00743 Host_ack_stall(); 00744 goto host_send_control_end; 00745 } 00746 } 00747 Host_ack_control_out(); 00748 } // end of OUT data stage 00749 Host_freeze_pipe(); 00750 Host_set_token_in(); 00751 Host_ack_in_received(); 00752 Host_unfreeze_pipe(); 00753 while(!Is_host_control_in_received()) 00754 { 00755 if (Is_host_emergency_exit()) 00756 { 00757 c=CONTROL_TIMEOUT; 00758 Host_freeze_pipe(); 00759 Host_reset_pipe(0); 00760 goto host_send_control_end; 00761 } 00762 if(Is_host_pipe_error()) 00763 { 00764 c = Host_error_status(); 00765 Host_ack_all_errors(); 00766 goto host_send_control_end; 00767 } 00768 if(Is_host_stall()) 00769 { 00770 c=CONTROL_STALL; 00771 Host_ack_stall(); 00772 goto host_send_control_end; 00773 } 00774 } 00775 Host_ack_control_in(); 00776 Host_freeze_pipe(); 00777 Host_send_control_in(); 00778 c=(CONTROL_GOOD); 00779 goto host_send_control_end; 00780 } 00781 host_send_control_end: 00782 #if(USB_HUB_SUPPORT==ENABLE && USER_PERIODIC_PIPE==ENABLE) 00783 unfreeze_user_periodic_pipe(); 00784 #endif 00785 return ((U8)c); 00786 }
| U8 host_check_VID_PID | ( | void | ) |
host_check_VID_PID
This function checks if the VID and the PID are supported (if the VID/PID belongs to the VID_PID table)
| none |
Definition at line 126 of file usb_host_enum.c.
References c, data_stage, S_usb_tree::device, Get_PID, Get_VID, HOST_FALSE, HOST_TRUE, LSB, MSB, OFFSET_FIELD_LSB_PID, OFFSET_FIELD_LSB_VID, OFFSET_FIELD_MSB_PID, OFFSET_FIELD_MSB_VID, S_usb_device::pid, registered_VID_PID, selected_device, and S_usb_device::vid.
00127 { 00128 U8 c,d; 00129 00130 // Rebuild VID PID from data stage 00131 LSB(usb_tree.device[selected_device].vid) = data_stage[OFFSET_FIELD_LSB_VID]; 00132 MSB(usb_tree.device[selected_device].vid) = data_stage[OFFSET_FIELD_MSB_VID]; 00133 LSB(usb_tree.device[selected_device].pid) = data_stage[OFFSET_FIELD_LSB_PID]; 00134 MSB(usb_tree.device[selected_device].pid) = data_stage[OFFSET_FIELD_MSB_PID]; 00135 00136 // Compare detected VID PID with supported table 00137 c=0; 00138 while (c< sizeof(registered_VID_PID)/2) // /2 because registered_VID_PID table is U16... 00139 { 00140 if (registered_VID_PID[c] == Get_VID()) // VID is correct 00141 { 00142 d = (U8)registered_VID_PID[c+1]; // store nb of PID for this VID 00143 while (d != 0) 00144 { 00145 if (registered_VID_PID[c+d+1] == Get_PID()) 00146 { 00147 return HOST_TRUE; 00148 } 00149 d--; 00150 } 00151 } 00152 c+=registered_VID_PID[c+1]+2; 00153 } 00154 return HOST_FALSE; 00155 }
| U8 host_check_class | ( | void | ) |
host_check_class
This function checks if the device class is supported. The function looks in all interface declared in the received dewcriptors, if one of them match with the CLASS/SUB_CLASS/PROTOCOL table
| none |
Definition at line 168 of file usb_host_enum.c.
References S_usb_interface::altset_nb, S_usb_device::bmattributes, c, S_usb_interface::class, data_stage, DESCRIPTOR_CONFIGURATION, DESCRIPTOR_INTERFACE, S_usb_tree::device, HOST_FALSE, HOST_TRUE, S_usb_device::interface, S_usb_interface::interface_nb, LSB, MAX_INTERFACE_FOR_DEVICE, S_usb_device::maxpower, MSB, S_usb_interface::nb_ep, S_usb_device::nb_interface, OFFSET_FIELD_ALT, OFFSET_FIELD_BMATTRIBUTES, OFFSET_FIELD_CLASS, OFFSET_FIELD_DESCRIPTOR_TYPE, OFFSET_FIELD_INTERFACE_NB, OFFSET_FIELD_MAXPOWER, OFFSET_FIELD_PROTOCOL, OFFSET_FIELD_SUB_CLASS, OFFSET_FIELD_TOTAL_LENGHT, OFFSET_FIELS_NB_OF_EP, S_usb_interface::protocol, registered_class, selected_device, SIZEOF_DATA_STAGE, S_usb_interface::subclass, and T_DESC_OFFSET.
00169 { 00170 U8 c; 00171 T_DESC_OFFSET descriptor_offset; 00172 T_DESC_OFFSET conf_offset_end; 00173 U16 config_size; 00174 U8 device_class; 00175 U8 device_subclass; 00176 U8 device_protocol; 00177 U8 nb_interface_supported; 00178 00179 00180 nb_interface_supported=0; //First asumes ,no interface is supported! 00181 if (data_stage[OFFSET_FIELD_DESCRIPTOR_TYPE] != DESCRIPTOR_CONFIGURATION) // check if configuration descriptor 00182 { return HOST_FALSE;} 00183 LSB(config_size) = data_stage[OFFSET_FIELD_TOTAL_LENGHT]; 00184 MSB(config_size) = data_stage[OFFSET_FIELD_TOTAL_LENGHT+1]; 00185 usb_tree.device[selected_device].bmattributes = data_stage[OFFSET_FIELD_BMATTRIBUTES]; 00186 usb_tree.device[selected_device].maxpower = data_stage[OFFSET_FIELD_MAXPOWER]; 00187 descriptor_offset = 0; 00188 conf_offset_end = descriptor_offset + config_size; 00189 00190 // Look in all interfaces declared in the configuration 00191 while(descriptor_offset < conf_offset_end) 00192 { 00193 // Find next interface descriptor 00194 while (data_stage[descriptor_offset+OFFSET_FIELD_DESCRIPTOR_TYPE] != DESCRIPTOR_INTERFACE) 00195 { 00196 descriptor_offset += data_stage[descriptor_offset]; 00197 if(descriptor_offset >= conf_offset_end) 00198 { 00199 if(nb_interface_supported) 00200 { 00201 return HOST_TRUE; 00202 } 00203 else return HOST_FALSE; 00204 } 00205 } 00206 // Found an interface descriptor 00207 // Get charateristics of this interface 00208 device_class = data_stage[descriptor_offset + OFFSET_FIELD_CLASS]; 00209 device_subclass = data_stage[descriptor_offset + OFFSET_FIELD_SUB_CLASS]; 00210 device_protocol = data_stage[descriptor_offset + OFFSET_FIELD_PROTOCOL]; 00211 // Look in registered class table for match 00212 c=0; 00213 while (c< sizeof(registered_class)) 00214 { 00215 if (registered_class[c] == device_class) // class is correct! 00216 { 00217 if (registered_class[c+1] == device_subclass) // sub class is correct! 00218 { 00219 if (registered_class[c+2] == device_protocol) // protocol is correct! 00220 { 00221 // Prepare for another item CLASS/SUB_CLASS/PROTOCOL in table 00222 c+=3; 00223 // Store this interface as supported interface 00224 // Memorize its interface nb 00225 usb_tree.device[selected_device].interface[nb_interface_supported].interface_nb=data_stage[descriptor_offset+OFFSET_FIELD_INTERFACE_NB]; 00226 // its alternate setting 00227 usb_tree.device[selected_device].interface[nb_interface_supported].altset_nb=data_stage[descriptor_offset+OFFSET_FIELD_ALT]; 00228 // its USB class 00229 usb_tree.device[selected_device].interface[nb_interface_supported].class=device_class; 00230 // its USB subclass 00231 usb_tree.device[selected_device].interface[nb_interface_supported].subclass=device_subclass; 00232 // its USB protocol 00233 usb_tree.device[selected_device].interface[nb_interface_supported].protocol=device_protocol; 00234 // the number of endpoints associated to this interface 00235 // Note: The associated endpoints addresses are stored during pipe attribution... 00236 usb_tree.device[selected_device].interface[nb_interface_supported].nb_ep=data_stage[descriptor_offset+OFFSET_FIELS_NB_OF_EP]; 00237 // Update the number of interface supported 00238 nb_interface_supported++; 00239 // Update the number of interface supported for the device 00240 usb_tree.device[selected_device].nb_interface++; 00241 // Check the maximum number of interfaces we can support 00242 if(nb_interface_supported>=MAX_INTERFACE_FOR_DEVICE) 00243 { 00244 return HOST_TRUE; 00245 } 00246 } 00247 } 00248 } 00249 c+=3; // Check other item CLASS/SUB_CLASS/PROTOCOL in table 00250 } 00251 descriptor_offset += data_stage[descriptor_offset]; // Next descriptor 00252 if(descriptor_offset > SIZEOF_DATA_STAGE) // Check overflow 00253 { 00254 if(nb_interface_supported) 00255 { 00256 return HOST_TRUE; 00257 } 00258 else return HOST_FALSE; 00259 } 00260 } 00261 if(nb_interface_supported) 00262 { 00263 return HOST_TRUE; 00264 } 00265 else return HOST_FALSE; 00266 }
| U8 host_auto_configure_endpoint | ( | ) |
This function configures the pipe according to the device class of the interface selected. THe function will configure the pipe corresponding to the last device selected
Definition at line 275 of file usb_host_enum.c.
References S_usb_interface::altset_nb, S_usb_interface::class, data_stage, DESCRIPTOR_ENDPOINT, S_usb_tree::device, S_usb_interface::ep, S_usb_endpoint::ep_addr, S_usb_endpoint::ep_size, S_usb_endpoint::ep_type, FALSE, get_interface_descriptor_offset(), Get_pipe_token, host_configure_pipe, host_determine_pipe_size(), Host_disable_pipe, Host_enable_pipe, HOST_FALSE, Host_get_selected_pipe, Host_select_pipe, Host_set_configured, HOST_TRUE, Host_unallocate_memory, i, S_usb_device::interface, S_usb_interface::interface_nb, Is_host_pipe_memory_allocated, MAX_EP_NB, MSK_EP_DIR, S_usb_tree::nb_device, S_usb_interface::nb_ep, S_usb_device::nb_interface, OFFSET_DESCRIPTOR_LENGHT, OFFSET_FIELD_DESCRIPTOR_TYPE, OFFSET_FIELD_EP_ADDR, OFFSET_FIELD_EP_INTERVAL, OFFSET_FIELD_EP_SIZE, OFFSET_FIELD_EP_TYPE, ONE_BANK, S_usb_endpoint::pipe_number, SIZE_8, SIZEOF_DATA_STAGE, T_DESC_OFFSET, TOKEN_IN, TWO_BANKS, TYPE_BULK, TYPE_INTERRUPT, user_periodic_pipe, and user_periodic_pipe_device_index.
00276 { 00277 U8 nb_endpoint_to_configure; 00278 T_DESC_OFFSET descriptor_offset; 00279 U8 physical_pipe=1; // =1 cause lookup table assumes that physical pipe 0 is reserved for control 00280 U8 i; 00281 U8 ep_index; 00282 U8 device,interface,alt_interface; 00283 U8 nb_interface; 00284 00285 // Get the last device number to configure 00286 device = usb_tree.nb_device-1; 00287 00288 // Get the nulber of interface to configure for the last device connected 00289 nb_interface = usb_tree.device[device].nb_interface; 00290 00291 // Look for first physical pipe free 00292 // TODO improve allocation mechanism... 00293 i = Host_get_selected_pipe(); // Save current selected pipe 00294 for(physical_pipe=1;physical_pipe<MAX_EP_NB-1;physical_pipe++) 00295 { 00296 Host_select_pipe(physical_pipe); 00297 if(Is_host_pipe_memory_allocated()==FALSE) break; // Pipe already allocated try next one 00298 } 00299 Host_select_pipe(i); //Restore previous selected pipe 00300 00301 // For all interfaces to configure... 00302 for(i=0;i<nb_interface;i++) 00303 { 00304 ep_index=0; 00305 // Look for the target interface descriptor offset 00306 interface = usb_tree.device[device].interface[i].interface_nb; 00307 alt_interface = usb_tree.device[device].interface[i].altset_nb; 00308 descriptor_offset = get_interface_descriptor_offset(interface,alt_interface); 00309 // Get the number of endpoint to configure for this interface 00310 nb_endpoint_to_configure = usb_tree.device[device].interface[i].nb_ep; 00311 // Get the first Endpoint descriptor offset to configure 00312 descriptor_offset += data_stage[descriptor_offset+OFFSET_DESCRIPTOR_LENGHT]; // pointing on endpoint descriptor 00313 00314 // While there is at least one pipe to configure 00315 while (nb_endpoint_to_configure) 00316 { 00317 // Check and look for an Endpoint descriptor 00318 while (data_stage[descriptor_offset+OFFSET_FIELD_DESCRIPTOR_TYPE] != DESCRIPTOR_ENDPOINT) 00319 { 00320 descriptor_offset += data_stage[descriptor_offset]; 00321 if(descriptor_offset > SIZEOF_DATA_STAGE) // No more endpoint descriptor found -> Errror ! 00322 { return HOST_FALSE; } 00323 } 00324 #if (SAVE_INTERRUPT_PIPE_FOR_DMS_INTERFACE==ENABLE) 00325 // @TODO HUB support & INTERRUPT PIPE No validated 00326 if(data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE]==TYPE_INTERRUPT && usb_tree.device[device].interface[i].class==0x08) 00327 { 00328 nb_endpoint_to_configure--; 00329 usb_tree.device[device].interface[i].nb_ep--; 00330 continue; 00331 } 00332 #endif 00333 00334 // Select the new physical pipe to configure and get ride of any previous configuration for this physical pipe 00335 Host_select_pipe(physical_pipe); 00336 Host_disable_pipe(); 00337 Host_unallocate_memory(); 00338 Host_enable_pipe(); 00339 00340 // Build the pipe configuration according to the endpoint descriptors fields received 00341 // 00342 // host_configure_pipe( 00343 // physical_pipe, // pipe nb in USB interface 00344 // data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE], // pipe type (interrupt/BULK/ISO) 00345 // Get_pipe_token(data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR]), // pipe addr 00346 // (data_stage[descriptor_offset+2] & MSK_EP_DIR), // pipe dir (IN/OUT) 00347 // host_determine_pipe_size((U16)data_stage[descriptor_offset+OFFSET_FIELD_EP_SIZE]),// pipe size 00348 // ONE_BANK, // bumber of bank to allocate for pipe 00349 // data_stage[descriptor_offset+OFFSET_FIELD_EP_INTERVAL] // interrupt period (for interrupt pipe) 00350 // ); 00351 00352 #if (USB_HUB_SUPPORT==ENABLE) 00353 // For USB hub move from interupt type to bulk type 00354 if(data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE]==TYPE_INTERRUPT && usb_tree.device[device].interface[i].class==0x09) 00355 { 00356 host_configure_pipe(physical_pipe, \ 00357 TYPE_BULK, \ 00358 TOKEN_IN, \ 00359 1, \ 00360 SIZE_8, \ 00361 ONE_BANK, \ 00362 0 ); 00363 } 00364 else // The device connected is not a hub 00365 { 00366 if( nb_hub_present==0) // No hub already exist in the USB tree 00367 { 00368 host_configure_pipe( \ 00369 physical_pipe, \ 00370 data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE], \ 00371 Get_pipe_token(data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR]), \ 00372 (data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR] & MSK_EP_DIR), \ 00373 host_determine_pipe_size((U16)data_stage[descriptor_offset+OFFSET_FIELD_EP_SIZE]),\ 00374 TWO_BANKS, \ 00375 data_stage[descriptor_offset+OFFSET_FIELD_EP_INTERVAL] \ 00376 ); 00377 } 00378 else // At least one hub is present in the usb tree 00379 { 00380 if(data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE]==TYPE_BULK ) // If BULK type : OK 00381 { 00382 host_configure_pipe( \ 00383 physical_pipe, \ 00384 data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE], \ 00385 Get_pipe_token(data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR]), \ 00386 (data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR] & MSK_EP_DIR), \ 00387 host_determine_pipe_size((U16)data_stage[descriptor_offset+OFFSET_FIELD_EP_SIZE]),\ 00388 TWO_BANKS, \ 00389 data_stage[descriptor_offset+OFFSET_FIELD_EP_INTERVAL] \ 00390 ); 00391 } 00392 #if (USER_PERIODIC_PIPE==ENABLE) 00393 else 00394 if(user_periodic_pipe==0 ) 00395 { 00396 user_periodic_pipe=physical_pipe; 00397 user_periodic_pipe_device_index=device; 00398 host_configure_pipe( \ 00399 physical_pipe, \ 00400 data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE], \ 00401 Get_pipe_token(data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR]), \ 00402 (data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR] & MSK_EP_DIR), \ 00403 host_determine_pipe_size((U16)data_stage[descriptor_offset+OFFSET_FIELD_EP_SIZE]),\ 00404 ONE_BANK, \ 00405 data_stage[descriptor_offset+OFFSET_FIELD_EP_INTERVAL] \ 00406 ); 00407 } 00408 else 00409 { 00410 nb_endpoint_to_configure--; 00411 usb_tree.device[device].interface[i].nb_ep--; 00412 continue; 00413 } 00414 #endif 00415 } 00416 } 00417 #else // NO HUB SUPPORT 00418 host_configure_pipe( \ 00419 physical_pipe, \ 00420 data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE], \ 00421 Get_pipe_token(data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR]), \ 00422 (data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR] & MSK_EP_DIR), \ 00423 host_determine_pipe_size((U16)data_stage[descriptor_offset+OFFSET_FIELD_EP_SIZE]),\ 00424 TWO_BANKS, \ 00425 data_stage[descriptor_offset+OFFSET_FIELD_EP_INTERVAL] \ 00426 ); 00427 #endif 00428 00429 // Update endpoint addr table in supported interface structure 00430 usb_tree.device[device].interface[i].ep[ep_index].ep_addr = data_stage[descriptor_offset+OFFSET_FIELD_EP_ADDR]; 00431 // Update physical pipe number used for this endpoint 00432 usb_tree.device[device].interface[i].ep[ep_index].pipe_number = physical_pipe; 00433 // Update endpoint size in supported interface structure 00434 usb_tree.device[device].interface[i].ep[ep_index].ep_size = data_stage[descriptor_offset+OFFSET_FIELD_EP_SIZE]; 00435 // Update endpoint type in supported interface structure 00436 usb_tree.device[device].interface[i].ep[ep_index].ep_type = data_stage[descriptor_offset+OFFSET_FIELD_EP_TYPE]; 00437 // point on next descriptor 00438 descriptor_offset += data_stage[descriptor_offset]; 00439 // Use next physical pipe 00440 if (physical_pipe++>=MAX_EP_NB) 00441 { 00442 return HOST_FALSE; 00443 } 00444 // To configure next endpoint 00445 ep_index++; 00446 // All target endpoints configured ? 00447 nb_endpoint_to_configure--; 00448 } //for(i=0;i<nb_interface;i++) 00449 } 00450 Host_set_configured(); 00451 return HOST_TRUE; 00452 }
get_interface_descriptor_offset
This function returns the offset in data_stage where to find the interface descriptor whose number and alternate setting values are passed as parameters
| interface | the interface nb to look for offset descriptor | |
| alt | the interface alt setting number |
Definition at line 465 of file usb_host_enum.c.
References data_stage, DESCRIPTOR_INTERFACE, HOST_FALSE, OFFSET_DESCRIPTOR_LENGHT, OFFSET_FIELD_ALT, OFFSET_FIELD_DESCRIPTOR_TYPE, OFFSET_FIELD_INTERFACE_NB, OFFSET_FIELD_NB_INTERFACE, SIZEOF_DATA_STAGE, and T_DESC_OFFSET.
00466 { 00467 U8 nb_interface; 00468 T_DESC_OFFSET descriptor_offset; 00469 00470 nb_interface = data_stage[OFFSET_FIELD_NB_INTERFACE]; // Detects the number of interfaces in this configuration 00471 descriptor_offset = data_stage[OFFSET_DESCRIPTOR_LENGHT]; // now pointing on next descriptor 00472 00473 while(descriptor_offset < SIZEOF_DATA_STAGE) // Look in all interfaces declared in the configuration 00474 { 00475 while (data_stage[descriptor_offset+OFFSET_FIELD_DESCRIPTOR_TYPE] != DESCRIPTOR_INTERFACE) 00476 { 00477 descriptor_offset += data_stage[descriptor_offset]; 00478 if(descriptor_offset > SIZEOF_DATA_STAGE) 00479 { return HOST_FALSE; } 00480 } 00481 if (data_stage[descriptor_offset+OFFSET_FIELD_INTERFACE_NB]==interface 00482 && data_stage[descriptor_offset+OFFSET_FIELD_ALT]==alt) 00483 { 00484 return descriptor_offset; 00485 } 00486 descriptor_offset += data_stage[descriptor_offset]; 00487 } 00488 return descriptor_offset; 00489 }
This function returns the physical pipe number linked to a logical endpoint address.
| ep_addr |
Definition at line 501 of file usb_host_enum.c.
References S_usb_tree::device, S_usb_interface::ep, S_usb_endpoint::ep_addr, i, S_usb_device::interface, j, MAX_EP_PER_INTERFACE, MAX_INTERFACE_FOR_DEVICE, S_usb_endpoint::pipe_number, and selected_device.
00502 { 00503 U8 i,j; 00504 for(j=0;j<MAX_INTERFACE_FOR_DEVICE;j++) 00505 { 00506 for(i=0;i<MAX_EP_PER_INTERFACE;i++) 00507 { 00508 if(usb_tree.device[selected_device].interface[j].ep[i].ep_addr==ep_addr) 00509 { return usb_tree.device[selected_device].interface[j].ep[i].pipe_number; } 00510 } 00511 } 00512 return 0; 00513 }
| void init_usb_tree | ( | void | ) |
init_usb_tree
This function initializes the usb_tree structure when no device is connected to the root downstream port
Definition at line 795 of file usb_host_enum.c.
References Host_select_device, i, MAX_DEVICE_IN_USB_TREE, S_usb_tree::nb_device, remove_device_entry(), user_periodic_pipe, and user_periodic_pipe_device_index.
00796 { 00797 U8 i; 00798 00799 // Clear all device entry 00800 for(i=0;i<MAX_DEVICE_IN_USB_TREE;i++) 00801 { 00802 remove_device_entry(i); 00803 } 00804 // By default select device 0 (connected to root port) 00805 Host_select_device(0); 00806 00807 #if (USB_HUB_SUPPORT==ENABLE) 00808 #if (USER_PERIODIC_PIPE==ENABLE) 00809 user_periodic_pipe=0; 00810 user_periodic_pipe_device_index=0; 00811 #endif 00812 for(i=0;i<HUB_MAX_NB_PORT;i++) 00813 hub_init(i); 00814 for(i=0;i<USB_MAX_HUB_NUMBER;i++) 00815 hub_device_address[i]=0; 00816 #endif 00817 00818 // Clear the number of device in the tree 00819 usb_tree.nb_device=0; 00820 00821 }
| void remove_device_entry | ( | U8 | device_index | ) |
remove_device_entry
This function reset the device entry required when a device disconnect from the usb tree
If the removed device is a hub, the function also removes the devices connected to this hub. The function is also in charge of the USB DPRAM desallocation mechanism. DPRAM is deallocated only if the removed device is the last device that allocate pipes.
| device_index | the device numer index in the usb_tree that disconnects |
Definition at line 836 of file usb_host_enum.c.
References S_usb_interface::altset_nb, S_usb_device::bmattributes, S_usb_interface::class, S_usb_tree::device, S_usb_device::device_address, S_usb_interface::ep, S_usb_endpoint::ep_addr, S_usb_device::ep_ctrl_size, S_usb_endpoint::ep_size, S_usb_endpoint::ep_type, Host_get_selected_pipe, Host_select_pipe, Host_unallocate_memory, HUB_CLASS, S_usb_device::hub_port_nb, i, S_usb_device::interface, S_usb_interface::interface_nb, j, MAX_DEVICE_IN_USB_TREE, MAX_EP_PER_INTERFACE, MAX_INTERFACE_FOR_DEVICE, S_usb_device::maxpower, S_usb_tree::nb_device, S_usb_interface::nb_ep, S_usb_device::nb_interface, S_usb_device::parent_hub_number, S_usb_device::pid, S_usb_endpoint::pipe_number, S_usb_interface::protocol, remove_device_entry(), S_usb_interface::subclass, and S_usb_device::vid.
00837 { 00838 U8 i,j,k,m; 00839 00840 #if (USB_HUB_SUPPORT==ENABLE) 00841 // Check if the disconnected device is a hub 00842 if(usb_tree.device[device_index].interface[0].class==HUB_CLASS) 00843 { 00844 nb_hub_present--; 00845 for(i=0;i<USB_MAX_HUB_NUMBER;i++) // For entire hub table 00846 { // Find the hub number that deconnects 00847 if(hub_device_address[i]==usb_tree.device[device_index].device_address) 00848 { // Reset its port state machine 00849 for(j=0;j<HUB_MAX_NB_PORT;j++) // For all ports 00850 { 00851 hub_port_state[i][j]=HUB_DEVICE_POWERED; 00852 } 00853 // Look devices previously connected to this hub and remove ther entries 00854 for(j=0;j<MAX_DEVICE_IN_USB_TREE;j++) 00855 { 00856 if(usb_tree.device[j].parent_hub_number==(i+1)) 00857 { 00858 usb_tree.nb_device--; 00859 // Caution recursive function !!!! 00860 remove_device_entry(j); 00861 } 00862 } 00863 hub_device_address[i]=0; 00864 break; 00865 } 00866 } 00867 } 00868 #endif 00869 00870 // Unallocate USB pipe memory only if the device disconnection is the last device 00871 // enumerated 00872 // TODO: Improve it for devices removing from hub. 00873 // But cannot unallocate USB DPRAM if there is an active pipe number > current pipe for the removed device.... 00874 if(usb_tree.nb_device==device_index+1) 00875 { 00876 for(j=0;j<MAX_INTERFACE_FOR_DEVICE;j++) 00877 { 00878 for(k=0;k<MAX_EP_PER_INTERFACE;k++) 00879 { 00880 m=usb_tree.device[device_index].interface[j].ep[k].pipe_number; 00881 if(m!=0) 00882 { 00883 i = Host_get_selected_pipe(); 00884 Host_select_pipe(m); 00885 Host_unallocate_memory(); 00886 Host_select_pipe(i); 00887 } 00888 } 00889 } 00890 } 00891 // Reset device entry fields ... 00892 usb_tree.device[device_index].device_address = 0; 00893 usb_tree.device[device_index].ep_ctrl_size = 0; 00894 usb_tree.device[device_index].hub_port_nb = 0; 00895 usb_tree.device[device_index].parent_hub_number = 0; 00896 usb_tree.device[device_index].nb_interface = 0; 00897 usb_tree.device[device_index].pid = 0; 00898 usb_tree.device[device_index].vid = 0; 00899 usb_tree.device[device_index].bmattributes = 0; 00900 usb_tree.device[device_index].maxpower = 0; 00901 00902 for(j=0;j<MAX_INTERFACE_FOR_DEVICE;j++) 00903 { 00904 usb_tree.device[device_index].interface[j].interface_nb = 0; 00905 usb_tree.device[device_index].interface[j].altset_nb = 0; 00906 usb_tree.device[device_index].interface[j].class = 0; 00907 usb_tree.device[device_index].interface[j].subclass = 0; 00908 usb_tree.device[device_index].interface[j].protocol = 0; 00909 usb_tree.device[device_index].interface[j].nb_ep = 0; 00910 for(k=0;k<MAX_EP_PER_INTERFACE;k++) 00911 { 00912 usb_tree.device[device_index].interface[j].ep[k].ep_addr = 0; 00913 usb_tree.device[device_index].interface[j].ep[k].pipe_number = 0; 00914 usb_tree.device[device_index].interface[j].ep[k].ep_size = 0; 00915 usb_tree.device[device_index].interface[j].ep[k].ep_type = 0; 00916 } 00917 } 00918 }
| void host_select_device | ( | U8 | i | ) |
Definition at line 957 of file usb_host_enum.c.
References S_usb_tree::device, S_usb_device::device_address, freeze_user_periodic_pipe(), Host_configure_address, and selected_device.
00958 { 00959 freeze_user_periodic_pipe(); 00960 selected_device=i; 00961 Host_configure_address(usb_tree.device[i].device_address); 00962 }
| void freeze_user_periodic_pipe | ( | void | ) |
Definition at line 923 of file usb_host_enum.c.
References Host_freeze_pipe, Host_select_pipe, Is_host_pipe_freeze, user_periodic_pipe, and user_periodic_pipe_freeze_state.
00924 { 00925 if(user_periodic_pipe) 00926 { 00927 Host_select_pipe(user_periodic_pipe); 00928 if(Is_host_pipe_freeze()) 00929 { 00930 user_periodic_pipe_freeze_state=0; 00931 } 00932 else 00933 { 00934 user_periodic_pipe_freeze_state=1; 00935 Host_freeze_pipe(); 00936 } 00937 } 00938 }
| void unfreeze_user_periodic_pipe | ( | void | ) |
Definition at line 942 of file usb_host_enum.c.
References Host_select_device, Host_select_pipe, Host_unfreeze_pipe, user_periodic_pipe, user_periodic_pipe_device_index, and user_periodic_pipe_freeze_state.
00943 { 00944 if(user_periodic_pipe) 00945 { 00946 if(user_periodic_pipe_freeze_state) 00947 { 00948 Host_select_pipe(user_periodic_pipe); 00949 Host_unfreeze_pipe(); 00950 } 00951 Host_select_device(user_periodic_pipe_device_index); 00952 } 00953 }
Definition at line 103 of file usb_host_enum.c.
The main structure that represents the usb tree connected to the host controller.
Definition at line 100 of file usb_host_enum.c.
| U8 data_stage[SIZEOF_DATA_STAGE] |
Public : U8 data_stage[SIZEOF_DATA_STAGE]; Internal RAM buffer for USB data stage content This buffer is required to setup host enumeration process Its contains the device descriptors received.
Depending on the device descriptors lenght, its size can be optimized with the SIZEOF_DATA_STAGE define of conf_usb.h file
/
Definition at line 169 of file usb_host_task.c.
Referenced by get_interface_descriptor_offset(), host_auto_configure_endpoint(), host_check_class(), host_check_VID_PID(), and usb_host_task().
Definition at line 171 of file usb_host_task.c.
Definition at line 110 of file usb_host_enum.c.
1.5.3