Defines | |
| #define | Host_select_pipe(p) (UPNUM = (U8)p) |
| selects pipe for CPU interface | |
| #define | Host_get_selected_pipe() (UPNUM ) |
| get the currently selected pipe number | |
| #define | Host_enable_pipe() (UPCONX |= (1<<PEN)) |
| enables pipe | |
| #define | Host_disable_pipe() (UPCONX &= ~(1<<PEN)) |
| disables pipe | |
| #define | Host_set_token_setup() (UPCFG0X = UPCFG0X & ~MSK_TOKEN_SETUP) |
| sets SETUP token | |
| #define | Host_set_token_in() (UPCFG0X = (UPCFG0X & ~MSK_TOKEN_SETUP) | MSK_TOKEN_IN) |
| sets IN token | |
| #define | Host_set_token_out() (UPCFG0X = (UPCFG0X & ~MSK_TOKEN_SETUP) | MSK_TOKEN_OUT) |
| sets OUT token | |
| #define | Host_get_endpoint_number() (UPCFG0X & (MSK_PEPNUM)) |
| returns the number of the endpoint associated to the current pipe | |
| #define | Host_get_pipe_interrupt() (UPINT) |
| returns pipe interrupt register | |
| #define | Host_set_interrupt_frequency(frq) (UPCFG2X = (U8)frq) |
| sets the interrupt frequency | |
| #define | Is_pipe_configured() (UPSTAX & (1<<CFGOK)) |
| tests if current pipe is configured | |
| #define | Is_host_one_bank_busy() ((UPSTAX & MSK_NBUSYBK) != 0) |
| tests if at least one bank is busy | |
| #define | Host_number_of_busy_bank() (UPSTAX & MSK_NBUSYBK) |
| returns the number of busy banks | |
| #define | Host_reset_pipe(p) (UPRST = 1<<p , UPRST = 0) |
| resets the pipe | |
| #define | Host_write_byte(dat) (UPDATX = dat) |
| writes a byte into the pipe FIFO | |
| #define | Host_read_byte() (UPDATX) |
| reads a byte from the pipe FIFO | |
| #define | Host_freeze_pipe() (UPCONX |= (1<<PFREEZE)) |
| freezes the pipe | |
| #define | Host_unfreeze_pipe() (UPCONX &= ~(1<<PFREEZE)) |
| un-freezees the pipe | |
| #define | Is_host_pipe_freeze() (UPCONX & (1<<PFREEZE)) |
| tests if the current pipe is frozen | |
| #define | Host_reset_pipe_data_toggle() (UPCONX |= (1<<RSTDT) ) |
| resets data toggle | |
| #define | Is_host_setup_sent() ((UPINTX & (1<<TXSTPI)) ? TRUE : FALSE) |
| tests if SETUP has been sent | |
| #define | Is_host_control_in_received() ((UPINTX & (1<<RXINI)) ? TRUE : FALSE) |
| tests if control IN has been received | |
| #define | Is_host_control_out_sent() ((UPINTX & (1<<TXOUTI)) ? TRUE : FALSE) |
| tests if control OUT has been sent | |
| #define | Is_host_stall() ((UPINTX & (1<<RXSTALLI)) ? TRUE : FALSE) |
| tests if a STALL has been received | |
| #define | Is_host_pipe_error() ((UPINTX & (1<<PERRI)) ? TRUE : FALSE) |
| tests if an error occurs on current pipe | |
| #define | Host_send_setup() (UPINTX &= ~(1<<FIFOCON)) |
| sends a setup | |
| #define | Host_send_control_in() (UPINTX &= ~(1<<FIFOCON)) |
| sends a control IN | |
| #define | Host_send_control_out() (UPINTX &= ~(1<<FIFOCON)) |
| sends a control OUT | |
| #define | Host_ack_control_out() (UPINTX &= ~(1<<TXOUTI)) |
| acks control OUT | |
| #define | Host_ack_control_in() (UPINTX &= ~(1<<RXINI)) |
| acks control IN | |
| #define | Host_ack_setup() (UPINTX &= ~(1<<TXSTPI)) |
| acks setup | |
| #define | Host_ack_stall() (UPINTX &= ~(1<<RXSTALLI)) |
| acks STALL reception | |
| #define | Host_send_out() (UPINTX &= ~(1<<FIFOCON)) |
| sends a OUT | |
| #define | Is_host_out_sent() ((UPINTX & (1<<TXOUTI)) ? TRUE : FALSE) |
| tests if OUT has been sent | |
| #define | Host_ack_out_sent() (UPINTX &= ~(1<<TXOUTI)) |
| acks OUT sent | |
| #define | Is_host_in_received() ((UPINTX & (1<<RXINI)) ? TRUE : FALSE) |
| tests if IN received | |
| #define | Host_ack_in_received() (UPINTX &= ~(1<<RXINI)) |
| acks IN reception | |
| #define | Host_send_in() (UPINTX &= ~(1<<FIFOCON)) |
| sends a IN | |
| #define | Is_host_nak_received() ((UPINTX & (1<<NAKEDI)) ? TRUE : FALSE) |
| tests if nak handshake has been received | |
| #define | Host_ack_nak_received() (UPINTX &= ~(1<<NAKEDI)) |
| acks NAk received sent | |
| #define | Is_host_read_enabled() (UPINTX&(1<<RWAL)) |
| tests if endpoint read allowed | |
| #define | Is_host_write_enabled() (UPINTX&(1<<RWAL)) |
| tests if endpoint read allowed | |
| #define | Host_standard_in_mode() (UPCONX &= ~(1<<INMODE)) |
| sets IN in standard mode | |
| #define | Host_continuous_in_mode() (UPCONX |= (1<<INMODE)) |
| sets IN in continuous mode | |
| #define | Host_in_request_number(in_num) (UPINRQX = (U8)in_num) |
| sets number of IN requests to perform before freeze | |
| #define | Host_get_in_request_number() (UPINRQX) |
| returns number of remaining IN requests | |
| #define | Host_data_length_U8() (UPBCLX) |
| returns number of bytes (8 bits) | |
| #define | Host_data_length_U16() ((((U16)UPBCHX)<<8) | UPBCLX) |
| returns number of bytes (16 bits) | |
| #define | Host_byte_counter() Host_data_length_U16() |
| for device compatibility | |
| #define | Host_byte_counter_8() Host_data_length_U8() |
| for device compatibility | |
| #define | Host_get_pipe_length() ((U16)0x08 << ((UPCFG1X & MSK_PSIZE)>>4)) |
| returns the size of the current pipe | |
| #define | Host_get_pipe_type() (UPCFG0X>>6) |
| returns the type of the current pipe | |
| #define | Host_error_status() (UPERRX & MSK_ERROR) |
| tests if error occurs on pipe | |
| #define | Host_ack_all_errors() (UPERRX = 0x00) |
| acks all pipe error | |
| #define | Host_enable_transmit_interrupt() (UPIENX |= (1<<TXOUTE)) |
| Enable pipe end transmission interrupt. | |
| #define | Host_disable_transmit_interrupt() (UPIENX &= ~(1<<TXOUTE)) |
| Disable pipe end transmission interrupt. | |
| #define | Host_enable_receive_interrupt() (UPIENX |= (1<<RXINE)) |
| Enable pipe reception interrupt. | |
| #define | Host_disable_receive_interrupt() (UPIENX &= ~(1<<RXINE)) |
| Disable pipe recption interrupt. | |
| #define | Host_enable_stall_interrupt() (UPIENX |= (1<<RXSTALLE)) |
| Enable pipe stall interrupt. | |
| #define | Host_disable_stall_interrupt() (UPIENX &= ~(1<<RXSTALLE)) |
| Disable pipe stall interrupt. | |
| #define | Host_enable_error_interrupt() (UPIENX |= (1<<PERRE)) |
| Enable pipe error interrupt. | |
| #define | Host_disable_error_interrupt() (UPIENX &= ~(1<<PERRE)) |
| Disable pipe error interrupt. | |
| #define | Host_enable_nak_interrupt() (UPIENX |= (1<<NAKEDE)) |
| Enable pipe NAK interrupt. | |
| #define | Host_disable_nak_interrupt() (UPIENX &= ~(1<<NAKEDE)) |
| Disable pipe NAK interrupt. | |
| #define | Get_pipe_token(x) ((x & (0x80)) ? TOKEN_IN : TOKEN_OUT) |
| #define Host_select_pipe | ( | p | ) | (UPNUM = (U8)p) |
selects pipe for CPU interface
Definition at line 771 of file usb_drv.h.
Referenced by freeze_user_periodic_pipe(), host_auto_configure_endpoint(), host_disable_all_pipe(), host_get_data(), host_get_data_interrupt(), host_send_control(), host_send_data(), host_send_data_interrupt(), host_template_task(), remove_device_entry(), unfreeze_user_periodic_pipe(), usb_general_interrupt(), usb_host_task(), and usb_pipe_interrupt().
| #define Host_get_selected_pipe | ( | ) | (UPNUM ) |
get the currently selected pipe number
Definition at line 774 of file usb_drv.h.
Referenced by host_auto_configure_endpoint(), remove_device_entry(), usb_general_interrupt(), and usb_pipe_interrupt().
| #define Host_enable_pipe | ( | ) | (UPCONX |= (1<<PEN)) |
enables pipe
Definition at line 777 of file usb_drv.h.
Referenced by host_auto_configure_endpoint(), and host_config_pipe().
| #define Host_disable_pipe | ( | ) | (UPCONX &= ~(1<<PEN)) |
disables pipe
Definition at line 779 of file usb_drv.h.
Referenced by host_auto_configure_endpoint(), and host_disable_all_pipe().
| #define Host_set_token_setup | ( | ) | (UPCFG0X = UPCFG0X & ~MSK_TOKEN_SETUP) |
| #define Host_set_token_in | ( | ) | (UPCFG0X = (UPCFG0X & ~MSK_TOKEN_SETUP) | MSK_TOKEN_IN) |
sets IN token
Definition at line 784 of file usb_drv.h.
Referenced by host_get_data(), host_get_data_interrupt(), and host_send_control().
| #define Host_set_token_out | ( | ) | (UPCFG0X = (UPCFG0X & ~MSK_TOKEN_SETUP) | MSK_TOKEN_OUT) |
sets OUT token
Definition at line 786 of file usb_drv.h.
Referenced by host_send_control(), and host_send_data().
| #define Host_get_endpoint_number | ( | ) | (UPCFG0X & (MSK_PEPNUM)) |
| #define Host_get_pipe_interrupt | ( | ) | (UPINT) |
returns pipe interrupt register
Definition at line 792 of file usb_drv.h.
Referenced by usb_get_nb_pipe_interrupt().
| #define Host_set_interrupt_frequency | ( | frq | ) | (UPCFG2X = (U8)frq) |
| #define Is_pipe_configured | ( | ) | (UPSTAX & (1<<CFGOK)) |
tests if current pipe is configured
Definition at line 798 of file usb_drv.h.
Referenced by host_config_pipe().
| #define Is_host_one_bank_busy | ( | ) | ((UPSTAX & MSK_NBUSYBK) != 0) |
| #define Host_number_of_busy_bank | ( | ) | (UPSTAX & MSK_NBUSYBK) |
returns the number of busy banks
Definition at line 802 of file usb_drv.h.
Referenced by host_send_data().
| #define Host_reset_pipe | ( | p | ) | (UPRST = 1<<p , UPRST = 0) |
resets the pipe
Definition at line 805 of file usb_drv.h.
Referenced by host_disable_all_pipe(), host_get_data(), host_get_data_interrupt(), host_send_control(), host_send_data(), and host_send_data_interrupt().
| #define Host_write_byte | ( | dat | ) | (UPDATX = dat) |
writes a byte into the pipe FIFO
Definition at line 808 of file usb_drv.h.
Referenced by host_send_control(), host_send_data(), host_send_data_interrupt(), and usb_pipe_interrupt().
| #define Host_read_byte | ( | ) | (UPDATX) |
reads a byte from the pipe FIFO
Definition at line 810 of file usb_drv.h.
Referenced by host_get_data(), host_send_control(), host_template_task(), usb_host_task(), and usb_pipe_interrupt().
| #define Host_freeze_pipe | ( | ) | (UPCONX |= (1<<PFREEZE)) |
freezes the pipe
Definition at line 813 of file usb_drv.h.
Referenced by freeze_user_periodic_pipe(), host_get_data(), host_send_control(), host_send_data(), usb_host_task(), and usb_pipe_interrupt().
| #define Host_unfreeze_pipe | ( | ) | (UPCONX &= ~(1<<PFREEZE)) |
un-freezees the pipe
Definition at line 815 of file usb_drv.h.
Referenced by host_get_data(), host_get_data_interrupt(), host_send_control(), host_send_data(), host_send_data_interrupt(), host_template_task(), unfreeze_user_periodic_pipe(), usb_host_task(), and usb_pipe_interrupt().
| #define Is_host_pipe_freeze | ( | ) | (UPCONX & (1<<PFREEZE)) |
tests if the current pipe is frozen
Definition at line 817 of file usb_drv.h.
Referenced by freeze_user_periodic_pipe().
| #define Host_reset_pipe_data_toggle | ( | ) | (UPCONX |= (1<<RSTDT) ) |
| #define Is_host_setup_sent | ( | ) | ((UPINTX & (1<<TXSTPI)) ? TRUE : FALSE) |
tests if SETUP has been sent
Definition at line 823 of file usb_drv.h.
Referenced by host_send_control().
| #define Is_host_control_in_received | ( | ) | ((UPINTX & (1<<RXINI)) ? TRUE : FALSE) |
tests if control IN has been received
Definition at line 825 of file usb_drv.h.
Referenced by host_send_control().
| #define Is_host_control_out_sent | ( | ) | ((UPINTX & (1<<TXOUTI)) ? TRUE : FALSE) |
tests if control OUT has been sent
Definition at line 827 of file usb_drv.h.
Referenced by host_send_control().
| #define Is_host_stall | ( | ) | ((UPINTX & (1<<RXSTALLI)) ? TRUE : FALSE) |
tests if a STALL has been received
Definition at line 829 of file usb_drv.h.
Referenced by host_get_data(), host_send_control(), host_send_data(), host_template_task(), usb_host_task(), and usb_pipe_interrupt().
| #define Is_host_pipe_error | ( | ) | ((UPINTX & (1<<PERRI)) ? TRUE : FALSE) |
tests if an error occurs on current pipe
Definition at line 831 of file usb_drv.h.
Referenced by host_get_data(), host_send_control(), host_send_data(), and usb_pipe_interrupt().
| #define Host_send_setup | ( | ) | (UPINTX &= ~(1<<FIFOCON)) |
| #define Host_send_control_in | ( | ) | (UPINTX &= ~(1<<FIFOCON)) |
| #define Host_send_control_out | ( | ) | (UPINTX &= ~(1<<FIFOCON)) |
| #define Host_ack_control_out | ( | ) | (UPINTX &= ~(1<<TXOUTI)) |
| #define Host_ack_control_in | ( | ) | (UPINTX &= ~(1<<RXINI)) |
| #define Host_ack_setup | ( | ) | (UPINTX &= ~(1<<TXSTPI)) |
| #define Host_ack_stall | ( | ) | (UPINTX &= ~(1<<RXSTALLI)) |
acks STALL reception
Definition at line 845 of file usb_drv.h.
Referenced by host_get_data(), host_get_data_interrupt(), host_send_control(), host_send_data(), and host_send_data_interrupt().
| #define Host_send_out | ( | ) | (UPINTX &= ~(1<<FIFOCON)) |
sends a OUT
Definition at line 848 of file usb_drv.h.
Referenced by host_send_data(), host_send_data_interrupt(), and usb_pipe_interrupt().
| #define Is_host_out_sent | ( | ) | ((UPINTX & (1<<TXOUTI)) ? TRUE : FALSE) |
tests if OUT has been sent
Definition at line 850 of file usb_drv.h.
Referenced by host_send_data(), and usb_pipe_interrupt().
| #define Host_ack_out_sent | ( | ) | (UPINTX &= ~(1<<TXOUTI)) |
acks OUT sent
Definition at line 852 of file usb_drv.h.
Referenced by host_send_data(), host_send_data_interrupt(), and usb_pipe_interrupt().
| #define Is_host_in_received | ( | ) | ((UPINTX & (1<<RXINI)) ? TRUE : FALSE) |
tests if IN received
Definition at line 854 of file usb_drv.h.
Referenced by host_get_data(), host_template_task(), usb_host_task(), and usb_pipe_interrupt().
| #define Host_ack_in_received | ( | ) | (UPINTX &= ~(1<<RXINI)) |
acks IN reception
Definition at line 856 of file usb_drv.h.
Referenced by host_get_data(), host_get_data_interrupt(), host_send_control(), host_template_task(), usb_host_task(), and usb_pipe_interrupt().
| #define Host_send_in | ( | ) | (UPINTX &= ~(1<<FIFOCON)) |
sends a IN
Definition at line 858 of file usb_drv.h.
Referenced by host_get_data(), host_template_task(), usb_host_task(), and usb_pipe_interrupt().
| #define Is_host_nak_received | ( | ) | ((UPINTX & (1<<NAKEDI)) ? TRUE : FALSE) |
tests if nak handshake has been received
Definition at line 860 of file usb_drv.h.
Referenced by host_get_data(), host_send_data(), usb_host_task(), and usb_pipe_interrupt().
| #define Host_ack_nak_received | ( | ) | (UPINTX &= ~(1<<NAKEDI)) |
acks NAk received sent
Definition at line 862 of file usb_drv.h.
Referenced by host_get_data(), host_get_data_interrupt(), host_send_data(), host_send_data_interrupt(), usb_host_task(), and usb_pipe_interrupt().
| #define Is_host_read_enabled | ( | ) | (UPINTX&(1<<RWAL)) |
| #define Is_host_write_enabled | ( | ) | (UPINTX&(1<<RWAL)) |
| #define Host_standard_in_mode | ( | ) | (UPCONX &= ~(1<<INMODE)) |
sets IN in standard mode
Definition at line 872 of file usb_drv.h.
Referenced by host_send_control().
| #define Host_continuous_in_mode | ( | ) | (UPCONX |= (1<<INMODE)) |
sets IN in continuous mode
Definition at line 874 of file usb_drv.h.
Referenced by host_get_data(), host_get_data_interrupt(), and host_template_task().
| #define Host_in_request_number | ( | in_num | ) | (UPINRQX = (U8)in_num) |
| #define Host_get_in_request_number | ( | ) | (UPINRQX) |
| #define Host_data_length_U8 | ( | ) | (UPBCLX) |
returns number of bytes (8 bits)
Definition at line 882 of file usb_drv.h.
Referenced by host_send_control().
| #define Host_data_length_U16 | ( | ) | ((((U16)UPBCHX)<<8) | UPBCLX) |
| #define Host_byte_counter | ( | ) | Host_data_length_U16() |
for device compatibility
Definition at line 886 of file usb_drv.h.
Referenced by host_get_data(), and usb_pipe_interrupt().
| #define Host_byte_counter_8 | ( | ) | Host_data_length_U8() |
| #define Host_get_pipe_length | ( | ) | ((U16)0x08 << ((UPCFG1X & MSK_PSIZE)>>4)) |
returns the size of the current pipe
Definition at line 891 of file usb_drv.h.
Referenced by host_get_data(), host_send_data(), host_send_data_interrupt(), and usb_pipe_interrupt().
| #define Host_get_pipe_type | ( | ) | (UPCFG0X>>6) |
returns the type of the current pipe
Definition at line 894 of file usb_drv.h.
Referenced by usb_general_interrupt(), and usb_pipe_interrupt().
| #define Host_error_status | ( | ) | (UPERRX & MSK_ERROR) |
tests if error occurs on pipe
Definition at line 897 of file usb_drv.h.
Referenced by host_get_data(), host_send_control(), host_send_data(), and usb_pipe_interrupt().
| #define Host_ack_all_errors | ( | ) | (UPERRX = 0x00) |
acks all pipe error
Definition at line 899 of file usb_drv.h.
Referenced by host_get_data(), host_send_control(), host_send_data(), and usb_pipe_interrupt().
| #define Host_enable_transmit_interrupt | ( | ) | (UPIENX |= (1<<TXOUTE)) |
Enable pipe end transmission interrupt.
Definition at line 902 of file usb_drv.h.
Referenced by host_send_data_interrupt().
| #define Host_disable_transmit_interrupt | ( | ) | (UPIENX &= ~(1<<TXOUTE)) |
| #define Host_enable_receive_interrupt | ( | ) | (UPIENX |= (1<<RXINE)) |
Enable pipe reception interrupt.
Definition at line 907 of file usb_drv.h.
Referenced by host_get_data_interrupt().
| #define Host_disable_receive_interrupt | ( | ) | (UPIENX &= ~(1<<RXINE)) |
| #define Host_enable_stall_interrupt | ( | ) | (UPIENX |= (1<<RXSTALLE)) |
Enable pipe stall interrupt.
Definition at line 912 of file usb_drv.h.
Referenced by host_get_data_interrupt(), and host_send_data_interrupt().
| #define Host_disable_stall_interrupt | ( | ) | (UPIENX &= ~(1<<RXSTALLE)) |
| #define Host_enable_error_interrupt | ( | ) | (UPIENX |= (1<<PERRE)) |
Enable pipe error interrupt.
Definition at line 917 of file usb_drv.h.
Referenced by host_get_data_interrupt(), and host_send_data_interrupt().
| #define Host_disable_error_interrupt | ( | ) | (UPIENX &= ~(1<<PERRE)) |
| #define Host_enable_nak_interrupt | ( | ) | (UPIENX |= (1<<NAKEDE)) |
Enable pipe NAK interrupt.
Definition at line 922 of file usb_drv.h.
Referenced by host_get_data_interrupt(), and host_send_data_interrupt().
| #define Host_disable_nak_interrupt | ( | ) | (UPIENX &= ~(1<<NAKEDE)) |
| #define Get_pipe_token | ( | x | ) | ((x & (0x80)) ? TOKEN_IN : TOKEN_OUT) |
1.5.3