#include "config.h"#include "conf_usb.h"#include "modules/usb/usb_task.h"#include "usb_host_task.h"#include "lib_mcu/usb/usb_drv.h"#include "lib_mcu/pll/pll_drv.h"#include "modules/usb/host_chap9/usb_host_enum.h"#include "modules/usb/host_chap9/usb_host_hub.h"
Go to the source code of this file.
Defines | |
| #define | Usb_id_transition_action() |
| #define | Host_device_disconnection_action() |
| #define | Host_device_connection_action() |
| #define | Host_sof_action() |
| #define | Host_suspend_action() |
| #define | Host_hwup_action() |
| #define | Host_device_not_supported_action() |
| #define | Host_device_class_not_supported_action() |
| #define | Host_device_supported_action() |
| #define | Host_device_error_action() |
| #define | LOG_STR_CODE(str) |
Functions | |
| void | usb_host_task_init (void) |
| void | usb_host_task (void) |
| U8 | host_send_data (U8 pipe, U16 nb_data, U8 *buf) |
| U8 | host_get_data (U8 pipe, U16 *nb_data, U8 *buf) |
| void | reset_it_pipe_str (void) |
| U8 | is_any_interrupt_pipe_active (void) |
| U8 | host_get_data_interrupt (U8 pipe, U16 nb_data, U8 *buf, void(*handle)(U8 status, U16 nb_byte)) |
| U8 | host_send_data_interrupt (U8 pipe, U16 nb_data, U8 *buf, void(*handle)(U8 status, U16 nb_byte)) |
| __interrupt void | usb_pipe_interrupt () |
Variables | |
| volatile S_pipe_int | it_pipe_str [MAX_EP_NB] |
| volatile U8 | pipe_nb_save |
| U8 | g_sav_int_sof_enable |
| U8 | device_state |
Public : U8 device_state Its value represent the current state of the device connected to the usb host controller Value can be:
| |
| S_usb_setup_data | usb_request |
| For control requests management over pipe 0. | |
| U8 | data_stage [SIZEOF_DATA_STAGE] |
| Public : U8 data_stage[SIZEOF_DATA_STAGE]; Internal RAM buffer for USB data stage content This buffer is required to setup host enumeration process Its contains the device descriptors received. | |
| U8 | device_status |
| U8 | request_resume = FALSE |
| U8 | force_enumeration = FALSE |
| U8 | new_device_connected = FALSE |
| static U16 | c |
| static U8 | i |
| static U8 | j |
| volatile U8 | hub_interrupt_sof = 0 |
| U8 | saved_device |
Definition in file usb_host_task.c.
| #define Usb_id_transition_action | ( | ) |
Definition at line 84 of file usb_host_task.c.
| #define Host_device_disconnection_action | ( | ) |
Definition at line 87 of file usb_host_task.c.
| #define Host_device_connection_action | ( | ) |
Definition at line 90 of file usb_host_task.c.
| #define Host_sof_action | ( | ) |
Definition at line 93 of file usb_host_task.c.
| #define Host_suspend_action | ( | ) |
Definition at line 96 of file usb_host_task.c.
| #define Host_hwup_action | ( | ) |
Definition at line 99 of file usb_host_task.c.
| #define Host_device_not_supported_action | ( | ) |
Definition at line 102 of file usb_host_task.c.
| #define Host_device_class_not_supported_action | ( | ) |
Definition at line 105 of file usb_host_task.c.
| #define Host_device_supported_action | ( | ) |
Definition at line 108 of file usb_host_task.c.
| #define Host_device_error_action | ( | ) |
Definition at line 111 of file usb_host_task.c.
| #define LOG_STR_CODE | ( | str | ) |
Definition at line 118 of file usb_host_task.c.
Referenced by usb_general_interrupt(), and usb_host_task().
| __interrupt void usb_pipe_interrupt | ( | ) |
USB pipe interrupt subroutine
| none |
Definition at line 1132 of file usb_host_task.c.
References DISABLE, S_pipe_int::enable, FALSE, g_sav_int_sof_enable, S_pipe_int::handle, Host_ack_all_errors, Host_ack_in_received, Host_ack_nak_received, Host_ack_out_sent, Host_byte_counter, Host_disable_sof_interrupt, Host_error_status, Host_freeze_pipe, Host_get_pipe_length, Host_get_pipe_type, Host_get_selected_pipe, Host_read_byte, Host_select_pipe, Host_send_in, Host_send_out, Host_stop_pipe_interrupt, Host_unfreeze_pipe, Host_write_byte, i, is_any_interrupt_pipe_active(), Is_host_in_received, Is_host_nak_received, Is_host_out_sent, Is_host_pipe_error, Is_host_stall, NAK_RECEIVE_TIMEOUT, NAK_SEND_TIMEOUT, S_pipe_int::nak_timeout, S_pipe_int::nb_byte_on_going, S_pipe_int::nb_byte_processed, S_pipe_int::nb_byte_to_process, PIPE_GOOD, PIPE_NAK_TIMEOUT, pipe_nb_save, PIPE_STALL, private_sof_counter, S_pipe_int::ptr_buf, S_pipe_int::status, S_pipe_int::timeout, TRUE, TYPE_INTERRUPT, and usb_get_nb_pipe_interrupt().
01134 { 01135 U8 pipe_nb; 01136 U8 *ptr_buf; 01137 void (*fct_handle)(U8 status,U16 nb_byte); 01138 U16 n; 01139 U8 i; 01140 U8 do_call_back=FALSE; 01141 01142 pipe_nb_save = Host_get_selected_pipe(); // Important! Save here working pipe number 01143 pipe_nb=usb_get_nb_pipe_interrupt(); // work with the correct pipe number that generates the interrupt 01144 Host_select_pipe(pipe_nb); // Select this pipe 01145 fct_handle=*(it_pipe_str[pipe_nb].handle); 01146 01147 // Now try to detect what event generate an interrupt... 01148 01149 if (Is_host_pipe_error()) // Any error ? 01150 { 01151 it_pipe_str[pipe_nb].status = Host_error_status(); 01152 it_pipe_str[pipe_nb].enable=DISABLE; 01153 Host_stop_pipe_interrupt(pipe_nb); 01154 Host_ack_all_errors(); 01155 do_call_back=TRUE; 01156 goto usb_pipe_interrupt_end; 01157 } 01158 01159 if (Is_host_stall()) // Stall handshake received ? 01160 { 01161 it_pipe_str[pipe_nb].status=PIPE_STALL; 01162 it_pipe_str[pipe_nb].enable=DISABLE; 01163 Host_stop_pipe_interrupt(pipe_nb); 01164 do_call_back=TRUE; 01165 goto usb_pipe_interrupt_end; 01166 } 01167 01168 #if (NAK_TIMEOUT_ENABLE==ENABLE) 01169 if (Is_host_nak_received()) // NAK ? 01170 { 01171 Host_ack_nak_received(); 01172 // check if number of NAK timeout error occurs (not for interrupt type pipe) 01173 if((--it_pipe_str[pipe_nb].nak_timeout==0) && (Host_get_pipe_type()!=TYPE_INTERRUPT)) 01174 { 01175 it_pipe_str[pipe_nb].status=PIPE_NAK_TIMEOUT; 01176 it_pipe_str[pipe_nb].enable=DISABLE; 01177 Host_stop_pipe_interrupt(pipe_nb); 01178 do_call_back=TRUE; 01179 goto usb_pipe_interrupt_end; 01180 } 01181 } 01182 #endif 01183 01184 if (Is_host_in_received()) // Pipe IN reception ? 01185 { 01186 ptr_buf=it_pipe_str[pipe_nb].ptr_buf+it_pipe_str[pipe_nb].nb_byte_processed; // Build pointer to data buffer 01187 n=it_pipe_str[pipe_nb].nb_byte_to_process-it_pipe_str[pipe_nb].nb_byte_processed; // Remaining data bytes 01188 Host_freeze_pipe(); 01189 if (Host_byte_counter()<=n) 01190 { 01191 if ((Host_byte_counter() < n)&&(Host_byte_counter()<Host_get_pipe_length())) //Received less than remaining, but less than pipe capacity 01192 //TODO: error code 01193 { 01194 n=0; 01195 } 01196 else 01197 { 01198 n-=Host_byte_counter(); 01199 } 01200 it_pipe_str[pipe_nb].nb_byte_processed+=Host_byte_counter(); // Update nb of byte received 01201 for (i=Host_byte_counter();i;i--) 01202 { *ptr_buf=Host_read_byte(); ptr_buf++;} 01203 } 01204 else // more bytes received than expected 01205 { // TODO error code management 01206 it_pipe_str[pipe_nb].nb_byte_processed+=n; 01207 for (i=n;i;i--) // Byte number limited to the initial request (limit tab over pb) 01208 { *ptr_buf=Host_read_byte(); ptr_buf++;} 01209 n=0; 01210 } 01211 Host_ack_in_received(); 01212 if(n>0) //still something to process 01213 { 01214 Host_unfreeze_pipe(); // Request another IN transfer 01215 Host_send_in(); 01216 private_sof_counter=0; // Reset the counter in SOF detection sub-routine 01217 it_pipe_str[pipe_nb].timeout=0; // Reset timeout 01218 it_pipe_str[pipe_nb].nak_timeout=NAK_RECEIVE_TIMEOUT; 01219 01220 } 01221 else //end of transfer 01222 { 01223 it_pipe_str[pipe_nb].enable=DISABLE; 01224 it_pipe_str[pipe_nb].status=PIPE_GOOD; 01225 Host_stop_pipe_interrupt(pipe_nb); 01226 do_call_back=TRUE; 01227 } 01228 } 01229 01230 if(Is_host_out_sent()) // Pipe OUT sent ? 01231 { 01232 Host_ack_out_sent(); 01233 it_pipe_str[pipe_nb].nb_byte_processed+=it_pipe_str[pipe_nb].nb_byte_on_going; 01234 it_pipe_str[pipe_nb].nb_byte_on_going=0; 01235 ptr_buf=it_pipe_str[pipe_nb].ptr_buf+it_pipe_str[pipe_nb].nb_byte_processed; // Build pointer to data buffer 01236 n=it_pipe_str[pipe_nb].nb_byte_to_process-it_pipe_str[pipe_nb].nb_byte_processed; // Remaining data bytes 01237 if(n>0) // Still data to process... 01238 { 01239 Host_unfreeze_pipe(); 01240 // Prepare data to be sent 01241 i = Host_get_pipe_length(); 01242 if ( i > n) // Pipe size> remaining data 01243 { 01244 i = n; 01245 n = 0; 01246 } 01247 else // Pipe size < remaining data 01248 { n -= i; } 01249 it_pipe_str[pipe_nb].nb_byte_on_going+=i; // Update nb data processed 01250 while (i!=0) // Load Pipe buffer 01251 { 01252 Host_write_byte(*ptr_buf++); i--; 01253 } 01254 private_sof_counter=0; // Reset the counter in SOF detection sub-routine 01255 it_pipe_str[pipe_nb].timeout=0; // Refresh timeout counter 01256 it_pipe_str[pipe_nb].nak_timeout=NAK_SEND_TIMEOUT; 01257 Host_send_out(); // Send the USB frame 01258 } 01259 else //n==0 Transfer is finished 01260 { 01261 it_pipe_str[pipe_nb].enable=DISABLE; // Tranfer end 01262 it_pipe_str[pipe_nb].status=PIPE_GOOD; // Status OK 01263 Host_stop_pipe_interrupt(pipe_nb); 01264 do_call_back=TRUE; 01265 } 01266 } 01267 01268 usb_pipe_interrupt_end: 01269 Host_select_pipe(pipe_nb_save); // Restore pipe number !!!! 01270 if (is_any_interrupt_pipe_active()==FALSE) // If no more transfer is armed 01271 { 01272 if (g_sav_int_sof_enable==FALSE) 01273 { 01274 Host_disable_sof_interrupt(); 01275 } 01276 } 01277 if(do_call_back) // Any callback functions to perform ? 01278 { 01279 fct_handle(it_pipe_str[pipe_nb].status,it_pipe_str[pipe_nb].nb_byte_processed); 01280 } 01281 }
| volatile S_pipe_int it_pipe_str[MAX_EP_NB] |
Definition at line 132 of file usb_host_task.c.
| volatile U8 pipe_nb_save |
Definition at line 134 of file usb_host_task.c.
Referenced by host_get_data_interrupt(), host_send_data_interrupt(), usb_general_interrupt(), and usb_pipe_interrupt().
Definition at line 177 of file usb_host_task.c.
Referenced by host_check_class(), host_check_VID_PID(), host_send_control(), host_send_data(), uart_getchar(), and usb_host_task().
Definition at line 181 of file usb_host_task.c.
Referenced by device_template_task(), host_auto_configure_endpoint(), host_disable_all_pipe(), host_get_data(), host_get_hwd_pipe_nb(), host_send_data_interrupt(), host_template_task(), host_template_task_init(), init_usb_tree(), is_any_interrupt_pipe_active(), remove_device_entry(), reset_it_pipe_str(), usb_general_interrupt(), usb_get_nb_pipe_interrupt(), usb_host_task(), and usb_pipe_interrupt().
Definition at line 181 of file usb_host_task.c.
Referenced by host_get_hwd_pipe_nb(), remove_device_entry(), and usb_host_task().
| volatile U8 hub_interrupt_sof = 0 |
Definition at line 182 of file usb_host_task.c.
Referenced by usb_general_interrupt(), and usb_host_task().
1.5.3