Go to the source code of this file.
Defines | |
Global Class, SubClass & Protocol constants for HUB | |
| #define | HUB_CLASS 0x09 |
| #define | HUB_SUB_CLASS NO_SUBCLASS |
| #define | HUB_PROTOCOL NO_PROTOCOL |
Definition in file usb_commun_hub.h.
| #define HUB_CLASS 0x09 |
Definition at line 49 of file usb_commun_hub.h.
Referenced by remove_device_entry(), and usb_host_task().
| #define HUB_SUB_CLASS NO_SUBCLASS |
Definition at line 50 of file usb_commun_hub.h.
| #define HUB_PROTOCOL NO_PROTOCOL |
Definition at line 51 of file usb_commun_hub.h.
1.5.3