#include "modules/usb/usb_commun.h"#include "modules/usb/usb_commun_hub.h"#include "modules/usb/usb_commun_hid.h"#include "modules/usb/usb_commun_ms.h"#include "modules/usb/usb_commun_cdc.h"
Go to the source code of this file.
Defines | |
| #define | USB_HOST_FEATURE ENABLED |
| #define | USB_DEVICE_FEATURE ENABLED |
| #define | USE_USB_PADS_REGULATOR ENABLE |
| #define | VID_PID_TABLE |
| #define | CLASS_SUBCLASS_PROTOCOL |
| #define | SIZEOF_DATA_STAGE 250 |
| The size of RAM buffer reserved of descriptors manipulation. | |
| #define | DEVICE_BASE_ADDRESS 0x05 |
| The address that will be assigned to the connected device. | |
| #define | MAX_EP_PER_INTERFACE 3 |
| The maximum number of endpoints per interface supported. | |
| #define | MAX_INTERFACE_FOR_DEVICE 3 |
| The maximum number of interface supported per device. | |
| #define | MAX_DEVICE_IN_USB_TREE 1 |
| The maximum number of devices in the USB tree. | |
| #define | SAVE_INTERRUPT_PIPE_FOR_DMS_INTERFACE ENABLE |
| #define | USB_HUB_SUPPORT DISABLE |
| Configuration for Hub support in host mode. | |
| #define | HOST_STRICT_VID_PID_TABLE DISABLE |
| The host controller will be limited to the strict VID/PID list. | |
| #define | HOST_AUTO_CFG_ENDPOINT ENABLE |
| Try to configure the host pipe according to the device descriptors received. | |
| #define | HOST_CONTINUOUS_SOF_INTERRUPT DISABLE |
| Host start of frame interrupt always enable. | |
| #define | HOST_ERROR_RESTART ENABLE |
| When Host error state detected, goto unattached state. | |
| #define | USB_HOST_PIPE_INTERRUPT_TRANSFER ENABLE |
| USB host pipes transfers use USB communication interrupt (allows to use none blocking functions). | |
| #define | ID_PIN_CHANGE_GENERATE_RESET ENABLE |
| Force WDT reset upon ID pin change. | |
| #define | TIMEOUT_DELAY_ENABLE ENABLE |
| Enable Timeout delay (time) for host transfer. | |
| #define | TIMEOUT_DELAY 1 |
| delay 1/4sec (250ms) before timeout value | |
| #define | NAK_TIMEOUT_ENABLE ENABLE |
| Enable cpt NAK Timeout for host transfer. | |
| #define | NAK_SEND_TIMEOUT 0x0010 |
| Number of NAK handshake before timeout for transmit functions (up to 0xFFFF). | |
| #define | NAK_RECEIVE_TIMEOUT 0x0010 |
| NAKNumber of NAK handshake before timeout for receive functions (up to 0xFFFF). | |
| #define | SOFTWARE_VBUS_CTRL ENABLE |
| For reduced host only allows to control VBUS generator with PIO PE.7. | |
| #define | User_configure_endpoint() |
| If no auto configuration of EP, map here user function. | |
| #define | Usb_id_transition_action() |
| #define | Host_device_disconnection_action() |
| #define | Host_device_connection_action() |
| #define | Host_sof_action() |
| #define | Host_suspend_action() |
| #define | Host_hwup_action() |
| #define | Host_device_not_supported_action() |
| #define | Host_device_class_not_supported_action() |
| #define | Host_device_supported_action() |
| #define | Host_device_error_action() |
| #define | USB_DEVICE_SN_USE DISABLE |
| #define | USE_DEVICE_SN_UNIQUE DISABLE |
| #define | EP_TEMP_IN 1 |
| #define | EP_TEMP_OUT 2 |
| #define | EP_TEMP_INT_IN 3 |
| #define | USB_LOW_SPEED_DEVICE DISABLE |
| The USB device speed mode (default DISABLE to get full speed connection). | |
| #define | USB_REMOTE_WAKEUP_FEATURE DISABLE |
| #define | Usb_sof_action() sof_action(); |
| #define | Usb_wake_up_action() |
| #define | Usb_resume_action() |
| #define | Usb_suspend_action() |
| #define | Usb_reset_action() |
| #define | Usb_vbus_on_action() |
| #define | Usb_vbus_off_action() |
| #define | Usb_set_configuration_action() |
Functions | |
| void | sof_action (void) |
Definition in file conf_usb.h.
1.5.3