#include "config.h"
Go to the source code of this file.
Functions | |
| Bool | usb_user_read_request (U8, U8) |
| This function checks the specific request and if known then processes it | |
| void | usb_user_endpoint_init (U8) |
| U8 | usb_user_interface_get (U16 wInterface) |
| void | usb_user_interface_reset (U16 wInterface, U8 alternate_setting) |
| Bool | usb_user_get_descriptor (U8, U8) |
| This function fills the global descriptor. | |
Variables | |
| code S_usb_device_descriptor | usb_dev_desc |
| code S_usb_user_configuration_descriptor | usb_conf_desc |
| code S_usb_manufacturer_string_descriptor | usb_user_manufacturer_string_descriptor |
| code S_usb_product_string_descriptor | usb_user_product_string_descriptor |
| code S_usb_serial_number | usb_user_serial_number |
| code S_usb_language_id | usb_user_language_id |
Definition in file usb_specific_request.h.
This function checks the specific request and if known then processes it
| type | corresponding at bmRequestType (see USB specification) | |
| request | corresponding at bRequest (see USB specification) |
FALSE, if the request is'nt know (STALL handshake is managed by the main standard request function).
Definition at line 80 of file usb_specific_request.c.
References FALSE, SETUP_GET_DESCRIPTOR, Usb_read_byte, USB_SETUP_GET_CLASS_INTER, USB_SETUP_GET_STAND_INTERFACE, and USB_SETUP_SET_CLASS_INTER.
00081 { 00082 U8 wValue_msb; 00083 U8 wValue_lsb; 00084 00085 // Read wValue 00086 wValue_lsb = Usb_read_byte(); 00087 wValue_msb = Usb_read_byte(); 00088 00089 //** Specific request from Class 00090 if( USB_SETUP_GET_STAND_INTERFACE == type ) 00091 { 00092 switch( request ) 00093 { 00094 case SETUP_GET_DESCRIPTOR: 00095 switch( wValue_msb ) // Descriptor ID 00096 { 00097 default: 00098 // TODO 00099 break; 00100 } 00101 break; 00102 } 00103 } 00104 if( USB_SETUP_SET_CLASS_INTER == type ) 00105 { 00106 switch( request ) 00107 { 00108 default: 00109 break; 00110 } 00111 } 00112 if( USB_SETUP_GET_CLASS_INTER == type ) 00113 { 00114 switch( request ) 00115 { 00116 default: 00117 break; 00118 } 00119 } 00120 return FALSE; // No supported request 00121 }
| void usb_user_endpoint_init | ( | U8 | conf_nb | ) |
This function configures the endpoints
| conf_nb | configuration number choosed by USB host |
Definition at line 128 of file usb_specific_request.c.
References DIRECTION_IN, DIRECTION_OUT, EP_TEMP_IN, EP_TEMP_INT_IN, EP_TEMP_OUT, NYET_ENABLED, ONE_BANK, SIZE_64, TYPE_BULK, TYPE_INTERRUPT, and usb_configure_endpoint.
00129 { 00130 usb_configure_endpoint(EP_TEMP_IN, \ 00131 TYPE_BULK, \ 00132 DIRECTION_IN, \ 00133 SIZE_64, \ 00134 ONE_BANK, \ 00135 NYET_ENABLED); 00136 usb_configure_endpoint(EP_TEMP_OUT, \ 00137 TYPE_BULK, \ 00138 DIRECTION_OUT, \ 00139 SIZE_64, \ 00140 ONE_BANK, \ 00141 NYET_ENABLED); 00142 usb_configure_endpoint(EP_TEMP_INT_IN,\ 00143 TYPE_BULK, \ 00144 TYPE_INTERRUPT,\ 00145 SIZE_64, \ 00146 ONE_BANK, \ 00147 NYET_ENABLED); 00148 }
This function returns the interface alternate setting
| wInterface | Interface selected |
Definition at line 157 of file usb_specific_request.c.
This function selects (and resets) the interface alternate setting
| wInterface | Interface selected | |
| alternate_setting | alternate setting selected |
Definition at line 168 of file usb_specific_request.c.
References EP_TEMP_IN, EP_TEMP_INT_IN, EP_TEMP_OUT, INTERFACE_NB_SECOND_TEMP, INTERFACE_NB_TEMP, Usb_disable_stall_handshake, Usb_reset_data_toggle, Usb_reset_endpoint, and Usb_select_endpoint.
00169 { 00170 // default setting selected = reset data toggle 00171 if( INTERFACE_NB_TEMP == wInterface ) 00172 { 00173 // Interface reset 00174 Usb_select_endpoint(EP_TEMP_IN); 00175 Usb_disable_stall_handshake(); 00176 Usb_reset_endpoint(EP_TEMP_IN); 00177 Usb_reset_data_toggle(); 00178 Usb_select_endpoint(EP_TEMP_OUT); 00179 Usb_disable_stall_handshake(); 00180 Usb_reset_endpoint(EP_TEMP_OUT); 00181 Usb_reset_data_toggle(); 00182 } 00183 if( INTERFACE_NB_SECOND_TEMP == wInterface ) 00184 { 00185 // Interface reset 00186 Usb_select_endpoint(EP_TEMP_INT_IN); 00187 Usb_disable_stall_handshake(); 00188 Usb_reset_endpoint(EP_TEMP_INT_IN); 00189 Usb_reset_data_toggle(); 00190 } 00191 }
This function fills the global descriptor.
| type | corresponding at MSB of wValue (see USB specification) | |
| string | corresponding at LSB of wValue (see USB specification) |
Definition at line 201 of file usb_specific_request.c.
References S_usb_serial_number::bLength, S_usb_product_string_descriptor::bLength, S_usb_manufacturer_string_descriptor::bLength, S_usb_language_id::bLength, data_to_transfer, DESCRIPTOR_STRING, f_get_serial_string, FALSE, LANG_ID, MAN_INDEX, pbuffer, PROD_INDEX, SN_INDEX, SN_LENGTH, TRUE, usb_user_language_id, usb_user_manufacturer_string_descriptor, usb_user_product_string_descriptor, and usb_user_serial_number.
00202 { 00203 switch(type) 00204 { 00205 case DESCRIPTOR_STRING: 00206 switch (string) 00207 { 00208 case LANG_ID: 00209 data_to_transfer = sizeof (usb_user_language_id); 00210 pbuffer = &(usb_user_language_id.bLength); 00211 return TRUE; 00212 break; 00213 00214 case MAN_INDEX: 00215 data_to_transfer = sizeof (usb_user_manufacturer_string_descriptor); 00216 pbuffer = &(usb_user_manufacturer_string_descriptor.bLength); 00217 return TRUE; 00218 break; 00219 00220 case PROD_INDEX: 00221 data_to_transfer = sizeof (usb_user_product_string_descriptor); 00222 pbuffer = &(usb_user_product_string_descriptor.bLength); 00223 return TRUE; 00224 break; 00225 00226 #if (USB_DEVICE_SN_USE==ENABLE) 00227 case SN_INDEX: 00228 data_to_transfer = sizeof (usb_user_serial_number); 00229 pbuffer = &(usb_user_serial_number.bLength); 00230 #if (USE_DEVICE_SN_UNIQUE==ENABLE) 00231 f_get_serial_string=TRUE; 00232 data_to_transfer += (SN_LENGTH*4); 00233 #endif 00234 return TRUE; 00235 break; 00236 #endif 00237 } 00238 break; 00239 } 00240 return FALSE; 00241 }
Definition at line 69 of file usb_descriptors.c.
Definition at line 88 of file usb_descriptors.c.
Definition at line 154 of file usb_descriptors.c.
Definition at line 163 of file usb_descriptors.c.
Definition at line 172 of file usb_descriptors.c.
Definition at line 186 of file usb_descriptors.c.
1.5.3