#include "config.h"#include "conf_usb.h"#include "lib_mcu/usb/usb_drv.h"#include "usb_descriptors.h"#include "modules/usb/device_chap9/usb_standard_request.h"#include "usb_specific_request.h"#include "lib_mcu/flash/flash_drv.h"
Go to the source code of this file.
This file contains the usb parameters that uniquely identify the application through descriptor tables.
Definition in file usb_descriptors.c.
Initial value:
{
sizeof(usb_dev_desc)
, DESCRIPTOR_DEVICE
, Usb_write_word_enum_struc( 0x0200 )
, 0
, 0
, 0
, 64
, Usb_write_word_enum_struc( VID_ATMEL )
, Usb_write_word_enum_struc( 0x0000 )
, Usb_write_word_enum_struc( 0x1000 )
, 0x01
, 0x02
, 0x03
, 1
}
Definition at line 69 of file usb_descriptors.c.
Definition at line 88 of file usb_descriptors.c.
Initial value:
{
sizeof(usb_user_manufacturer_string_descriptor)
, DESCRIPTOR_STRING
, { ((U16)( 'A' )) , ((U16)( 'T' )) , ((U16)( 'M' )) , ((U16)( 'E' )) , ((U16)( 'L' )) }
}
Definition at line 154 of file usb_descriptors.c.
Referenced by usb_user_get_descriptor().
Initial value:
{
sizeof(usb_user_product_string_descriptor)
, DESCRIPTOR_STRING
, { ((U16)( 'A' )) ,((U16)( 'V' )) ,((U16)( 'R' )) ,((U16)( ' ' )) ,((U16)( 'U' )) ,((U16)( 'S' )) ,((U16)( 'B' )) ,((U16)( ' ' )) ,((U16)( 'D' )) ,((U16)( 'E' )) ,((U16)( 'V' )) ,((U16)( 'I' )) ,((U16)( 'C' )) ,((U16)( 'E' )) }
}
Definition at line 163 of file usb_descriptors.c.
Referenced by usb_user_get_descriptor().
Initial value:
{
sizeof(usb_user_serial_number)+4*SN_LENGTH
, DESCRIPTOR_STRING
}
Definition at line 172 of file usb_descriptors.c.
Referenced by usb_user_get_descriptor().
Initial value:
{
sizeof(usb_user_language_id)
, DESCRIPTOR_STRING
, Usb_write_word_enum_struc( 0x0409 )
}
Definition at line 186 of file usb_descriptors.c.
Referenced by usb_user_get_descriptor().
1.5.3